• MIMXRT1060-EVK flashing red light rapidly during debug

    I'm running the example hello world example for the MIMXRT1060-EVK and it builds fine, but when i try to debug it, it stops at the first function inside main.c, which is BOARD_ConfigMPU(). It says there is a temporary...
    Ahmed Mostafa
    last modified by Ahmed Mostafa
  • Update problems MCUExpresso - ConfigTools

    MCUExpresso on Ubuntu 18.04 using LPC11u68.   All was going well, until the other night I clicked on the message  that said that updates were available. I started the update and it looked as if the downloa...
    Tim Janes
    last modified by Tim Janes
  • IDE 11.1.1 SDK examples fail - fsl_common.h not found

    Hi, I've just upgraded to MCUXpresso IDE 11.1.1 and important an SDK example to get started. When building it the compiler complains that the file fsl_common.h is not found. But that file is included with the exampl...
    Torbjörn Johansson
    last modified by Torbjörn Johansson
  • Add Custom Tool to Toolchain

    I want to add some tools to the toolchain.  This is to add some steps that prepare and package the firmware image for OTA programming.  The idea is to get the IDE do it as part of the bui...
    Denis Collis
    last modified by Denis Collis
  • how to run gdb outside of the IDE?

    I am using MCUxpresso 11.1 with a stock MIMXRT1060-EVK board.   Can anybody provide guidance on how to manually start gdb outside the IDE and attach to the board?   I've found the gdb executable (/arm-none...
    Rob Yu
    last modified by Rob Yu
  • Can't delete terminated debug sessions

    I copied/reloaded a couple of projects coming from MCUXpresso 10 into a new MCUXpresso 11.1.1 workspace, but every time I launch debugger looks like it can't be properly terminated. After that, the only way to start a...
    Luca Matteini
    last modified by Luca Matteini
  • K64 UART1 first char is zero

    I setup a K64 uart1 to windows host ( c#)  two thing i see  1. The first byte that being sent is always zero. i am using the polling example ( modified to UART1)  2. the tx output fifo is inverted b...
    Eli Arad
    last modified by Eli Arad
  • OS ABSTRACTION LAYER TIMER

    qn9080-001-m17 wirelessuart periodictimer   Sebastián Del Río   Hi Devs, Sorry for my bad English I've been trying to get some data from the qn9080 and send it through wireless uart. But ...
    ASWIN P RAJ
    last modified by ASWIN P RAJ
  • Can not launch the debugger on MCUXpresso 11.1.1

    I just install the latest MCUXpresso IDE (MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02]) on my 64bits win10 surface pro 4. And importing a SDK sample for FRDM-KE06Z board, then make it is OK, but when I debug ...
    Zhong Shen
    last modified by Zhong Shen
  • LPC55S69 PLL1 does not function

    Hi     I am trying to use the inbuilt Clocks tool within MCUXpresso to configure the clocks for the FROHF96 functional group, for the LPC55S69EVK board.  I want to use PLL1 with the SD card, so I can r...
    Rory Hand
    last modified by Rory Hand
  • MIMXRT685-EVK trace

    I was trying to debug my program in MIMXRT685-EVK board via SEGGER J-Trace. However, the instruction trace cannot detect my target device and shows the following error:     Does it mean MIMXRT685-EVK trac...
    JIAMENG SHI
    last modified by JIAMENG SHI
  • QN9080 SDK sample project cannot be opened.

    Hello,   I am using QN9080SIP-DK to learn the basics of Bluetooth.   I downloaded the SDK. (SDK_2.2.2_QN908XCDK) However, the SDK project cannot be opened.   Please tell me how to avoid this. ...
    toshiyuki takagi
    last modified by toshiyuki takagi
  • MCUXpresso : create NOLOAD section

    Hi !   Does it possible to specify via IDE in MCU setting, RAM section what is not initialised at all ?   .data_SRAM4 0x30040000 (NOLOAD) : ALIGN(32) { }   Regards, Eugene
    Eugene Hiihtaja
    last modified by Eugene Hiihtaja
  • FreeRTOS TAD plug-in Task list view empty

    Greetings! I have some trouble with TAD for FreeRTOS on MCUExpresso IDE ( v10.2.1 [Build 795] [2018-07-25] ). I use FreeRTOS V10.1.1. I see nothing in Task list view, but other views (Heap, queue, timer) a...
    Valentin Nechunaev
    last modified by Valentin Nechunaev
  • Migrate from C to C++ project in MCUXpresso Ide

    Dear NXP,   We have project based on IMXRT1050 processor, existing project is based on the C now we want to migrated to C++, for that I have change the library based on the NXP document, then I added some C++ co...
    Dilli Babu
    last modified by Dilli Babu
  • MCUXpresso Flash Programmer - program binary w/ offset

    I'm trying to program custom data to flash on the RT1050.   If I program this custom data to the default start address (0x6000_0000), then it works fine - but I need to put the data at 0x6200_0000. FYI - Max ad...
    variable_andrew
    last modified by variable_andrew
  • QN9090 flash for LPC-LINK2 GUI Flash tool

    I am trying to Flahs Binary to QN9090 using LPC-link2. An error message is output and flashing is not possible. I need help. I don't know what is matter. i attached imaga.   MCUXpressoIDE version : MCUXpresso...
    Seungyeob Yi
    last modified by Seungyeob Yi
  • Why do I get "Processor 'MKV31F512xxx12' is not supported.. opening Config Tools?

    I'm trying to create a project using MCUXpresso V11 to run on a FRDM-KV31 eval board.  I started with File->New->New C/C++ Project (SDK Wizard), selected the eval board and added a few components.  Whe...
    Lance Fisher
    last modified by Lance Fisher
  • command line build run not successfull after first 1-3 tries

    Hello,   we are using a script to custumer board releases. When starting the build I see the 1-3 times the following output: Opening 'trunk'. Saving workspace. Mcuxpressoide: An error has occurred. See the log f...
    Lutz Volkmann
    last modified by Lutz Volkmann
  • MCUXpresso:  Missing header files even with correct include paths

    Hello,    I'm working on a project with the MK22FN1M0Axxx12 chip.   In my MCUXpresso project, I am using the SDK_2.x_MK22FN1M0Axxx12.  I have a few components from the SDK enabled such a...
    Carson Ennis
    last modified by Carson Ennis