• MCUXpresso IDE - Release History

    This document contains a history of the releases of MCUXpresso IDE, with links to the announcement blog for each release.   Receive email notification for new releasesIf you would like to receive notifi...
    LPCX presso support
    last modified by LPCX presso support
  • Exploring the Latest Features of MCUXpresso IDE v11.1.pdf

    View Webinar Recording
    Ethan Fernandes
    last modified by Ethan Fernandes
  • Important updates when using LPCXpresso55S69 Revision A2 boards and 1B silicon

    The LPC55S6x family was initial silicon die version was 0A, and this silicon was using on Revision A1 LPCXpresso55S69 boards. Revision 1B silicon has been used on Revision A2 boards. Both versions of silicon support t...
    Brendon Slade
    created by Brendon Slade
  • 在MCUXpresso IDE v11.0.0中使用LPC55S69 SDK Trustzone示例

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2019/06/12/using-lpc55s69-sdk-trustzone-examples-with-mcuxpresso-ide-v1100
    Leo Lin
    last modified by Leo Lin
  • Not able to download MCUXpresso IDE if account is inactive

    As a heads-up: several uses reported a problems with downloading the MCUXpresso IDE setup/installer program.   If pressing the 'Download' button, you might come back to the login screen (to log into your NXP use...
    Erich Styger
    last modified by Erich Styger
  • MCUXpresso IDE and Semihosting

    Semihosting printf with MCUXpresso IDE When importing MCUXpresso SDK projects into MCUXpresso IDE, they will be configured by default to use “semihosting” for the terminal output. This means the project w...
    Anthony Huereca
    last modified by Megan Hansen
  • Import project(s) from file system MCUXpresso IDE

    Dear Community,     The purpose of this document is to show how to integrate projects from the file system to MCUXpresso IDE.   It is actually not that complicated as you might have imagined.  &#...
    IvanRuiz
    last modified by IvanRuiz
  • Moving to MCUXpresso IDE from Kinetis Design Studio

    MCUXpresso IDE combines the best features of the LPCXpresso IDE and Kinetis Design Studio. For users more familiar with KDS, here’s a high level overview of some of the things that are different in basic interac...
    Anthony Huereca
    last modified by Megan Hansen
  • Generate disasseble file in MCUXpresso IDE

    Checking disassemble code is often needed for programmers when developing a project. This article will introduce two methods of generating disassemble file with GNU utility objdump under MCUXpresso IDE 10.1.0. If use...
    ZhangJennie
    last modified by ZhangJennie
  • How to create and use static library in MCUXpresso IDE

    For the previous KDS or CodeWarrior users, they may not create and use static library under MCUXpresso IDE without a hitch, because the methods are not exactly same. MCUXpresso IDE supports adding static library in u...
    ZhangJennie
    last modified by ZhangJennie
  • MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery)

    This tip will show you how to re-trigger a full probe discovery.  The feature is very useful for the customer who may use multiple debug probes.     The first time you debug a project, MCUXpresso ...
    Robin_Shen
    last modified by Robin_Shen
  • Importing an MCUXpresso SDK into MCUXpresso IDE

    MCUXpresso SDK packages are downloaded as .zip files. If you are using a 3rd party IDE such as IAR or Keil, then the package must be unzipped in order to access the project files. Also an unzipped SDK folder must be a...
    Anthony Huereca
    last modified by Megan Hansen
  • MCUXpresso IDE: Creating Binary Files (S-Record, Intel Hex, Binary)

    The MCUXpresso IDE has a versatile way to create different binary files (S-Record/S19, Intel Hex or raw Binary) which then can be used by other tools like flash programmer or bootloaders. Check out the IDE documentat...
    Erich Styger
    last modified by Erich Styger
  • MCUXpresso IDE: Fact Sheets

    Attached MCUXpresso IDE fact sheet gives an overview about the IDE and its capabilities. More information is available on MCUXpresso IDE|NXP .
    Erich Styger
    last modified by Erich Styger
  • MCUXpresso IDE: Overview (v10.0.0)

    As part of my university engagement, I have posted an overview article about the new MCUXpresso IDE: (external link): MCUXPresso IDE: Unified Eclipse IDE for NXPs ARM Cortex-M Microcontrollers | MCU on Eclipse ...
    Erich Styger
    last modified by Erich Styger
  • FAQ: MCUXpresso Software and Tools

    What is MCUXpresso software and tools? The MCUXpresso toolkit include three components: MCUXpresso IDE – an integrated development environment (IDE) MCUXpresso SDK  –  embedded runtime software ...
    Megan Hansen
    created by Megan Hansen
  • MCUXpresso Supported Devices Table

    MCUXpresso Supported Devices Table Supported devices and boards can also be viewed by searching within the MCUXpresso SDK Builder, please visit https://mcuxpresso.nxp.com/en/select. 
    Megan Hansen
    created by Megan Hansen