MCUXpresso IDE v10.1.1 Now Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE v10.1.1 Now Available

lpcxpresso_supp
NXP Employee
NXP Employee
0 0 10.3K

We are pleased to announce that MCUXpresso IDE v10.1.1 (build 606) is now available.

 

This is a minor update to the MCUXpresso IDE v10.1.0 release, the main changes being to fix a small number of SDK handling related issues.

 

To download the installer for all platforms, please login to our download site via:

 

Overview of Changes - version 10.1.1 - released Jan 2018

  • Fixed an issue seen when importing a single SDK example, in which example-specific settings could in some circumstances be overridden by IDE defaults
  • Fixed an issue with SDK example import failing to set the correct memory definition in a generated project, in a situation where there is an example-specific memory configuration and also one in the manifest for the board itself