• LPC Link2 COM port

    Content originally posted in LPCWare by dalzan on Tue May 17 15:45:50 MST 2016 Hi, I am a beginner with LPC/ARM. When I connect LPC Link2 via USB to my computer and launch Debug there appear 2 "HID Standard Devices" ...
    lpcware
    last modified by lpcware
  • void vPortEndScheduler( void ) Cortex-M3  implementation?

    Content originally posted in LPCWare by alanisgp on Wed Apr 18 07:22:42 MST 2012 Hello, I am using the version of FreeRTOS for Cortex-M3. For an application of secondary bootloader. My application download and save i...
    lpcware
    last modified by lpcware
  • Migraton from IAR project to LPCXpresso IDE

    Hello,   I have problem to migrate IAR IDE project to LPCxpresso IDE. uC is lpc1313.   I have project in IAR ide(iar compailer) with iar's bit fields register description. Because of certain reasons I need...
    zigamahne
    last modified by zigamahne
  • How to write datas in lpc1769 i2c eeprom  which is above page boundary

    Content originally posted in LPCWare by aarthi on Thu Aug 04 06:13:24 MST 2011 Hi,    i am not able to write databytes in lpc1769 i2c-eeprom(at24c08) which is above the pageboundary of the at24c08.i also use...
    lpcware
    last modified by lpcware
  • Still bug in AN11538 SCTimer/PWM cookbook

    Content originally posted in LPCWare by 1234567890 on Tue Jun 02 05:17:32 MST 2015 Fig 2 on page 6 of AN11538 Rev. 3.1: LPC_SCT->MATCHREL[0].U = SystemCoreClock/100; // match 0 @ 100 Hz = 10 msec must be L...
    lpcware
    last modified by lpcware
  • LPC1343 VCOM driver + Windows 7 64bits

    Content originally posted in LPCWare by Lean966 on Tue Jun 01 14:06:49 MST 2010 Hi, I want to know if exits lpc134x-vcom.inf file for Win 7 64 bits. The file in the usbcdc folder is for 32 bits OS. I hope that someone...
    lpcware
    last modified by lpcware
  • I'm new to LPC and need help with I2C

    Content originally posted in LPCWare by jherrera8 on Fri Oct 07 11:20:12 MST 2011 Hello, I am working on a school project and I need some help understanding the code for I2C. I have a 1769 and I am trying to use an ...
    lpcware
    last modified by lpcware
  • Arrays in struct

    Hello, i am new with lpc1549 in the om13056 board. I am using it for one of my master's project and i am having few problems. In some part i am calculating a controller and for that i new some values, i took th...
    Ander Goya Aguirre
    last modified by Ander Goya Aguirre
  • LPCXpresso lpc1769 rev-c board

    Content originally posted in LPCWare by barianand on Sat Oct 24 04:04:36 MST 2015 Hello, I am beginner in lpc1227. I am trying to program for lpc1227 with lpcxpresso v7.9.2_493 & through the LPCXpresso lpc1769 rev...
    lpcware
    last modified by lpcware
  • External makefile project debugging problem

    Content originally posted in LPCWare by ArtjomGromak on Fri Mar 02 15:32:24 MST 2012 Hi! I use LPCXpresso for debug my program(as toolchain I use YAGARTO). But I want use LPCXpresso for editing and building too. I imp...
    lpcware
    last modified by lpcware
  • LPC1768, uart using FDR at higher baud rates

    Content originally posted in LPCWare by pausten on Sat Jan 01 16:52:52 MST 2011 Hi, I've modified some of the uart example code to configure the baud rates using the uart fractional divider register (as per the data ...
    lpcware
    last modified by lpcware
  • Managed linker scripts not generated

    Content originally posted in LPCWare by safarmer on Mon Nov 24 00:36:11 MST 2014 Hi, When I try to build my project, I get an error about linker scripts not being found:   ld: cannot open linker script file proj...
    lpcware
    last modified by lpcware
  • is on-chip RTC in LPC1769 accurate?

    Content originally posted in LPCWare by karuna on Wed May 18 01:11:24 MST 2011 I am using LPC1769 controller. I need a perfect time reference. Is it preferable to use on-chip RTC?   Because I am using external cr...
    lpcware
    last modified by lpcware
  • How to run LPCpresso54608

    When  I biuld demo sample "lpcxpresso54608_demo_apps_touch_cursor" and run(run as/run configuration/run) on MCUXpresso ,the error occured. Comment is"" Launching lpcxpresso54608_demo_apps_to...
    実 奥山
    last modified by 実 奥山
  • No connection to emulator device

    Content originally posted in LPCWare by Simon Stark on Wed May 11 05:13:24 MST 2016 Hello, I'm using a LPC 4357 Board mit LPCLink2. When I try to flash a program onto the board I get the following message: Ni: LPCXp...
    lpcware
    last modified by lpcware
  • Multiple markers at this line / Breakpoint attribute problem:  installation failed

    Content originally posted in LPCWare by Meyer on Mon Oct 21 02:42:13 MST 2013 Hí Lpcxpresso-Team, I have a problem when debugging my project. I can put in any C file a breakpoint except IoDrvSimple.c. It compil...
    lpcware
    last modified by lpcware
  • Driver 4-bit 16x2 LCD display LPC1769

    Content originally posted in LPCWare by tmoerkerken on Sun Feb 02 16:05:34 MST 2014 Hey guys, I'm new to the lpcxpresso. I have a simple 16x2 LCD display which I want to interface with 4 datapins. I want to display s...
    lpcware
    last modified by lpcware
  • LPCXpresso: Unable to add a header file (undefined reference error)

    Hi!   I am trying to separate led code in a different file and I am facing following issues:   Issue #1    I Created a new folder by    Right clicking project -> New...
    kembed
    last modified by kembed
  • LPC4330FBD144, Problems booting from reset and cold

    Hi.   I've designed a custom board using an LCP4330 and trying to some leds to turn on as a first step. All was fine downloading the image with the debugger LPC-LINK2 and the program started ok and the leds lit ...
    hans söderlund
    last modified by hans söderlund
  • Customize perspective

    Content originally posted in LPCWare by renan on Thu Jan 06 03:06:50 MST 2011 When I try to customize the Develop perspective, this is the toolbar visibility tab I get (all versions of LPCXpresso are exactly like this...
    lpcware
    last modified by lpcware