• Latest UART Driver for Kinetis K60

    Hello,   Where can I get the latest version (2.1.5) of UART driver for Kinetis K60?   With MCUXpresso (MCUXpresso IDE v11.0.0 as well as the previous version) and Kinetis SDK (Release Name: MCUXpresso Soft...
    Satish Acharya
    last modified by Satish Acharya
  • [Solved] FRDM-K64F -> SDK_2.6.0 -> lwip_mqtt(bare metal)

    Hello, I am looking for a lwip_mqtt (bare metal) example, I want to use it to do some applications, but currently in the FRDM-K64F SDK_2.6.0, lwip_mqtt example only provides FreeRTOS version. I would like to ask if t...
    York Tsai
    last modified by York Tsai
  • No source available for "(gdb[1].proc[42000].threadGroup[i1],gdb[1].proc[42000].OSthread[1]).thread[1].frame[0]"

    I am working on FRDM-K64F board. I build the project and after debugging I get the following: No source available for "(gdb[1].proc[42000].threadGroup[i1],gdb[1].proc[42000].OSthread[1]).thread[1].frame[0]" No sourc...
    kirantujare
    last modified by kirantujare
  • Number conversion host to big endian

    Hi,   I'm working on MKE1xF family over SDK2.5 and I'm looking for a solution for endian to host converter like htons(). My problem is that if I had a number and I want to convert to little/big endian, what is...
    Jordi Becares
    last modified by Jordi Becares
  • MCU Bootloader for Frdm MKV31F

    Hey, I am trying to run an application(led_demo_a000) on on mkv31f board, but first I was wanting to run the bootloader. The steps I followed were similar to mentioned in MCU bootloader demo application.  Issue...
    sidhant singhal
    last modified by sidhant singhal
  • CAN transmisison on S32k146

    Hi Team   CAN communication development on S32K146 microcontroller and facing below issues. Could you please help us in resolving these.   1) After transmission, not able to see respective buffer bit set...
    SUDEENDRA S
    last modified by SUDEENDRA S
  • CAN issues on S32K146

    Hi   CAN communication development on S32K146 microcontroller and facing below issues. Could you please help us in resolving these.   1) After transmission, not able to see respective buffer bit set in I...
    SUDEENDRA S
    last modified by SUDEENDRA S
  • SDK for KEAZN32Q64 FRDM EVAL BOARD

    Hi Using KEAZN32Q64 freedom eval board. i am not able to find SDK related to this board.Please help to get the link of SDK;s   Regards Sudeendra S
    SUDEENDRA S
    last modified by SUDEENDRA S
  • Regard to the cdc endpoint in usb composite ( cdc + msd ) 

    Hello, I create the usb composite cdc msc project, and I'm going  to see usb_device_descriptor.c/.h, I don't understand that Bulk IN and Bulk OUT endpoint number is same in the endpoint descriptor of Data Interf...
    JingHuan Huang
    last modified by JingHuan Huang
  • Kinetis SDK Printer Class Demo App Bug

    All,   I'm writing this discussion to bring to light a bug in the printer class example code in the Kinetis SDK. Specifically in the demo app that is provided. The example is called "usb_device_printer_virtual_p...
    Matt Lang
    last modified by Matt Lang
  • LWIP_INIT

    Good morning   I need to reinit the stack run time. I tried to use the lwip_init() but it craches. Has someone a good suggestion on how to reinit the stack at a later time???   Thank You   Pietro
    Pietro di Castri
    last modified by Pietro di Castri
  • How do you detect (and handle!) a lwIP disconnection?

    My application handles graceful closing of the socket, but it does not recognize when the Ethernet cable has been disconnected.   In my packet-handling loop, I check the result of all netconn commands used, whic...
    dave408
    last modified by dave408
  • K21 UART4 RX with DMA problem

    Hi,   I meet a problem on UART4 Rx with DMA. I tried to modify and build driver_examples\uart\edma_transfer in KSDK2.0. The modifications as following: pin_mux.c CLOCK_EnableClock(kCLOCK_PortC); PORT_SetPinM...
    Jim Yang
    last modified by Jim Yang
  • OM40007 LPC54018-based IoT Module with Amazon FreeRTOS example error

    In the SDK example , lpc54018iotmodule_aws_aws_shadow_wifi_qspi_xip , I see some errors as below : 2769 1550441 [ShDemoUpdt] Successfully performed update. 2770 1555027 [Shd-IOT-0] Shd-IOT-0 changing desired state. ...
    Rick Tseng
    last modified by Rick Tseng
  • Brief Introduction to LwIP stack in MCUXpresso SDK

      LwIP is a small independent implementations of the TCP/IP protocol suite that has been initially developed by Adam Dunkels . The focus of the lwIP TCP/IP implementation is to reduce resource usage while still...
    Daniel Chen
    last modified by Daniel Chen
  • UART transmission for PN7462

    Where can I find the sample code about the UART transmission for PN7462?   Thanks in advance, Vincent
    Vincent Chen
    last modified by Vincent Chen
  • Secure Bootloader AES help

    Hello! I would like to use on kinetis KV11Z and MK22FX the bootloader with security aes. When I try to compile, it asks me for the file aes_security.h and I can't find it. Can anyone help me? Is there a step by ste...
    Marco Bologna
    last modified by Marco Bologna
  • Latest data sheet for TWRK60D100M board required

    I am using tower board TWRK60D100M with 700-27291 REVA board.When I checked the data sheet,the one which is existing is not matching with the case of jumper for example J19 jumper information is not present in the dat...
    sunil vasudevan
    last modified by sunil vasudevan
  • SDK2.6 composite cdc msc lite example with printf on the LPC54608

    Hello,     I am trying to merge printf functionality from the hello world example in the sdk with the composite cdc msc example project.  the composite device project works fine, and i'm able ...
    Eileen Radzwion
    last modified by Eileen Radzwion
  • FreeRTOS + TCP

    Hi   Does NXP has plan to support FreeRTOS + TCP in SDK ?
    David Zhu
    last modified by David Zhu