• Brief Introduction to LwIP stack in MCUXpresso SDK

      LwIP is a small independent implementations of the TCP/IP protocol suite that has been initially developed by Adam Dunkels . The focus of the lwIP TCP/IP implementation is to reduce resource usage while still...
    Daniel Chen
    last modified by Daniel Chen
  • How to create an FreeRTOS project with MCUXpresso IDE

    This article is for beginners. It describes how to create an FreeRTOS project based on MCUXpresso IDE 10.2.1.   Software and Tools In this article, I’m using the following: MCUXpresso IDE 10.2.1 ...
    Daniel Chen
    last modified by Daniel Chen
  • Let´s start with FreeMASTER!

    What is it FreeMASTER?   FreeMASTER is a tool with variety GUIs in one offered free. FreeMASTER is a user-friendly real-time debug monitor and data visualization tool −GUI can be easily extend by multimed...
    Iva Susnova
    last modified by Diana Torres
  • An example to use MCUXpresso Pins Tool in a FreeRTOS project

    MCUXpresso Pins Tool allows you to configure pin routing and generates ‘pin_mux.c & h’ source files. This article describes how to configure Pins in a FreeRTOS project with MCUXpresso pins tool.  ...
    Daniel Chen
    last modified by Daniel Chen
  • An example project for FIR function implement on KV31 with SDK and CMSIS

    This example project shows how to use CMSIS DSP functions to implement a digital filter. The project is based on Kinetis KV31F512.   It first generates a mixed signal which is composed by two sine waves.  ...
    Fiona Kuang
    last modified by ebiz_ws_prod
  • A demo project of USB HID bi-directional generic device for Kinetis SDK 1.1.0

    The latest Kinetis SDK 1.1.0 supported HID bi-directional communication, the new API USB_Class_HID_Recv_Data() can be used to receive data from USB HOST. But without demo and test tool, customer still has no idea abou...
    Neo Xiong
    last modified by ebiz_ws_prod
  • DAC Sinus Demo (using PEx + KSDK 1.2 + KDS 3.0)

    Created DAC Sinus example is PIT triggered with own buffer and is for FRDM-K64F.  adding analog component fsl_dac peripheral driver to project setting Voltage reference - Reference 2 for dac component (daConv...
    Iva Susnova
    last modified by ebiz_ws_prod
  • UART Example with KSDK

    I created easy tutorial for UART KSDK blocking demo which works as echo. The demo works with KSDK 1.1. and is created for KDS 2.0.   Because it could be problem if was used this pin by this reason was chos...
    Iva Susnova
    last modified by ebiz_ws_prod
  • KSDK Clock configurations and Low Power modes with Processor Expert

    Hello dear community:   The attached document is an introductory guide to the Clock configuration system and Power manager system in KSDK v1.3 and its configuration using Processor Expert.   Some topics co...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • Integrating NFC Controller library with KSDK

    Hello community:   This document shows how to integrate a basic NFC (Near Field Communication) library to a KSDK project and explain its use with a simple demo project.   INTEGRATING NFC CONTROLLER LIBRARY...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • Driving 16x2 LCD using KSDK drivers

    Hello to all,   This document explains how to drive a 16x2 LCD using the KSDK Drivers using the FRDM-KL25Z.     Project Generator, KSDK1.3 and KDS3.0 are used in this example.   I hope you fin...
    David Diaz Marin
    last modified by ebiz_ws_prod
  • Configuring Kinetis Software Development Kit (SDK) to measure distance with infrared (IR) sensor

    For this demo, Kinetis SDK was configured to implement a distance meter using a FRDM-K64F and the GP2D12 IR Sensor. The operating principle of this sensor consists in sending IR pulses and according to the existing di...
    Abigail Inzunza Lopez
    last modified by ebiz_ws_prod
  • Using DMA to Emulate ADC Flexible Scan Mode with KSDK

    This community post describes how to combine the ADC and DMA using KSDK to simulate a flexible peripheral storing the ADC results into a buffer stored in memory.   In this configuration the MCU uses less res...
    Ricardo Olivares Duran
    last modified by ebiz_ws_prod
  • How to implement a USB Device MSD demo based on KSDK PEx components and KDS 3.0

    Hardware and software configuration: FRDM-K22F, SCH-28164 REV D OpenSDA: J-Link firmware KDS 3.0 with SDK 1.2.0 Eclipse update installed   KSDK 1.2 provides an Eclipse update for those who want to use the Ki...
    Kan_Li
    last modified by ebiz_ws_prod
  • Rainbow color using FTM PWM with KSDK 1.3

    Hi all,   there is a simple modification of ftm driver example based on KSDK 1.3, KDS 3.0 on FRDM-K22F.   enabling clocks for PORTs in hardware_init.c   void hardware_init(void) {    /* enab...
    Iva Susnova
    last modified by ebiz_ws_prod
  • Create new KSDK Projects

    At the moment the best way to create a new KSDK example project is copying one of the existing projects in the /demos folder and renaming all the files and text to the new name. I've created a simple script that does ...
    Anthony Huereca
    last modified by ebiz_ws_prod
  • Kinetis SDK and FRDM-K64F

    Kinetis SDK is a new complimentary software offering from Freescale for Kinetis microcontrollers. The Kinetis software development kit (SDK) provides an extensive suite of robust peripheral drivers, stacks, middleware...
    Anthony Huereca
    last modified by ebiz_ws_prod
  • FatFs + SDHC data logger with KSDK in Kinetis Design Studio

    Hello KSDK friends:   This time I want to share with the community a project using FatFs and the SDHC + I2C drivers provided with the Kinetis SDK platform. This is a baremetal project with no RTOS.   If yo...
    Jorge_Gonzalez
    last modified by ebiz_ws_prod
  • [SDK 2.0]ADC demo with DMA support

    This demo is based on adc12_polling example , and so far I just tested it with FRDM-KE15Z, so please download SDK_2.0_FRDM-KE15Z.zip from Welcome to MCUXpresso | MCUXpresso Config Tools before you try that demo.  ...
    Kan_Li
    last modified by ebiz_ws_prod
  • Line scan camera with KSDK [ADC + PIT + GPIO]

    Hello community,   This document shows the ease of use of the peripheral drivers from Kinetis SDK applied to the Freescale Cup smart car. This time I bring to you a document which explains how to make the line s...
    Earl Orlando Ramirez Sanchez
    last modified by ebiz_ws_prod