• Hexiwear programming on KDS

    Hi, I am being interrupted to program Hexiwear because of error that appear while build process.  When I try build MK64 KDS that error comes up. What should I do for that?
    Subin Seonwoo
    last modified by Subin Seonwoo
  • Memory Problems with KE06Z

    I am using the MKE06Z128 44 pin chip to replace the current processor for our company. I have been trying to understand memory issues and where my problems may lie.    Currently I have strange problems...
    cody hubman
    last modified by cody hubman
  • KDS Projects in Windows 7 transfer to Windows 10

    Hello,   We have a firmware project that's based-on Kinetis MK22FX512 MCU which was developed in Kinetis Design Studio v3.0.0 using KSDK  v1.3.0, all under Windows 7.     I took ov...
    M I
    last modified by M I
  • Problems with importing NXP examples into Codewarrior V11.1

    Hi, I loaded the examples for Gen4xs switches (Gen4eXtremeSwitch_PEx_SW.zip) and wanted to add the examples to Codewarrior workspace. I created a new project with existing code, select the directory and let copy the ...
    Mehrdad Ostovary
    last modified by Mehrdad Ostovary
  • Semi-Hosting in Kinetis Design Studio with MQX

    Hello, When I build a baremetal project in Kinetis Design studio using the KSDK I can successfully get semi-hosting to work with printf outputs on the console inside of KDS. This is configured in the Debug Configurat...
    jschepler
    last modified by jschepler
  • fatal error: PE_low_level_init.h: No such file or directory

    Hi everyone. I'm having a problem (actually two) when compiling my project. When I do it, I get this message that you can see on the image below. The first error, the file exist, but it is in another path. I ...
    Nícolas Ludwig
    last modified by Nícolas Ludwig
  • Can't Install New Software in KDS 3.2

    Hello,  I have installed KDS 3.2 today and have been trying to follow this introduction, https://www.allaboutcircuits.com/projects/getting-started-with-freescales-kinetis-design-studio/ however whenever I try ...
    Stephen Bates
    last modified by Stephen Bates
  • OM13260 replacement board

    Hi,   I would like to use efficient NXP Fm program for testing PCAL6524 build boards. What is replacement for use USB to I2C interface OM13260 board, which not more manufactured. Can I connect FRDM-MKL25Z demo b...
    Marceli Firlej
    last modified by Marceli Firlej
  • Use MIMXRT1052CVL5B Drive FT6336U

    Use the SDK_2.5.0_MIMXRT1052xxxxB2\boards\evkbimxrt1050\emwin_examples\emwin_gui_demo drive the FT6336U TFT LCD. First I used the demo touchpanel code fsl_ft5406_rt.c, change the I2C_slave_ADDRESS,find the c...
    DEGANG YU
    last modified by DEGANG YU
  • How to send 2 or more bytes of data by using PE KEA128

    Hi all,      I'm developing some audio application with KEA128, I was able to generate a sound using analog ports mainly PWM, for now, I moved to a digital audio application which KEA128 not so strong...
    Sheng Zhang
    last modified by Sheng Zhang
  • Function placed in RAM - assembler warnings

    Hello everybody, I'm using KDS 3.0.0 and the micro is Kinetis K10. I need to place a function in RAM (and of course run it from there!) As suggested in the application notes "Relocating Code and Data Using the ...
    alessandro carozzi
    last modified by alessandro carozzi
  • TWR-K60f120m and FRDM-K64f CAN communication

    I'm trying to setup CAN communication between the FRDM-K64f and the TWR-K60f120m with a TWR-SER board. I'm running the Flexcan example from the KSDK for the FRDM and the Flexcan example from MQX 4.2 for the TWR. I was...
    Timothy Smith
    last modified by Timothy Smith
  • Can we store hex data through UART into flash and RUN it from that particular location

    I am trying to store my hex file in another sector of the flash memory i.e (0x00050000) I want to store a hex file at different sector of the flash and to change the execution point to that address through my bootload...
    Keerthana R
    last modified by Keerthana R
  • Relocating Code and Data Using the MCUXpresso IDE

    This document provides some sample codes and steps for relocating Code and Data into RAM/FLASH. Please look at them with projects in attachment. It is based on “MCUXpresso_IDE_User_Guide.pdf”, so about the...
    Alice_Yang
    last modified by ebiz_ws_prod
  • Relocating Code and Data Using the KDS GCC Linker File for Kinetis

    This document provides guidance for relocating Code and Data within the MCU memory map. As part of this process it explains how create new memory segments and sections by editing the GCC Linker File (.ld) for Kinetis ...
    Carlos_Mendoza
    last modified by Diana Torres
  • Need help to develop a custom flash bootloader for firmware updating KL27Z

    Hi fellow community members,   I'm wondering if anybody can give me some advice how to start developing a custom bootloader in flash for the Kinetis MKL27Z256? I'm using this MCU to connect with a BLE module thr...
    Daniel Truong
    last modified by Daniel Truong
  • How to flash the micro every time debug is entered

    KDS is being used to develop a M0+ project. The problem I am having is it appears when debugging, KDS does not reprogram the flash every time. Sometimes it does and sometimes it does not. It seems program changes are ...
    KEVIN KRATZER
    last modified by KEVIN KRATZER
  • How to debug with CYCLONE Universal on KDS?

    Hi,   After spending a couple of hour searching for information online without luck, I decided to present my question here, we have a "Cyclone Universal" from P&EMicro, and I want to use as debugger to track...
    Enlai Aranzabal
    last modified by Enlai Aranzabal
  • Update KDS compiler

    Hi,   I have a very big project on KDS 3.2 with SDK 1.3 and my eclipse version is Luna SR2 (4.4.2).   I'm using GCC/G++ 5.2 and I'd like to know if its possible to upgrade it to a newer version, like a 7.x...
    Arthur Passos
    last modified by Arthur Passos
  • KDS - attach debugger issue

    Using KDS 3.0, SDK 1.3, PE Multilink JTAG.   I just started using my app with the Kinetis bootloader. Prior to using the bootloader I was able to use a debug configuration to attach to an already installed appl...
    Randy Hermes
    last modified by Randy Hermes