• How do I compare output from two different KDS (eclipse/codewarrior) installations?

    I have a production machine which has been working well and generating the code I want.  Now I need to take it on the road--after much struggle i have KDS running on my laptop.  Is there a way to check the o...
    Andrew Meyer
    last modified by Andrew Meyer
  • Energy metering TWR-KM34T75M

    Hello, I bought the TWR-KM34Z75M development kit. I would like to realize a 1 phase energy measurement with it.   However, it does not want to work. There are already problems building the project using the exam...
    Hurek Dariusz
    last modified by Hurek Dariusz
  • breakpoint - "No source file named"

    Hi There,   I have recently moved a project from an old hard drive to a new one.  I have been able to import this project into KDS and build no problems.  But, when I go to debug I get "No source file ...
    mjg8t
    last modified by mjg8t
  • USB Serial on frdm-k82f with Android

    Hello,   I am working on the frdm-k82f:to have a serial communication between board and Android device. But all the sample programs from the SDK I have tried was a failure.   The android device is ab...
    Ajayan Edayillam
    last modified by Ajayan Edayillam
  • Update fails

    When I check for updates, KDS 3.2 says there are a few updates to things like PEMicro debugger and FreeRTOS debugging plugin.  When I try to update, I get this:   An error occurred while collecting items to...
    David Sherman
    last modified by David Sherman
  • Kinetics design studio repository problem

    Ik krijg volgende foutmelding bij het zoeken naar updates en het installeren van new software in Kinetics Design Studio V3.2.0   No repository found at http://gnuarmeclipse.sourceforge.net/updates.   Ieman...
    kurt plaetevoet
    last modified by kurt plaetevoet
  • Not able to debug the code.

    Hello,   Currently, I am working on FRDM-KW36 development board. As per the BLE demo application user guide document I have uploaded the code of HRS(Heart Rate Sensor) on the development board. Then i checked it...
    Chintan Patel
    last modified by Chintan Patel
  • Which is recommended utility vs nanolibc for M0+

    I am planning to add assertions to my debugging tool capabilities.  Erich Styger has a couple of very helpful posts explaing how to get around the code bloat of stdio.h.  There are two different recommendati...
    KEVIN KRATZER
    last modified by KEVIN KRATZER
  • How to install and make USBDM programmer work in KDS 3.2

    Hello, pgo   I just bought a programmer running your USBDM from Luciano in Brazil.   Could you please explain me how to install USBDM plugin to make KDS 3.2 recognize USBDM programmer? I have carefully fol...
    Marco Aurelio P. Coelho
    last modified by Marco Aurelio P. Coelho
  • MCU bootloader Crc Check Option leads to to security breach

    Hello,   One question about mcu bootloader on MCU Xpresso V11.01 and KinetisFlashTools. Like i can see in the picture below it is possible to the mcu boot loader to launch an application whihout checking the cr...
    Didier JEANJEAN
    last modified by Didier JEANJEAN
  • Compile PE KDS project using ARM Compiler 6

    I have a c++17 project currently compiling with G++ 8.x, but I'm running out of flash memory. I've read that the ARM Compiler 6, used on Keil, is very effective on reducing the binary size, so I'm trying to migrate fr...
    Arthur Passos
    last modified by Arthur Passos
  • How to Maximize FLEXCAN Throughput?

    Hi everyone,   I'm trying to get the K20 series chip's CAN controller to have the highest throughput possible. I've configured my CAN 1 port at 500 kbps and am transmitting an extended (J1939) frame every 1...
    Brad Shelton
    last modified by Brad Shelton
  • Link m_text section to the D-FLash

    Hello, I am facing a problem that my code exceeds the plash size. Since the microcontroller that i am working with have a d-flash. Is it possible to specify for the linker to move the m_text section to the d-flash in...
    Haggui Souhail
    last modified by Haggui Souhail
  • WARNING: Failed to read memory @ address 0x00000000

    Hi,   I'm running k66 with MQX 4.02. I'm getting the warning randomly. When this happens the debugger is disconnected but the target keeps running and it appears it runs correctly. Any idea how to debug?  ...
    Ariela Blumer
    last modified by Ariela Blumer
  • KBOOT for KDS3.2.0 with SDK2.0

    Hello,I have to integrate a bootloader on a MK22FN512, For an important finished application developed on KDS3.2.0 with Eclipse and SDK 2.0 I want to load application firmware via UART0 interface. We bought 2500 parts...
    Didier JEANJEAN
    last modified by Didier JEANJEAN
  • How to detect Low voltage on K64  using Processor expert?

    Hi , I am working on K64FN controller with KDS 3.2.0. I would like to detect low voltage on K64 for writing data to flash to protect it from being erase on power on reset. I am using processor expert for my project. ...
    kirti raje
    last modified by kirti raje
  • Relocating specific function in RAM Location

    Hi,   I am using MKE04Z128VLH4 controller in one of my project. I am using this controller for parallel communication with other controller using GPIO lines. But the timming whihc is comming is not as exepe...
    Gaurav More
    last modified by Gaurav More
  • LWIP 2.0.0 problem

    Hi,   I am using KDS3.2.0 with LWIP 2.0.0 on K66. I am using sample httpd web server and found the following problem:   Sometime, I got "LWIP_ASSERT("tcp_input: pcb->next != pcb (before cache)", pc...
    Christie Su
    last modified by Christie Su
  • Workspace will not connect with KDS?!!!

    I have selected my workspace location, and the project explorer is empty. I have also switched the workspace using the File directory but the explorer remains empty. It seems like there is a discontinuity between the ...
    Jose Tafolla
    last modified by Jose Tafolla
  • KDS project wizard

    Hi I need to maintain a project based on K27. I'd like to test on frdm K27 some things before to work on the official project but I can not see in the wizard menu the K27 freedom board just to start. From the new pr...
    Claudio Brunelli
    last modified by Claudio Brunelli