• Relocating specific function in RAM Location

    Hi,   I am using MKE04Z128VLH4 controller in one of my project. I am using this controller for parallel communication with other controller using GPIO lines. But the timming whihc is comming is not as exepe...
    Gaurav More
    last modified by Gaurav More
  • LWIP 2.0.0 problem

    Hi,   I am using KDS3.2.0 with LWIP 2.0.0 on K66. I am using sample httpd web server and found the following problem:   Sometime, I got "LWIP_ASSERT("tcp_input: pcb->next != pcb (before cache)", pc...
    Christie Su
    last modified by Christie Su
  • Kinetis Bootloader for FRDM-K64

    After we released the "Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4" (Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4 ), many customers want to port it to FRDM...
    Alice_Yang
    last modified by ebiz_ws_prod
  • Workspace will not connect with KDS?!!!

    I have selected my workspace location, and the project explorer is empty. I have also switched the workspace using the File directory but the explorer remains empty. It seems like there is a discontinuity between the ...
    Jose Tafolla
    last modified by Jose Tafolla
  • KDS project wizard

    Hi I need to maintain a project based on K27. I'd like to test on frdm K27 some things before to work on the official project but I can not see in the wizard menu the K27 freedom board just to start. From the new pr...
    Claudio Brunelli
    last modified by Claudio Brunelli
  • The project description file (.project) for my project is missing

    Context: I know that KDS is being phased out, but I have a client who needs a bugfix.    Problem: When I launched KDS 3.2 with the client's workspace, I got the message: The project description file (.proj...
    Robert Poor
    last modified by Robert Poor
  • assert() behaviour

    KDS 3.0 SDK 1.2 Using MQX   I'm using assert() to check some parameter ranges.   When it is triggered it drops into a infinite loop and nothing is output on the debug console. There isn't any source for...
    Randy Hermes
    last modified by Randy Hermes
  • Failure in the NXP Website. Cant find page.

    Hi,   When I go in the page https://community.nxp.com/docs/DOC-103698 to bottom and click on Kinetis design studio page then I get an error that the page is not found.   Best regards, Osto
    Mehrdad Ostovary
    last modified by Mehrdad Ostovary
  • KV58 S19 file

    Hi,   I am using "arm-none-eabi-objcopy --srec-len=64 --srec-forceS3 -O srec "aaa.elf"  "aaa.S19"" to generate S19 file. The generated S19 as follows. At the end of file, it is not 64-bit alignment... " ...
    Christie Su
    last modified by Christie Su
  • srec file is not deleting on clean

    Hello Team,   https://community.nxp.com/thread/445108 above link worked for me to generate srec file.    My question is upon Clean, only elf file is getting deleted and srec file is not getting delet...
    sudhanshu mehta
    last modified by sudhanshu mehta
  • Hexiwear programming on KDS

    Hi, I am being interrupted to program Hexiwear because of error that appear while build process.  When I try build MK64 KDS that error comes up. What should I do for that?
    Subin Seonwoo
    last modified by Subin Seonwoo
  • Memory Problems with KE06Z

    I am using the MKE06Z128 44 pin chip to replace the current processor for our company. I have been trying to understand memory issues and where my problems may lie.    Currently I have strange problems...
    cody hubman
    last modified by cody hubman
  • KDS Projects in Windows 7 transfer to Windows 10

    Hello,   We have a firmware project that's based-on Kinetis MK22FX512 MCU which was developed in Kinetis Design Studio v3.0.0 using KSDK  v1.3.0, all under Windows 7.     I took ov...
    M I
    last modified by M I
  • Problems with importing NXP examples into Codewarrior V11.1

    Hi, I loaded the examples for Gen4xs switches (Gen4eXtremeSwitch_PEx_SW.zip) and wanted to add the examples to Codewarrior workspace. I created a new project with existing code, select the directory and let copy the ...
    Mehrdad Ostovary
    last modified by Mehrdad Ostovary
  • Semi-Hosting in Kinetis Design Studio with MQX

    Hello, When I build a baremetal project in Kinetis Design studio using the KSDK I can successfully get semi-hosting to work with printf outputs on the console inside of KDS. This is configured in the Debug Configurat...
    jschepler
    last modified by jschepler
  • fatal error: PE_low_level_init.h: No such file or directory

    Hi everyone. I'm having a problem (actually two) when compiling my project. When I do it, I get this message that you can see on the image below. The first error, the file exist, but it is in another path. I ...
    Nícolas Ludwig
    last modified by Nícolas Ludwig
  • Can't Install New Software in KDS 3.2

    Hello,  I have installed KDS 3.2 today and have been trying to follow this introduction, https://www.allaboutcircuits.com/projects/getting-started-with-freescales-kinetis-design-studio/ however whenever I try ...
    Stephen Bates
    last modified by Stephen Bates
  • OM13260 replacement board

    Hi,   I would like to use efficient NXP Fm program for testing PCAL6524 build boards. What is replacement for use USB to I2C interface OM13260 board, which not more manufactured. Can I connect FRDM-MKL25Z demo b...
    Marceli Firlej
    last modified by Marceli Firlej
  • Use MIMXRT1052CVL5B Drive FT6336U

    Use the SDK_2.5.0_MIMXRT1052xxxxB2\boards\evkbimxrt1050\emwin_examples\emwin_gui_demo drive the FT6336U TFT LCD. First I used the demo touchpanel code fsl_ft5406_rt.c, change the I2C_slave_ADDRESS,find the c...
    DEGANG YU
    last modified by DEGANG YU
  • How to send 2 or more bytes of data by using PE KEA128

    Hi all,      I'm developing some audio application with KEA128, I was able to generate a sound using analog ports mainly PWM, for now, I moved to a digital audio application which KEA128 not so strong...
    Sheng Zhang
    last modified by Sheng Zhang