• KDS 3.0 Command Line Limit issue

    Hi, i have encountered the known issue of 8192 characters limit for Windows command line during the build. So i follow the proposed guide to solve it (Solving the 8192 Character Command Line Limit on Windows | MCU o...
    Francesco Salvatore
    last modified by Francesco Salvatore
  • USBDM Updated for KDS 3.0.0 and KSDK 1.2.0

    Dear All,   USBDM has been updated to support the latest versions of KDS and KSDK.   A video introduction is available at: USBDM with Kinetis Design Studio and Kinetis SDK - YouTube   The software i...
    pgo
    last modified by pgo
  • KDS 3.0.0 freezes from the start

    Hi, I am a new user both of Mac OS X (currently it is version 10.11.3) and wished to use KDS 3.0.0 (and of course 3.1.0) on Mac. In downloaded the KDS package for OS X and installed it. When starting the program it s...
    Tomás Bautista
    last modified by Tomás Bautista
  • Problem with KDS and Processor expert

    Hello, I have an old project wich works fine for me (it uses FRDMKL25, the include MMA8451 and an external I2C component). I would like to start a similar new project, unfortunatly something is going wrong. In my ol...
    Michel Meunier
    last modified by Michel Meunier
  • TOWER-K64F120 +FREERTOS+SHELL

    Hello, My target is TWR-K64F120 +TWR-SER2, using KDS and FREERTOS, I've created  a project which is running OK and I can communicate over the serial link to a terminal using the DB9 connector on the SER2 board...
    Koorosh Hajiani
    last modified by Koorosh Hajiani
  • How to configure MCU enter Vll0 and wake by lptmr and port in KDS 3

    I am using MKL02 and developemnt toos is KDS   How to configure MCU enter Vll0 and wake by lptmr and port in KDS 3(KSDK 1.3)?   i am not found componment in componment library.
    Thooman Wang
    last modified by Thooman Wang
  • KDS on OS X El Capitan (Beta)

    Hello,   If someone is trying to use/install KDS v3.0 on the public beta (4) of OS X El Capitan (10.11), you'll probably have a problem at the workspace selection. As i found no information about this on the In...
    Valentin Py
    last modified by Valentin Py
  • Firmware Version update

    Hello all,   i have a question if it is possible use the eclipse template or others for update a constant value define as:   static const unsigned short firmware_version =  0001;   for update au...
    Daniele Cortellazzi
    last modified by Daniele Cortellazzi
  • KDS Kinetis DMA Example

    Dear all, as I had a hard time figuering the DMA out, i created a simple example, showing a simple copy example for the DMA with error checking maybe somebody will find this useful. uint8_t source[]={0,1,2,3,4,5,6,7,...
    Michael Heidinger
    last modified by Michael Heidinger
  • GDB Server Stucking

    Hi,   I am working with KDS3.0.0 and MQX 4.2. I have created an MQX project in KDS. Everything was working fine until I start to debug code. When I tried to debug the code that seems to stuck at 95% of Projec...
  • GCC: KDS toolchain segfaults when dividing _Accum types

    I use the gcc's fixed point extensions, which have been present in the gcc for Cortex-M since 2011.   The toolchain which is included in the current version of KDS (4.8.4 20140725 (release)) gives me a segmentat...
    Dominikus Gierlach
    last modified by Dominikus Gierlach
  • Doxygen for MK22FX512VLQ12

    Hi all,   I'm developing a project with MK22FX512VLQ12 in LQFP 144-pin package. I use the Doxygen and Eclox plugin. When I generate the doc in html format, the pin s allocation for this package is not supported....
    Joaquim Martinez
    last modified by Joaquim Martinez
  • Processor Expert to KSDK-2.0

    Hi!,   I have one FRDM-K64F-AGM01 and also one BRKT-STBC-AGM01. I have tested some examples with mbed code and work. Both, the compiler online as exporting to KDS 3.0.2.   I have tried the FXO8700CQ integ...
    javierhernandezdeniz
    last modified by javierhernandezdeniz
  • K24 qfp-100 breakout

    I designed a breakout for the K24F in QFP-100 and shared the project on oshpark, details here:   http://jacobjennin.gs/post/145282647930/kinetis-k-series-qfp100-breakout   It may be pin compatible with oth...
    Jacob Jennings
    last modified by Jacob Jennings
  • KL15Z UART buffer "stutter"

    EDIT: After retrying different UART channels and un-commenting the code while(uart_GetCharsInTxBuf()!=0); My program is now working. There must have been an error in the generated code or init configuration that wa...
    Kevyn Schwab
    last modified by Kevyn Schwab
  • A message to KDS3.2 .deb package maker

    This message is to the person making the KDS3.2 package: Your dependency list is not full, especially that the 64bit system requires serveral 32bit dependencies. (e.g. libc 32bit). It would be significant more frictio...
    Michael Heidinger
    last modified by Michael Heidinger
  • How to properly import MBED-RTOS Libs to KDS

    Hi All,   I'm currently working on setting up KDS on my Mac so that I can develop on the FRDM-K64F. I have had a lot of success so far setting up my computer and mcu to debug using the Segger J-link debugger and...
    Jeremy Kramer
    last modified by Jeremy Kramer
  • Re: DAC not working on FRDM-K22F ver 2

    HI guys, I'm also having troubles to make the DAC works. I tried your previuos tips but unsuccessfully. I'm using kinetisstudio 3.0.2 and k22f. Could you help me?
    Julio Ruzicki
    last modified by Julio Ruzicki
  • KDS Problems with Windows 10 Anniversary Edition

    Customer has installed KDS3.2 and KSDK1.3 on new laptop with Win10 Anniversary Edition.   When he types File-->Import the widow does not populate files as shown below. Any suggestions or recommendations?
    Brad Stewart
    last modified by Brad Stewart
  • Error with CRC_GetBlockCRC function

    I'm trying to use the CRC component to check an SPI communication but by using the function CRC1_GetBlockCRC this way CRC1_GetBlockCRC(CRC1_TDeviceData, &RVG_SPIReadBuffer, RVG_SPIReadBufferSize*sizeof(uint8_t),...
    Nadia Jarray
    last modified by Nadia Jarray