• Summary of FRDM-K22F debug interface

    NXP Freedom K22F is an ultra-low-cost development platform for Kinetis K22 MCUs. This board is already widely used among NXP customers. http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-K22F   ...
    ZhangJennie
    last modified by ebiz_ws_prod
  • SD Card Bootloader :how to using SD card to update existing firmware on CodeWarriror or KDS

    This SD card bootloader demo offers to user a way how to using SD card to update existing firmware. The two project of attachment are the demo code create by CodeWarrior 10.6 and KDS 3.0 . The document of attachment...
    Alice_Yang
    last modified by ebiz_ws_prod
  • How to Create a C++ Project Using MQX RTOS for KSDK1.2

    Hi everybody,   this time you will find in the attached document the required settings to build a C++ project using KDS3.0 and MQX for KSDK1.2.   For information about creating a simple C MQX RTOS for KSDK...
    Carlos_Musich
    last modified by ebiz_ws_prod
  • Using FRDM-K64F with P&E and Segger OpenSDAv2 Firmware

    The FRDM-K64F board comes with the mbed CMSIS-DAP firmware installed by default. CMSIS-DAP can be used with KDS using OpenOCD. There are two alternative firmware files available for the FRDM-K64F (which runs OpenSDAv...
    Erich Styger
    last modified by ebiz_ws_prod
  • How to use printf() to print string to Console and UART in KDS2.0

    This document summarizes how to use printf() to print string to Console and UART in KDS2.0 .   Printing string to Console and UART both includes three conditions: Processor Expert project, KSDK project and bare...
    Alice_Yang
    last modified by ebiz_ws_prod
  • OpenOCD support for K22FN512 & K24FN256 in KDS

    Introduction  OpenOCD is the PC host application that is used by OpenSDAv2 (CMSIS-DAP application) for debugging. The standard installation of KDS does not include support for debugging the K22FN512 & K24FN2...
    martynhunt
    last modified by ebiz_ws_prod
  • Adding a new chip to Embsys Registers.

    Normally when debugging you need to know the status of your registers in the Embsys Registers section. Most of the time when a board or chip are just released you are not able to select them (because they're not avail...
    IvanRuiz
    last modified by IvanRuiz
  • New Kinetis Design Studio v3.2.0 available

    Greetings, a new release of Kinetis Design Studio (KDS) is available: the version v3.2.0!   The KDS v3.2.0 is an update with includes all existing updates to the v3.0.0 release. So instead downloading and insta...
    Erich Styger
    last modified by Diana Torres
  • KDS Debug Configurations (OpenOCD, P&E, Segger)

    NOTE: the screenshots below are for KDS V1.0.1-beta!   After creating a new debug configuration is simple: Select either 'GDB OpenOCD Debugging', 'GDB PEMicro Interface Debugging' or 'GDB SEGGER J-Link Debuggin...
    Erich Styger
    last modified by Diana Torres
  • kds_quick_start has ommision error.

    For the Windows version of SDK, I was not able to use the OpenSDA with CMSIS-DAP running on the FRDM-KL25Z.. The Quick Start guide Figure 12 shows the a blank field for "Other options". You must enter "-f kinetis.cf...
    Brad Stewart
    last modified by Diana Torres
  • Semihosting for Kinetis Design Studio

    The following link has the information how to enable semihosting inside Kinetis Design Studio:   Semihosting with Kinetis Design Studio | MCU on Eclipse
    Erich Styger
    last modified by Diana Torres
  • Tutorials using the Kinetis SDK with Kinetis Design Studio

    This is a list of tutorials about using the Kinetis SDK with either Kinetis Design Studio or Eclipse Kepler and the GNU ARM build tools. They use the FRDM-K64F board, but any other board/microcontroller supported by ...
    Erich Styger
    last modified by Diana Torres
  • Kinetis Design Studio V1.0.1 Beta Release Notes

    (NOTE: this document gets constantly updated with new information)   =========================================================================== Release Notes: Kinetis Design Studio (KDS) V1.0.1 Beta Date: 06-Ju...
    Erich Styger
    last modified by Diana Torres
  • Changing the ARM GNU Tool Chain in Kinetis Design Studio

    KDS V1.0.1 (beta) is using the GNU 4.8.0 toolchain, while the latest and greatest from ARM Inc. on launchpad is the 4.8.2 GCC ARM Embedded.   KDS V1.0.1 (beta) is using an older newlib nano which requires at l...
    Erich Styger
    last modified by Diana Torres
  • Kinetis Design Studio V1.1.0: Release Notes and News

    (NOTE: this document gets constantly updated with new information) =============================================================================== Release Notes and News: Kinetis Design Studio V1.1.0 Version Date: 05...
    Erich Styger
    last modified by Diana Torres
  • FRDM-K22F: Debugging with P&E OpenSDAv2.1 Firmware

    This document explains how you can debug the FRDM-K22F board with the P&E OpenSDAv2.1 Firmware and the Kinetis Design Studio V1.1.0.   Applicable to: OpenSDAv2.1 boards (FRDM-K22F for now) Kinetis Design S...
    Erich Styger
    last modified by Diana Torres
  • Toggling the FRDM-K64F RGB LED using interrupts in Kinetis Design Studio (KDS)

      Hello Freedom community users Bheema has posted on the Element14 community a very clear tutorial (accessible following the link below) to create from scratch a basic project example for the FRDM-K64 with Kine...
    Gregory Camuzat
    last modified by Diana Torres
  • Quickstart Guide for KDS v1.0.1 beta

    NOTE: with the release of KDS V1.1.0 this quickstart is depreciated!   Note that this quickstart guide is an update/newer version than the one installed by the installer.
    Erich Styger
    last modified by Diana Torres
  • Kinetis Design Studio V1.1.1 Released!

    Greetings, A new release V1.1.1 of KDS is available from the Download tab on http://www.freescale.com/kds V1.1.1 is a full release, and it is recommended to use this new release going forward. V1.1.1 supports Window...
    Erich Styger
    last modified by Diana Torres
  • Uninstalling KDS: "Error opening installation log file."

    In case you are running into this error while trying to uninstall KDS on Windows (I had it with KDS V1.1.0, but it might apply to other versions too):   "Error opening installation log file. Verify that the speci...
    Erich Styger
    last modified by Diana Torres