•   MCUXpresso Software and Tools – New Releases Available

    NXP has released the newest versions of MCUXpresso SDK, IDE, Configuration Tools, and Secure Provisioning Tool. In addition to new product support, you will find these updates and enhanced features in the new rel...
    Devonna Dorton
    created by Devonna Dorton
  • MCUXpresso IDE v11.2.0 Now Available

    We are pleased to announce that MCUXpresso IDE v11.2.0 (build 4120) is now available. This is a major new version of the IDE, and contains new features, enhancements and bug fixes over the previous versions, incl...
  • Share your FreeMASTER dashboard designs, get a free board!

    Share your FreeMASTER dashboard designs, get a board!   Calling all FreeMASTER fans!   Are you an experienced FreeMASTER user who has already created custom dashboards, or are you an HTML/Javascript coder wh...
    Brendon Slade
    last modified by Brendon Slade
  • New/updated MCUXpresso tool training videos available

    Thanks to all of you that joined the MCUXpresso training we've been providing over the last few weeks and months via our webinars. We've also been adding more training videos covering some of the items from the webina...
    Brendon Slade
    last modified by Brendon Slade
  • MCUXpresso IDE v11.1.1 Now Available

    We are pleased to announce that MCUXpresso IDE v11.1.1 (build 3241) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v11.1.0, and we recommend that all existing ...
  • LPCScrypt v2.1.1 is now available

    LPCScrypt v2.1.1 | NXP  is now available. This release incorporates the latest versions of LPC-Link2 firmware for both CMSIS-DAP and also SEGGER J-Link.   LPCScrypt is a command-line based, fast flash (inte...
  • MCUXpresso IDE v11.1.0 SDK Handling Hotfix

    An issue has been identified in MCUXpresso IDE v11.1.0 with SDK 2.7 that in certain circumstances can cause the IDE to issue one or more erroneous duplicate file error popups when importing SDK examples or creati...
  • Modifying the latest Adafruit 2.8" LCD for SDK graphics examples

    Our MCUXpresso SDK is expanding to include more and more graphics examples, including LittleVGL and emWIN support for SPI-based LCDs. The examples we provide can be ported to different controllers, but are based/...
    Brendon Slade
    last modified by Brendon Slade
  • MCUXpresso IDE v11.1.0 - Board SDK Creator

    NXP provides MCUXpresso SDKs that are configured for use with our standard evaluation boards. These can be used when carrying out your initial evaluation of our MCUs and early development work. However, in most cases ...
  • MCUXpresso Ecosystem Enhancements

    NXP's MCUXpresso Software and Tools has expanded to include a new Secure Provisioning Tool, support for integrated third software solutions and has major improvements in the user experience for software selection. Thi...
    Devonna Dorton
    created by Devonna Dorton
  • New Secure Provisioning Tool and IDE, SDK, Config Tools Releases Now Available

    New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available, along with a new Secure Provisioning Tool. Please see below to learn more about these updates updates and enhanced features in the new re...
    Megan Hansen
    last modified by Megan Hansen
  • MCUXpresso IDE v11.1.0 Now Available

    We are pleased to announce that MCUXpresso IDE v11.1.0 (build 3209) is now available. This is a major new version of the IDE, and contains many new features and enhancements over the previous MCUXpresso IDE v11.0...
  • Using MCUXpresso IDE on macOS 10.15 (Catalina)

    MCUXpresso IDE is currently supported on macOS 10.12 to 10.14.   In macOS 10.15 (Catalina), Apple have introduced a new additional "signing" mechanism for software that is download outside of the Apple App Store...
  • MCUXpresso IDE v11.0.1 LPC55xx Debug Hotfix

    Background  As part of the MCUXpresso IDE v11.0.1 release, we had to make some major changes to our LinkServer debugging mechanism to support the latest silicon revision of the LPC55xx family of devices (revisio...
  • MCUXpresso IDE v11.0.1 Now Available

    We are pleased to announce that MCUXpresso IDE v11.0.1 (build 2563) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v11.0.0 release, and we recommend that all e...
  • Over 100,000 Downloads of the MCUXpresso SDK

    In March of 2017, NXP released the debut version of the MCUXpresso SDK along with an IDE and set of Config Tools under the same MCUXpresso name.  Since that time we have seen an amazing response from developers d...
    Clark Jarvis
    last modified by Clark Jarvis
  • New MCUXpresso Software Releases Now Available

    New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available. In addition to new product support, you will find these updates and enhanced features in the new releases:   MCUXpresso SDK v2.6.0 ...
    Miguel Hernandez
    created by Miguel Hernandez
  • MCUXpresso IDE v11.0.0 Now Available

    We are pleased to announce that MCUXpresso IDE v11.0.0 (build 2516) is now available.   This is a major new version of the IDE, and contains many new features and enhancements over the previous MCUXpresso IDE v10...
  • MCUXpresso IDE v10.3.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.1 (build 2233) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.3.0 release, and we recommend that all e...
  • MCUXpresso Software and Tools - New Releases Available

    NXP has released the newest versions of MCUXpresso SDK, IDE, and configuration tools. In addition to new product support, you will find these updates and enhanced features in the new releases:   MCUXpresso SDK v...
    Megan Hansen
    created by Megan Hansen