• kernel panic when booting the s32v234sbc

    Sorry, i'm not good at using English. I have a s32v234sbc package and i am trying to boot it with yocto image. (* VisionSDK_S32V2_RTM_1_5_0_img_yocto.tar.gz) Used image is yocto origianl image(Image, fsl-s32v2...
    namsu kang
    last modified by namsu kang
  • How to add a new camera driver for toolbox

    I am trying to using a different camera other than the default one. Can you provide the instructions so that I can add its ISP driver in? For example, GMSL Camera with OV10635 & Maxim Deserilaizer .....
    Jim Duan
    last modified by Jim Duan
  • where can I find this SW Activation Code

    when I installed the VSDK, the NXP Compiler for APU must be installed,So,where can I find the  Activation Code?
    yongchao yang
    last modified by yongchao yang
  • How to get and use opengl drivers for S32V234  SBC

    Dear All,   I am new to this community and using NXP S32V234 first time.   I was searching for a good processor with integrated GPU and Display Controller unit and I found NXP S32V234 vision processor. I a...
    RAJNEESH Saini
    last modified by RAJNEESH Saini
  • Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

    Dears   What machine is fsl-image-ubuntu currently compatible with? Where can I see a list of compatible machines? Will fsl-image-ubuntu be compatible with s32v234sbc in the future? When will it be supported? &#...
    Shuo Feng
    last modified by Shuo Feng
  • point cloud library @ yocto S32V234

    Dears   Is there recipes for "Point Cloud Library" for yocto image build? Has anyone used PCL (point cloud library) on S32V234? Can APEX accelerate PCL? Does NXP have corresponding technical support?   Thank...
    Shuo Feng
    last modified by Shuo Feng
  • point cloud library @ yocto S32V234

    Dears   Is there recipes for "Point Cloud Library" for yocto image build? Has anyone used PCL (point cloud library) on S32V234? Can APEX accelerate PCL? Does NXP have corresponding technical support?   Thank...
    Shuo Feng
    last modified by Shuo Feng
  • point cloud library @ yocto S32V234

    Dears   Is there recipes for "Point Cloud Library" for yocto image build? Has anyone used PCL (point cloud library) on S32V234? Can APEX accelerate PCL? Does NXP have corresponding technical support?   Thank...
    Shuo Feng
    last modified by Shuo Feng
  • Invalid Pointer error when running CNN example from NXPVT on S32V234SBC

    Hello,   I am currently trying to get a CNN running on the S32V234SBC.    I am using the following setup: Windows10 Matlab R2019b NXP Vision Toolbox 1.2.0 NXP Vision SDK 1.4.0 NXP Compiler for AP...
    Franz Huber
    last modified by Franz Huber
  • How to use the CAN Bus on S32V234

    Hi, I want to use the build in CAN Bus of the S32V234 to communicate with an Teensy 3.2. For debugging, I've connected a PeakCan USB dongle to the boards CAN0 to send and recieve messages. I connected my PC via Putt...
    Sebastian Kruse
    last modified by Sebastian Kruse
  • where can I find the SBC-S32V Demo's Schemtic

    I can find S32V-R3V Schemtic,but I think this is not the SBC-S32V Demo's Schemtic thanks!
    yongchao yang
    last modified by yongchao yang
  • Need information on connecting S32V234-EVB2 to other MCU using UART

    Hello,   We wanted to connect NXP-S9KEA8P44M48SF0 to S32V234-EVB2 board using UART. Please do share details about connecting.   We understand that, S32v234-Evb2 has serial to USB converter chip ( tty...
    Prem J
    last modified by Prem J
  • S32V234 how to do communication between cortex A53 and Cortex M4

    Hi , Have you find a solution for communicating with A53 and M4?   I have a subject to use M4 for real time control which receive information from image process result on A53 then run rea...
    askariz askariz
    last modified by askariz askariz
  • Reboot issue for NXP S32V234 EVB

    Hi Support team,   We are using S32V234-EVB2 evaluation board for my custom work. we are facing an issue with S32V234 SD card boot. During our testing NXP board suddenly started rebooting co...
    Pratik Parvati
    last modified by Pratik Parvati
  • Need Help for  a  installation of libGLESv3 lib on S32V234EVB board

    Hello , We are using S32V234-EVB2- SC29288, and wanted to set up libGLESv3 . As of now we are using libGLESv2.so files for running OPENGL qt base application for displaying purpose. But our  requirment is libGL...
    vaibhav nanoti
    last modified by vaibhav nanoti
  • Develop camera with S32Design integrated environment

     Is there a way to get data directly from CSI?I write my own graphic algorithm, and I write my own Framebuffer output.I just want to get the image data a little bit easier Thanks
    国栋 范
    last modified by 国栋 范
  • How to get data source directly from CSI?Not through the CSI-SRAM-FDMA-DDR approach

    Isp_csi_dcu routine development, using different types of cameras, how can more directly get the camera information?
    国栋 范
    last modified by 国栋 范
  • need support for S32V234 EVB2 linux kernel sources code set up on our PC(locally)

    Hello, We are using S32V234-EVB2- SC29288, and wanted to set up LINUX KERNEL 4.19. version locally. Please do provide documents to set up kernel source code base locally. i.e complete kernel sources, including all d...
    vaibhav nanoti
    last modified by vaibhav nanoti
  • Vision Toolbox Setup Problems

    Hi, I'm using the S32V234-SBC Board with the goal to run Matlab Code on it. I've followed the instructions given in the PDF 'Vision Toolbox Quick Start' https://www.nxp.com/docs/en/quick-reference-guide/Vis...
    Sebastian Kruse
    last modified by Sebastian Kruse
  • 2019b

    Does this toolbox support Matlab 2019b? 
    Jim Duan
    last modified by Jim Duan