• RDK-S32R274 Demo controller application not starting after installation

    We have installed the RDK-S32R274 Demo controller application on a Windows 10 laptop. When running the application after installation nothing happens, i.e. no application window appears. In task manager we see that th...
    Lars van Meurs
    last modified by Lars van Meurs
  • RRU SPT issues

    The result are different between the NXP simulator and the embedded system   Here are the two results for the first FFT16 with windowing:   From simulator:   0xa000; 0xfff31c +i 0x000dd6 0xa001; 0x0000a...
    Moez Selmi
    last modified by Moez Selmi
  • RRU SPT issues

    The result are different between the NXP simulator and the embedded system   Here are the two results for the first FFT16 with windowing:   From simulator:   0xa000; 0xfff31c +i 0x000dd6 0xa001; 0x0000a...
    Moez Selmi
    last modified by Moez Selmi
  • FS32R274KBK2MMM,和FS32R274KCK2MMM的区别

     雷达芯片FS32R274KBK2MMM,和FS32R274KCK2MMM,之间有什么区别吗?可以替换吗?这个CSE代表什么含义?请帮忙告知一下,谢谢了。  
    星章 宣
    last modified by 星章 宣
  • Release Announcement: Model-Based Design Toolbox for SPT version 1.3.0

          Product Release Announcement Automotive Microcontrollers and Processors Model-Based Design Toolbox for SPT - 1.3.0       Austin, Texas, USA November 11th, 2019   ...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • RDK-S32S274 ADC data stream

    rdk-s32r274 ADC Raw data stream: I am using the Demo Controller software for the RDK. When I switch from Peaks to ADC samples in Output stream drop-down I don't get any response. Can you please help on how can we...
    Rahul Jaiswal
    last modified by Rahul Jaiswal
  • Can we capture the two dimensional FMCW raw data by using RDK-S32R274?

    can we capture the raw FMCW data, so one can apply to his own algorithm in Matlab to do the range and Doppler processing to perform the range doppler imaging?#rdk-s32R274#radar signal processing
    Neeraj Pandey
    last modified by Neeraj Pandey
  • RDK-S32R274: S32R27 kit to do range-Doppler Imaging

    I want to purchase RDK-S32R274: S32R27 for varying my simulation-based model results by capturing measurement data in real scenarios for the automotive radar target and perform range doppler imaging for short-range ra...
    Neeraj Pandey
    last modified by Neeraj Pandey
  • 1024 FFT for SPT simulation issues with model base design toolbox 

     I tried to simulate 1024 FFT using model base design toolbox.     The twiddle factor was generated by following code NFFT =1024   for mm = 0:1:(NFFT-1) theta = (-2*pi*mm*1/NFFT); twiddle...
    Morris Li
    last modified by Morris Li
  • CACFAR IN S32R274 RSDK1.2.1

    S32R274,     I want to ask a question about cacfar in demo 1.2.1,in my understanding, traditional cacfar algorithm is using the sum of neighbor reference bin,and averaging the sum as the noise threshold,an...
    Liu Xianyong
    last modified by Liu Xianyong
  •           TDA3619/N2 Couldn't find a Datasheet about this parts

    Good day everybody,   i don't find a datasheet about this parts could somebody help me out thank
    Steffen Thelen
    last modified by Steffen Thelen
  • ADC data acquisition in s32r274

    Hi Guys, I'm using OneRF_4Antennas_demo_s32r274, I'm able to get ADC dumps for the last two chirps and also range data.    After plotting 1d FFT values from those two chirps data, it is foun...
    Chidvilas Y
    last modified by Chidvilas Y
  • 3 TXs running at the same time

    As far as I know, in the Radar SDK, the available demos can only run 1 TX. I am learning with the DCC development kit. I want to have 3 TXs running at the same time. How can I modify the code? Is there any relevant in...
    Jane Yu
    last modified by Jane Yu
  • RSDK1.2.0 cann't work

    I am using RSDK1.2.0 After I downloaded the program The radar completes the parameter configuration from the tftp server  Tef8102 initialization status is successful and the SPT initialization stat...
    Longfei Wang
    last modified by Longfei Wang
  • I face the problem about the licence

    I face the problem about the licence even though I did the installation as requirement. I install the matlab 2018a.   (1) Firstly, I download the package from the Release Announcement: Model-Based Des...
    梦杰 张
    last modified by 梦杰 张
  • S32R274  Log2 operation

      What is the principle of adding a constant 22?
    Longfei Wang
    last modified by Longfei Wang
  • Release Announcement: Model-Based Design Toolbox for SPT 2.0/2.5/2.8 version 1.2.0

            Product Release Announcement Automotive Microcontrollers and Processors Model-Based Design Toolbox for SPT - 1.2.0             Austin, Texas,...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Do S32RXXX MCU have Sleep or Standby mode?

    Now we want use S32RXX+TEF810X in our Radar Level meter project. as Radar meter can only operating in low power consumption mode. So if S32RXXX MCU have sleep or standby mode, which can make total power consumption down?
    Samuel Guangzhu LI
    last modified by Samuel Guangzhu LI
  • S32R27 Reference Design Kit

    I am planning to buy "S32R27  Design Kit " how to applicate or tell me a way what i should do. thanks a lot
    yong zhang
    last modified by yong zhang
  • How to use the scalar product command scp_mex() in Matlab (Radar SPT core)

    I’m trying to get familiar with the SPT core and like to use the scalar product command. The goal is to perform 8 multiply operations and compute the sum (don’t care about the Im() parts, set to 0). ...
    Andreas Schibilla
    last modified by Andreas Schibilla