• RSDK1.2.0 cann't work

    I am using RSDK1.2.0 After I downloaded the program The radar completes the parameter configuration from the tftp server  Tef8102 initialization status is successful and the SPT initialization stat...
    Longfei Wang
    last modified by Longfei Wang
  • I face the problem about the licence

    I face the problem about the licence even though I did the installation as requirement. I install the matlab 2018a.   (1) Firstly, I download the package from the Release Announcement: Model-Based Des...
    梦杰 张
    last modified by 梦杰 张
  • S32R274  Log2 operation

      What is the principle of adding a constant 22?
    Longfei Wang
    last modified by Longfei Wang
  • Do S32RXXX MCU have Sleep or Standby mode?

    Now we want use S32RXX+TEF810X in our Radar Level meter project. as Radar meter can only operating in low power consumption mode. So if S32RXXX MCU have sleep or standby mode, which can make total power consumption down?
    Samuel Guangzhu LI
    last modified by Samuel Guangzhu LI
  • S32R27 Reference Design Kit

    I am planning to buy "S32R27  Design Kit " how to applicate or tell me a way what i should do. thanks a lot
    yong zhang
    last modified by yong zhang
  • How to use the scalar product command scp_mex() in Matlab (Radar SPT core)

    I’m trying to get familiar with the SPT core and like to use the scalar product command. The goal is to perform 8 multiply operations and compute the sum (don’t care about the Im() parts, set to 0). ...
    Andreas Schibilla
    last modified by Andreas Schibilla
  • Further details of the SCP command of the SPT 2.0 core

    I'm trying to get as much information from the Reference manual of the S32R274, but the following points are still unclear: Does the scalar product SCP command (8 coefficientc case ) "dst_addr" support unaligned addr...
    Andreas Schibilla
    last modified by Andreas Schibilla
  • How to activated the license in matlab 2018b

    Did anybody activated the model-based design toolbox in matlab 2018b? I have tried many times ,but failed 
    zhou ke
    last modified by zhou ke
  • register Model-Based Design Toolbox

    Hi I need download Model-Based Design Toolbox for SPT ,i should register first,so i need Registration Code Thanks
    zhai rui
    last modified by zhai rui
  • Can't download Model-Based Design Toolbox for SPT 2.0/2.5

    Hi I want download Model-Based Design Toolbox for SPT ,and it shows error message , i submit the problem but i can't find theToolbox in product list    Release Announcement: Model-...
    zhai rui
    last modified by zhai rui
  • IS there any another debugger to debug SPT ?

    Hi,     I do not have Lauterbach debugger can I use  PE Micro Multilink Universal for debugging SPT instructions or view SPT memories, modify memories dump contents? If Yes then, please tell m...
    Ankush Sangwan
    last modified by Ankush Sangwan
  • S32R274

    Hi,   I want to collect ADC samples for the radar sensor. How to configure s32r274 to receive chirp acquisition done interrupt to the Z7 core? Such that I can memcpy the adc buffer into a different bu...
    Chidvilas Y
    last modified by Chidvilas Y
  • how to use S32R274 UART

    hello, I have a doubt regarding S32R274 daughter card can we use UART without connecting the daughter card with EVB     If yes then Can you tell me how to set it up? or can you share any documen...
    Ankush Sangwan
    last modified by Ankush Sangwan
  • What is the latest version of the Radar SDK?

    What is the latest version of the Radar SDK? Is there a newer version than SW32R37-RSDK-RTM-1.1.1? Thank you!
    Jane Yu
    last modified by Jane Yu
  • S32R274   IC5000 code overlapping

    I encountered the following problem when I used the IC5000 to write ELF file to S32R274. The file is  generated by S32DS.  I want to ask if other people have encountered this problem. Can you help solv...
    wanglongfei lf
    last modified by wanglongfei lf
  • S32R2: Software Initialization Guide

    Hi All, Could any body please provide me the " Software Initialization and Optimization" or Guide documents for S32R274. i mean where I can get the idea about the startup sequence of core or how the core are wo...
    DSPIC MIC
    created by DSPIC MIC
  • CAN TX in S32R274

    CAN TX in S32R274 I USE THE CAN at loopback mode ,BUT    always wait here     while (CAN_1.MCR.B.FRZACK & CAN_1.MCR.B.NOTRDY) {} /* Wait to clear */        ...
    anson an
    last modified by anson an
  • How to run 1RF 4Antennas Demo

    Hi, I downloaded the Radar SDK and read RSDK_User_Manual. I am using the DCC Development kit, I want to run 1RF 4Antennas Demo, but I can't compile this project. What do I do? Is there a more detailed expla...
    Jane Yu
    last modified by Jane Yu
  • 77G Radar

    Hi All,     I'd want to know how should I do can get the 77G Radar EVM board ?     And if we want to development it,do you have any suggestion ?
    1807599346@qq.com
    last modified by 1807599346@qq.com
  • creat my own command list

    hallo, MCU S32R274 is used in my application.  I am starting looking into how to program the SPT module in S32DS.  I am totally new here and struggling with the command list.  I could not figure out h...
    Jie Zhang
    last modified by Jie Zhang