• Freemaster with MPC5744P: Can not detect the board information ! The communication will be paused. Error code: 0x80000101 (Response timeout)

    Hi NXP team,   I use hardware "DEVKIT-MPC5744P REV.E.", My Aim to use software Model-Based Design Tools and  Freemaster. Firstly, I use SOFTWARE INTEGRATION GUIDE (SWIG) document and I run a very simple c...
    eCar German
    last modified by eCar German
  • How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for MPC5744P v2.0)

    In case you need to export the generated code to S32 Design Studio for PA IDE, now there is an easy way. No more painful job of reconstruction the project manually and setting all sort of compiler flags. Here is what ...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Motor Control Class: Lecture 5 - Hall Sensors

    In this fifth lecture of the motor control course we discuss about how can we read the hall sensors to obtain the rotor position in order to know how to apply the correct voltage sequence to the motor phases...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • S32K144 board detection problem

    Hello, recently, I have bought S32k144 EVB and I have watched tutorials how to control it and etc, but the thing is that I cannot establish communication between this board and my laptop. When I turn on Freemaster pr...
    Tautvydas Karvelis
    last modified by Tautvydas Karvelis
  • Module 5: V/F Scalar Control

        INTRODUCTION   In this module of the 3-Phase PMSM Control Workshop with NXP's Model-Based Design Toolbox , we are going to spin the PMSM for the first time with S32K and...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Using Model-Based Design Toolbox for S9S12VR64.

    Dear MBDT Community, I am writing just to inquire whether if I am able to use the NXP's Model-Based Design Toolbox to model the S9S12VR64/MC9S12VR-family MCUs in my MATLAB/Simulink environment? Best regards, David
    David HEE
    last modified by David HEE
  • MPC5744p RevE communication problem

    Hi NXP team and fellow members,   I have recently ordered MPC5744P DevKit and received the Rev E DevKit. I tried to compile and download the code from Simulink model-based toolbox example by following the quick s...
    SHAO Jianbo
    last modified by SHAO Jianbo
  • MPC5744P RevE CCP communication error

    Hi NXP team and fellow members,   I have recently ordered MPC5744P DevKit and received the Rev E DevKit. I tried to compile and download the code from Simulink model-based toolbox example by following the quick ...
    aung myat
    last modified by aung myat
  • where is 'SCB_SCR' ?

    Hi ,    Can't found 'SCB_SCR'  in <S32K-RM.pdf>. Who can give help ?     in S32DS, you can configure 'Sleep on Exit Value' with 'power_manager' component.
    王 从伟
    last modified by 王 从伟
  • NXP BGA6130 PA device design s parameter s2p file

    Dear Sir,   I am Sagar Mistry from the system level Solution Pvt Ltd(India).   I required your technical help and guidance regarding the simulation file S parameter s2P file of NXP BGA6130 PA for the RF si...
    Sagar Mistry
    last modified by Sagar Mistry
  • "powerpc-eabivle-gcc.exe: fatal error: cannot specify -o with -c, -S or -E with multiple files" Error

    Hello,   I have actually imported a generated code from Matlab to the S32 Design software by following the below form instructions: How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for...
    Erfan Bashar
    last modified by Erfan Bashar
  • HotFix: MBD Toolbox rev2.0.0 for MPC5744P (Panther)

    HotFix_1: Missing lsp.h file    Problem: Model compilation terminates with the following error: SWLIBS_Defines.h:132:17: fatal error: lsp.h: No such file or directory #include <lsp.h>   ...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • How to use CAN Pack in Simulink with NXP MBDT ?

    我也有相同的问题,并想到了一个解决办法。不知道你是否已经解决。
    Tian LiJun
    last modified by Tian LiJun
  • Module 1: Environment Setup

    INTRODUCTION In this module of the 3-Phase PMSM Workshop, the focus is on the hardware and software setups that are going to be used throughout this workshop to implement and test a complete 3-phase Permanent Mag...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Module 6: Current Sensing (Part 1/2)

          INTRODUCTION   In this module of the 3-Phase PMSM Control Workshop with NXP's Model-Based Design Toolbox , we are going to implement and test the most critical part of the...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • HotFix: MBD Toolbox 3.0.0 for MPC57xx

    HotFix_1: eTimer pins initialization not working properly, added support for ADC internal temperature sensor.   Problem: When using other port than PORTA on eTimer input channels, the initialization was no...
    Marius-lucian Andrei
    last modified by Marius-lucian Andrei
  • Module 7: Torque Control

    EV Powertrain  source: carmagazine.co.uk      INTRODUCTION   Nowadays, are we witnessing the start of a global revolution within the automotive industry, where more and more car manufac...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • Please provide support for Matlab 2016a

    Thanks you folks at nxp providing such great tool. We would like to log a formal request to have this tool to support matlab 2016a since our toolchain has not been updated for stability reason.   @Razvan Ionescu...
    guoliangzhang
    last modified by guoliangzhang
  • HotFix: MBD Toolbox S32K v4.1.0

    Cumulative patch:   As you know, we're only giving out cumulative patches for a while now - they come in the form of self-extracting zips and contain all the patches, up-to-date. A user can install at any po...
  • Module 10: Sensorless Speed Control

        INTRODUCTION   In this article we are going to discuss a couple of aspects that you should expect when building complex applications like Motor Control Speed Control of PMSM based on Sensorless meth...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa