• What's the difference between SIENF and IENF

    I have a GPIO interrupt working on an LCP11Uxx. There are two registers SIENF and IENF that seem to do the same thing. They both set a bit in IENF. The datasheet says writing to IENF sets an interrupt, and writing to ...
    Lydia Johnson
    last modified by Lydia Johnson
  • CAN FD max data rate

    What's the max CANFD databandrate?  I can't find the define in the User manual and Data sheet; the demo give max 4M; when i try to set to 5M, it seems someting error;
    黎明 孟
    last modified by 黎明 孟
  • LPCXpresso845MAX FreeRTOS

    Hello community,   I am currently using the above board based on LPC845 with Cortex M0+ core, I was wondering if there is an example project of basic FreeRTOS for this microcontroller such as the one in Debug fr...
    Eddie Vazquez
    last modified by Eddie Vazquez
  • Entering ISP mode from user code with LPC11U68JBD48

    I'm using LPC11U68JBD48 microprocessor. I have a switch which toggles PIO0_1 pin. I can go into the ISP mode by pressing the switch and by applying power to the board (Resetting board).   Now I have my applicati...
    David Yun
    last modified by David Yun
  • LPCUSBSIO

    Hello,   i would like to extend the functionality of the given library/firmware by enabling i2c slave mode of the MCU. Therefore, it would be helpful to have the source code of the firmware. I'm working on a LPC...
  • LPC546xx minimal clock speed when using USB1 in full speed

    We are using the USB1 (high speed USB peripheral) from the LPC54606, but we are using it in Full Speed mode (which is a lower speed than high speed). The reference manual mentions that the system clock should be at l...
    Arno Moonen
    last modified by Arno Moonen
  • LPC1788 and SDRAM 512Mbit structured as 4 Meg x 32 bits x 4 banks

    I'm using an external SDRAM connected to the LPC1788FDB208 microcontroller. As SDRAM I chose (and unfortunately already bought many pieces) the IS42S32160F-7TLI model ( http://www.issi.com/WW/pdf/42-45R-S-32160F....
    Nico Aprile
    last modified by Nico Aprile
  • How to Program LPC-link2 in CMSIS or J-Link mode

    Hi everybody   I'm working with LPC microcontrollers and using LPC-Link2 board to work with, I would like to share a tutorial about how to change LPC-Link2 board between CMSIS and J-Link mode, I hope this could ...
    Oscar Niño
    last modified by Oscar Niño
  • P&E Micro Multilink Universal Debug ISsue for LPC4367

    I am using P&E Micro Multilink Universal for debugging my development board. I am using LPC4367. It was ok till the time i was using LPC link3 which is there in the evaluation board OM13088.  Since our new d...
    Gaurav More
    last modified by Gaurav More
  • LPC546xx mismatch between SDK and UM10912 static and dynamic memory region

    Hi NXP community   I am using LPC546xx and have found a mismatch between the SDK 2.5.0 and User Manual UM10912 concerning static and dynamic memory regions depending on Cip Select:   Static Memory Chip Sel...
    Daniel Gull
    last modified by Daniel Gull
  • find demo binaries for LPC54114 audio and voice recognition kit

    Hi everyone,   I just ordered a LPC54114 audio and voice recognition kit. But it seems the pre-loaded software with the kit does not have audio and voice recognition function.   From NXP website, I downl...
    xiaowei zhang
    last modified by xiaowei zhang
  • LPC845 sampling time

    Good morning, I'm working with an LPC845 microcontroller. For a specific application I need to know how many TAD implies the sampling process of the A/D converter over the entire conversion time. I have searched on ...
    Pasquale Barrega
    last modified by Pasquale Barrega
  • 2 channel HSADC (40 Msps) and DMA

    Hi all   we need the LPC4370 for sampling 2 ADC channels with 20 Msps each (not continous but 1000 samples per channel in a row). This works with the Audio PLL at 80 MHz very well. We are able to acquire 1000 sa...
    lorenz.aebi@helbling.ch
    last modified by lorenz.aebi@helbling.ch
  • GPIO mode setting for USB in LPC4357

    Hi, We are using LPC4357 processor. Pin 116 (or P2_1) is used as USB enable for USB1. We are using UBS 1 as mass storage host. Since P2_1 is also GPIO 5 bit 1 we are configuring through the control register SFSP2_1 (...
    S S
    last modified by S S
  • How to send and receive data via usb

    Content originally posted in LPCWare by sadeghjun on Tue Sep 30 07:38:14 MST 2014 Hi everybody. I want to send and receive data from PC to My board (MCB1700) and i need about 2Mbps speed, but i have some problem: [col...
    lpcware
    last modified by lpcware
  • Drive i2c device with LPC8N04

    Can I talk to a peripheral device using i2c with the LPC8N04 when it's powered by NFC? May I power a peripheral device from the LPC8N04? What is the output voltage and current supplied by the LPC8N04 when powered vi...
    pmg
    created by pmg
  • Help with using libusb or vcom to receive bulk data

    Hi! I am working on a project that requires bulk data transfer. I was trying to use the given examples to learn how to use the usbd_rom_cdc_vcom and usbd_rom_libusb examples, but am not able to figure out how to ...
    Visweshwar Srinivasan
    last modified by Visweshwar Srinivasan
  • MCUXpresso IDE v10.3.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.1 (build 2233) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.3.0 release, and we recommend that all e...
  • LPCxpresso 54628 I2C slave stop condition issue

    Hi All,  I'm using a LPCxpresso 54628 and am running the I2C interrupt driven slave example code. My issue is that, while I see all my data come in on a ReceiveEvent, the I2C callback routine never hits the...
    Mike Spenard
    last modified by Mike Spenard
  • I2C library config for LPC1769

    Hi I'm making a project with an LPC1769. I'm trying to make a pulsioximeter using a MAX30100. This device is an optical sensor with an adc that transmit the data that it sense using I2C (and much more b...
    Javier Nakama
    last modified by Javier Nakama