• LPCxxxx flash programmer 'mxli' with Raspberry Pi support

    Hello Guys,   I'd like to announce the update of my open-source command-line flash programmer 'mxli' . I know, that many programmers don't appreciate using command-line tools these days, so skip this, if you're ...
    Marc Prager
    last modified by Marc Prager
  • LPCXpresso 54608 connection issue

    When trying to debug using link 2 probe (link server) this error occurs  Error in final launch sequence Failed to execute MI command: -target-select extended-remote | crt_emu_cm_redlink -msg-port=54569 -g -mi -2 ...
    yash bohra
    last modified by yash bohra
  • two sets of API/driver functions ... there's the kind in the SDK, yet another that comes preloaded with MCUXpresso... why?

    Hello,      I was wondering if anyone could shed some light on this issue.      I am working with the LPC54114 board, a.k.a the OM13089 board, but I am assuming this issue exi...
    Takis Zourntos
    last modified by Takis Zourntos
  • LPC8xx.h

    We are using the LPC804 and IAR.  The LPC8xx.h header file from the example projects does not include defines for the CTIMER peripheral.   I found an LPC804.h file but is also not complete.   Thanks &...
    Richard Soennichsen
    last modified by Richard Soennichsen
  • FTDI FT800 LCD TFT display + LPC1769 - some problems with graphic commands

    Content originally posted in LPCWare by teslabox on Wed May 11 13:07:22 MST 2016 Hi guys, I am dealing with FT800 FTDI LCD TFT 5 inches display. I run it via SPI0/SSP0 at 10 MHz with my LPCXpresso LPC1769 Rev. C and ...
    lpcware
    last modified by lpcware
  • LPCXpresso 54608 not recognized

    I'm using LPC 54608 board for the first time, Initially out of the box demo was working fine, and also only for once it worked as mass stoarge device using Full speed port then as per instructions i deleted the firmwa...
    yash bohra
    last modified by yash bohra
  • Mistake in LPC804 Users manual v1.3

    Hello there,   I found small mistake in LPC804 Users manual v1.3 - 12.July 2018 (https://www.nxp.com/webapp/Download?colCode=UM11065 )   On page 52, fig 6 - signal "main_clk" from MAINCLKSEL regi...
    pepoja
    last modified by pepoja
  • LPC54608 Usart Interrupt Example

    Hello, I have a question in relation about the Usart Interrupt LPC54608 example, that I re-write down here:     First question: Why I collect data from the usart also if I have an error (kUSART_RxError) ...
    Marco Pazzi
    last modified by Marco Pazzi
  • LPC1788 and SDRAM 512Mbit structured as 4 Meg x 32 bits x 4 banks

    I'm using an external SDRAM connected to the LPC1788FDB208 microcontroller. As SDRAM I chose (and unfortunately already bought many pieces) the IS42S32160F-7TLI model ( http://www.issi.com/WW/pdf/42-45R-S-32160F....
    Nico Aprile
    last modified by Nico Aprile
  • lpc3240 download to nandflash

    lpc 3240 , how can I download .hex to nandflash ? (No OS ,standalone),thanks a lot
    gan zhang
    last modified by gan zhang
  • FR_NO_FILESYSTEM error on FAFTS working SD card FAT32 with MCI interface on LPC1788

    Content originally posted in LPCWare by sipel_tp on Thu Aug 22 08:54:00 MST 2013 Hello everybody, I've tried to inicialize a SD card using the elm-chan.org FATFS library with a LPC1788 and the MCI interface. I man...
    lpcware
    last modified by lpcware
  • vcom_connected() == FALSE Ubuntu Linux 14.04 - Use USB for Serial Monitor

    Content originally posted in LPCWare by a_bet on Fri Mar 18 07:14:02 MST 2016 Hi everyone, I'm new to lpcxpresso and to the arm world. I've bought a lpcxpresso 43s37 board, which is doing fine with all the lpcopen exa...
    lpcware
    last modified by lpcware
  • Low Pin count uC with LF Osc?

    Does the LPC line include a model with low pin counts and a LF osc (with XTAL pins, for 32.768 KHz xtal)?   I need a real RTC....     Thanks   Rich
    Richard Soennichsen
    last modified by Richard Soennichsen
  • LPC845-BRK example ADC: Mex-file differs from code

    Well, I just started to explore the ADC example of  https://www.nxp.com/downloads/en/software/LPC845BRK_Examples.zip (LPC845_ADC_LDR). The function BOARD_InitPins() in pin_mux.c contains: As you can see in th...
    12345 67890
    last modified by 12345 67890
  • Error when reselect debugging

    I have the same error on 2 different machines (both Kubuntu 18.04 64 bit, MCUXPresso 10.3.1 and SDK for LPC845 Version 2.5.0: I abort debugging by clicking the red symbol in the upper menu. Then (doing some other thi...
    12345 67890
    last modified by 12345 67890
  • UDA1380 I2S - registers coniguration

    Content originally posted in LPCWare by paavo91 on Wed Nov 26 04:09:25 MST 2014 Hi everyone! I have lpc4088 and UDA1380 codec and want to initiate some audio. Could anyone tell me which registers I need to set to tra...
    lpcware
    last modified by lpcware
  • Getting start with LPCXpresso54608 & emWin Graphics;

    This tutorial explains some basic knowledge about drawing texts and images on  LPCXpresso54608 TFT screen using emWin library.   Tools Required: ->MCUXpresso IDE ->LPCXpresso54608 SDK 2.0.0 ->em...
    Ashok Ra
    last modified by Ashok Ra
  • LPC2138 and DS18B20 interfacing (1wire protocol in lpc21XX)

    Content originally posted in LPCWare by eric_s88 on Fri Nov 15 01:10:47 MST 2013 hi everyone! I want to drive ds18b20 via lpc2138. this temperature sensor has an output via 1wire protocol. Codevision has a librarie...
    lpcware
    last modified by lpcware
  • oled with ssd1306 library for keil ide

    Content originally posted in LPCWare by alikari on Sat Dec 26 10:10:56 MST 2015 Hi I am new to LPC1768 arm  and have some experience with GPIO  , UART , character LCD . Now I  want to use adafruit OLE...
    lpcware
    last modified by lpcware
  • "New Project" wizzard and Pins tool MCUXpresso for LPC845

    1.) The wizzard asks for driver inclusion. Why aren't the chosen drivers not automatically included, e.g. #include "fsl_gpio.h" in main.c when I chose the GPIO driver in the wizzard?   2.) Why do I have to call ...
    12345 67890
    last modified by 12345 67890