• TrustZone on the LPC55S6x

    This documet is an introduction about TrustZone on the LPC55S6x devices.   LPC55S6x MCU platform and general-purpose blocks     The LPC55S69 has one 100-MHz Cortex-M33 core with TrustZone, MPU, FPU, a...
    soledad
    last modified by soledad
  • Test Elapsed time based on CTimer module

    Test Elapsed time based on CTimer module   Sometimes, It is required to test the time which an api function takes when the function is executed, for example, some users want to test the flash erasing time and f...
    xiangjun.rong
    last modified by xiangjun.rong
  • MCUXPresso IDE SWO Trace function

    The MCUXpresso IDE SWO trace function is a special feature which enables user to observe variable update, interrupt entry/exit timing, interrupt event statistic, to print information in SWO ITM Console while the MCU i...
    xiangjun.rong
    last modified by xiangjun.rong
  • Useful LPC documents and questions

    The following document contains a list of documents, questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getti...
    Erik Bustos
    last modified by Erik Bustos
  • [LPCXpresso804 board(OM40001)] on-board debugger issue: only can receive first byte.

    LPCXpresso804 board has a on-board debugger developed with LPC11U35. Old batches of the board uses the old firmware for LPC11U35 debugger.   The old firmware has some issues such as that when you send a str...
    Hao Liu
    last modified by Hao Liu
  • How to Debug TrustZone Project on MCUXpresso DIE

    This document introduces how to debug TrustZone project on MCUXpresso IDE.   Use the latest version of MCUXpresso IDE v10.3.1. Project is from SDK_2.5.0_LPCXpresso55S69. Board is LPCXpresso55s69, use the Link...
    Alice_Yang
    last modified by Alice_Yang
  • GPS Application Example Using LPC845 Breakout Board

    This is a quick introduction that shows how to interface a popular GPS module to the LPC845 Breakout Board using the UART drivers from the MCUXpresso SDK. This example reads and parses GPS data from the module when th...
  • Capacitive Touch example using the LPC845 Breakout Board

    This blog posting is an introduction to Capacitive Touch provided for the LPC845 MCU device. We are going to take advantages of the features that the LPC845 Breakout Board to show how to interface with the onboar...
  • OLED Display Application Example using LPC845 Breakout Board and SPI

    This is a quick introduction that shows how to interface the LPC845 Breakout Board with an OLED display based on the popular SSD1306 controller, using SDK drivers for SPI. With this application, you can print a t...
  • Using the SPIFI library with the LPC4370.

    In this document, I will explain how to create a project to use the SPIFI library version 1.03 with the LPC4370. For this we will need the following tools: MCUXpresso IDE 10.2. Link LPC-LINK2 to use it as an evaluat...
    Victor Jimenez
    last modified by Victor Jimenez
  • LPC MCU Training Session _ SCT Cook Book

    This cook book includes lots of interesting examples leveraging LPC MCU's powerful SCT Timer. Have fun using them, creating more and sharing more.   Original Attachment has been moved to: code-examples.zip...
    Eric Ding
    last modified by Juan Padilla
  • LPC804: PLU Hands-on Lab Guide

      Hello Community! This document is provided as a hands-on lab guide.  The intent of the lab is to demonstrate how to program the LPCXpresso804 board with the MCUXpresso IDE making use of the SDK examples...
    Carlos_Mendoza
    last modified by Carlos_Mendoza
  • LPC8N04: NFC Hands-on Lab Guide

    Hello Community!   This document is provided as a hands-on lab guide.  The intent of the lab is to demonstrate how to program and use the LPC8N04 development board by using the LPC8N04 board support package...
    Carlos_Mendoza
    last modified by Carlos_Mendoza
  • How to use the PLU configuration tool

    This document is an introduction to how to use the PLU configuration tool.         The PLU programming tool suite that is provided facilitates configuring the PLU to implement the desired l...
    soledad
    last modified by soledad
  • The LPC804 Programmable Logic Unit (PLU) 

    This document is an introduction to the Programmable Logic Unit (PLU) provided for the LPC804 MCU device.   PLU is used to create small combinatorial and/or sequential logic networks including simple state machi...
    soledad
    last modified by soledad
  • How to boot from the external flash for LPC54018

            In recent years of MCU technology evolving, booting from the external flash seems to become more and more popular, actually, LPC already has employed this technology for many...
    jeremyzhou
    last modified by jeremyzhou
  • LPC804 Capacitive Touch Demo Testing Resport

            In recently, NXP released a new sub-series: LPC80x which contains two kinds: LPC802 and LPC804 now, they have a variety of package types for choose and the LPC804 seems like ...
    jeremyzhou
    last modified by jeremyzhou
  • LPC54608 LIN slave basic usage sharing

    1 Abstract       This post is mainly about the LPC54608 LIN slave basic usage, it is similar to the post about the LPC54608 LIN master basic usage.        &...
    Kerry Zhou
    last modified by Kerry Zhou
  • LPC54608 LIN master basic usage sharing

    1 Abstract       In the previous time, I have shared one post about the kinetis L series LIN slave basic usage. Now, because the LPC54608 still don’t have any sample code about the LIN, ...
    Kerry Zhou
    last modified by Kerry Zhou
  • LPC4300 10-bit ADC performance test

    LPC4300 10-bit ADC module Introduction        LPC4300 Series microcontrollers combine the high performance and flexibility of an asymmetric dual-core architecture (ARM Cortex-M4F and Cor...
    Hui_Ma
    last modified by Hui_Ma