• MCUXpresso IDE v10.3.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.1 (build 2233) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.3.0 release, and we recommend that all e...
  • New debug probe firmware & drivers for MAX boards

    You may be interested to know that we recently released a new set of debug firmware and Windows 7 drivers for our boards that feature the LPC11U3x MCU as a debug probe (so all the "MAX" boards). The new firmware can b...
    Brendon Slade
    last modified by Brendon Slade
  • LPC845-BRK Board Projects

    The LPC845-BRK is a great tiny sub-$6 breakout board featuring the LPC845M301JBD4 MCU: ARM Cortex-M0+ 30 MHz, 64 KByte FLASH, 16 KByte SRAM On-board CMSIS-DAP debug interface, works out-of-the-box with NXP MCUXpres...
    Erich Styger
    last modified by Erich Styger
  • LPCScrypt v2.1 is now available

    LPCScrypt v2.1 is now available. This release incorporates bug fixes and the latest versions of LPC-Link2 CMSIS-DAP firmware.   LPCScrypt is a command-line based, fast flash (internal and QSPI), EEPROM, OTP and ...
  • LPC845 Breakout board now in stock (sub $6!)

    We've been working on making the flagship member of the LPC800 series more accessible to more users than ever before, and are delighted to announce the LPC845 Breakout Board is now available from our distribution...
    Brendon Slade
    last modified by Brendon Slade
  • Controlling LPC845 Breakout Board LED brightness using SDK Drivers

    The new LPC845 breakout board has 3 onboard LEDs- Red, Green, and Blue. The brightness of these LEDs can be controlled using a PWM signal by changing the duty cycle values for each of them. As this board has an S...
    Disha Anil Patil
    last modified by Disha Anil Patil
  • Accelerometer controlled LED for LPC845 Breakout using SDK drivers

    I have built an application to interface an accelerometer with the new LPC845 Breakout board using the I2C SDK driver. The accelerometer acts as an I2C slave device to the LPC845 master device. Colors on the on-board ...
    Disha Anil Patil
    last modified by Disha Anil Patil
  • Light intensity measurement using the new LPC845 Breakout Board

    Using SDK drivers for LPC845 Breakout Board, this project measures the ambient light intensity by using LDR (Light Dependent Resistor). The voltage values from LDR are read through an ADC. The new LPC84...
    Disha Anil Patil
    last modified by Disha Anil Patil
  • MCUXpresso IDE v10.3.0 Now Available

    We are pleased to announce that MCUXpresso IDE v10.3.0 (build 2200) is now available.   This is a major new version of the IDE, and contains many new features and enhancements over the previous v10.2.1 and earli...
  • MCUXpresso IDE v10.2.1 Now Available

    We are pleased to announce that MCUXpresso IDE v10.2.1 (build 795) is now available.   This is a maintenance release that builds upon the previous MCUXpresso IDE v10.2.0 release, and we recommend that all e...
  • LPC546xx: Enable EEPROM clock in AHBCLKCTRL0 before IAP EEPROM write API

    The LPC546xx IAP EEPROM Write page API  does not enable the EEPROM clock for the write operation. This causes  EEPROM write operation to fail when using the IAP API.  This problem does not occur for IAP...
    SowmyanKousthubadharan
    last modified by SowmyanKousthubadharan
  • LPC540xx OTP Programming Example

    Hi folks, Attached is a sample source code for OTP programming in NXP LPC54018 MCU. Brief about the example: The example programs 4 words of data each into OTP bank 1 and OTP bank 2. The example uses LPC54018 SDK...
    SowmyanKousthubadharan
    last modified by SowmyanKousthubadharan
  • A perfect fit for power conscious designs that require high-performance capabilities

    If you are searching for a high-performance, power efficient, yet cost sensitive MCU for your designs, then here is the exciting news: NXP recently introduced the LPC51U68 MCU.   Power efficient solution for f...
    Omar Cruz
    last modified by Omar Cruz
  • 2016.  LPC Microcontrollers.  An amazing year in review

    The year when two titans came together forming what is now the #1 supplier to the broad based MCU market.  To the industry, it was the year of the merger, clouded in uncertainty.   Not so for LPC.  &...
    Justin Mortimer
    last modified by Justin Mortimer
  • LPCXpresso54608 Touch screen tutorials on mbed

    @jennymplunkett from the Arm mbed team just posted a great tutorial using the LPCXpresso54608 touch screen on her blog... check it out at https://os.mbed.com/blog/entry/How-to-LPCXpresso54608-touch-panel/ Same c...
    Brendon Slade
    last modified by Brendon Slade
  • LPC800 DIP board now available from Coridium

    The LPC800-DIP board is now being sold by Coridium for just $10: http://www.coridium.us/coridium/shop/boards/bd07-special   They have their own version of gcc and BASIC running on it too, available for ju...
    Brendon Slade
    last modified by Brendon Slade
  • OM13086 ZentriOS Device Setup failure

    I have the OM13086 Cloud Connectivity Kit I have been following the ZentriOS "Quickstart Guide". As part of the Zentri OS Quickstart procedures, I chose "Custom Install", so instead of using the "Zentri IDE", I'm uisn...
    Randy Lathrop
    last modified by Randy Lathrop
  • LPC546xx Training Slides are Coming now~~~

    Hi LPC fans,   We have very good news to share with you today. As you know, one of the major roadmap for LPC this year is the LPC546xx release. And it will be coming soon~~~, as you all expected. For this new and...
    Eric Ding
    last modified by Eric Ding
  • LPC54114 dual-core example

    Some days before, there is a great post about LPC dual-core, LPC key feature_DualCore  This time, we show a LPC5411x based dual-core example. It shows all aspects about dual-core development, startup, commu...
    Rocky Song
    last modified by Rocky Song
  • MCUXpresso IDE v10.1.0 Now Available

    We are pleased to announce that MCUXpresso IDE v10.1.0 (build 589) is now available.   This incorporates many new features, as well as enhancements based on feedback that we have received since the original...