Skip navigationLog in to follow, share, and participate in this community. I am using LPC11U68 eval board to program and debug a off board target processor (LPC11U68). The debug session does not start and I get the following errors: MCUXpresso IDE RedlinkMulti Driver v10.2 (Jul 25 201... Debugger probe problem LPC11U68
BackContent originally posted in LPCWare by drvrh on Thu Aug 20 03:05:34 MST 2015 Hello, I have a problem with LED blinking and my LPC11e14, programming it's OK but on my ouput pin have nothing. On all IO pin have voltag... Problem with LED blinking LPC11e14
BackHi, On a fresh Windows 10 setup, running MCUXpresso IDE v10.2.1 [Build 795] I cannot debug my LPCXpresso V2 boards LPC11U68 or LPC1549. Both Debug Probes show up fine as LPC-LINK2 CMSIS-DAP V5.183 with no driv... LPC1549 and LPC11U68 Failed on connect: Ee(42). Could not connect to core.
BackHello, I´ve being trying to use the source code and schematic provided by NXP in the AN11153 (DMX/RDM slave) but I can´t seem to make it work. I´m using a LPC1112/102, and I tried compiling ... DMX512 Slave SDK not working
BackHi, I've tried to communicate to the LPC11A04UK (WLCSP20 package) without success. I'm using the LPC-Link-2 CMSIS-DAP V5.173 I get the following error message : --------------------------... Can't connect to LPC11A04UK
BackHi! I am using LPC11uxx and trying to configurate UART smart card mode. When I filled register DLM value, IER also fiiled by the same value? Is it normal? If yes, why it is happens? Hello! I'm try to implement connection between LPC11u12 and smart card via UART. To provide the right clock to the smart card I should to fill UART DLL and DLM registers this way: uint32_t divider = ((( sys_clk / ((sc... Hi, I've got some very old IOH libraries for the 11U37 and was just looking to see if they'd been updated since 2013 but they seem to have disappeared. Any idea where the libraries and documentation have... Where have the IOH libraries gone for the LPC11U37H?
BackHi! Can anybody help me to config the 32-bit timer to catch 3 * 10^(-6) seconds? I did smth like that: if my freq equal to 48MHz, then every 154 ticks has passed 3 nsec. Using that idea, I avoid of configure prescaler... I have a question regarding bypassing the system oscillator in LPC1114. If I enable the system oscillator bypass enable (set bit 0 of SYSOSCCTRL to be 1), I could connect an external clock source to XTALIN pin as the ... LPC1114 bypassing the system oscillator
Back你好! 请问有SPI方式的Nor Flash 型号为GD25Q64的参考代码吗?我看网上似乎是有相关才考代码的,但是没有找到。方便提供一下吗? Hi, we are using the LPC11u37 as a serial to USB converter. When we connect it to a WIN7 PC every thing ist working fine. When we use a nativ WIN10 PC, the PC recognised the USB device but we get a exclamation mark a... LPC11U37 not working with WIN10
BackI am using the LPC11C24 board OM13093 to test the deep-sleep mode. According to the manual of LPC11xx and the application note AN11027, I set three pins (p0.6, p0.11, p1.0) connect the start l... LPC11C24 can't wake up from Deep-Sleep
BackHello, I'm hoping to create a board using the LPC11D14 and am curious how exactly the SWD/JTAG header is to be connected to the processor in order to flash the part correctly using an LPC-LINK 2. I app... How to transfer the data between the GPIO port to internal memory SRAM in LPC4370 without using the DMA technique such that is there is any single Embedded C instruction to transfer the any one of the GPIO port data i... How to transfer the data between the GPIO port to internal memory SRAM in LPC4370 without using the DMA technique such that is there is any single Embedded C instruction to transfer the any one of the GPIO port data into the internal SRAM specified addres
BackHello, I'm developing an application using Deep Sleep mode with the LPC11C24 board. As our setup we are using the LPCXpresso LPC-Link LPC11C24 Rev B board and MCUXpresso 10.2. I just tried to work on the code ... LPC11C24 ResetISR() error
BackHello, I'm currently working on an application that involves the LPC11C24 board and we're using the LPCXpresso LPC11C24 Rev B board (with LPC-Link) to test it. We want to make use of the deep sleep mode so... LPC11C24 Deep Sleep Wakeup Handler
BackHi, I am currently working on a project including the LPC11C24 board (in particular, we're testing using LPCXpresso LPC11C24 Rev B board) and I would like to implement deep-sleep mode. I searched through Interne... [SOLVED] Deep-Sleep mode on LPC11C24
BackHi, I am testing the Interrupt with LPC1114. LPCOpen nxp_lpcxpresso_11c24_periph_pinint worked. But GPIO Port1 any pin does not respond. Is there anything I have to add something? Thank you. /* GPIO pin for ... How can I enable the interrupt of GPIO Port 1?
BackHi, I am working with the LPCXpresso LPC11C24 board using USB to flash code on the board and to debug it, but I keep getting the error MCUXpresso IDE RedlinkMulti Driver v10.2 (Jul 25 2018 11:29:34 - crt_... [SOLVED] LPC-Link Debug Error
Back