• OM13085 User Manual - overdue...

    Where is the user manual promised by Embedded Artists for the end of 2018?  I just need to know if a user manual will soon be released (and when), so that if not I can choose another product.   This is non-...
    Jeff Lloyd
    last modified by Jeff Lloyd
  • How to enter into ISP mode through 'reinvoke ISP' in LPC1759

    In LPC1759, I entered ISP through "reinvoke ISP" with the following steps Disable PLL Reset timer 1 Re-map interrupt vectors Set watch dog timeout Reinvoke ISP After entering into ISP, What exactly happens in the cont...
    Keerthana R
    last modified by Keerthana R
  • LPC5500 Series MCU availability?

    Could you please update when LPC5500 series controller will be available in market?   What about the development board availability?
    jtro9
    last modified by jtro9
  • LPC2478FBD208,551/Over Current Sense pin

    Hello,   I am using LPC2478FBD208,551 in my project. Here I am going to use 2 USB type A and LCD Interface. For Both the USB Type A i am using USB Over Current Sense IC which send OCE Signal to LPC247...
    Alpesh Borad
    last modified by Alpesh Borad
  • LPC55S69 documentation

    Hi,    When should the LPC55S69 reference manual and datasheet be available?  Ari.
    Ari Mendes
    last modified by Ari Mendes
  • LPC1768 PCB Design Course

    # I have question about Dutch course to studding how to use Arm LPC1768 inside of our PCB as a stand alone Micro-controller and to easy on board or separate programming them? If it in English or Nederlands is where ...
    Farbod Miri
    last modified by Farbod Miri
  • LPC5500 with DSP accelerator

    Hi, I'm very excited about the  announcement of the new LPC5500 family. I'm especially curious about the DSP accelerator. Is it accessed as extension instruction set? Or is it a coprocessor? Or is it a per...
    Ari Mendes
    last modified by Ari Mendes
  • Can it possible to implement NIST test suit functionality with LPC1788 ?

    I want to test TRNG random data generated by FPGA .   Data comes from FPGA to LPC1788 through SPI . Can it possible to implement NIST test suit functionality with LPC1788 ? I don't have any external PC com...
    Pravin Patil
    last modified by Pravin Patil
  • How to transfer the data between the GPIO port to internal memory SRAM in LPC4370 without using the DMA technique such that is there is any single Embedded C instruction to transfer the any one of the GPIO port data into the internal SRAM specified addres

    How to transfer the data between the GPIO port to internal memory SRAM in LPC4370 without using the DMA technique such that is there is any single Embedded C instruction to transfer the any one of the GPIO port data i...
    sujay p
    last modified by sujay p
  • LPC2148 datacode or something mark

    Hello all, im bought MCs LPS2148FBD64 with marking on the last row on case "ZSD1807C" and my soft as Boot Loader ID v2.13 cant work with this, he asks v2.12. Before im bought with mark "ZSD0834A" and all working...
    Dima Marushak
    last modified by Dima Marushak
  • Missing SRAM layout of LPC546xx 136KB RAM version in doc

    LPC546XX has 136KB RAM and 256KB flash version, but I cannot find the 136KB SRAM memory map in the reference manual, which all describe RAM as 200KB.   My question is which is the SRAM layout for 136KB RAM ver...
    Yao Zou
    last modified by Yao Zou
  • MCUXpresso SDK support for LPCXpresso43S67

    Will there be MCUXpresso SDK support for the LPCXpresso43S67?
    Nick Guzzardo
    last modified by Nick Guzzardo
  • Problem sending mail via LPC1769, RL-TCPnet Keil IDE

    Hello, I am working on LPC1769, Keil IDE and using RL Tcpnet. I am unable to send emails via SMTP. I am either getting  a SMTP timeout or SMTP error. i tried using port 25  and port 80 but it didnt wor...
    Zaid Shaikh
    last modified by Zaid Shaikh
  • The security certificate for downloading the LPC SDK Builder has expired and is no longer valid.

    Hello -   Wanted to download the LPC SDK Builder and both Firefox and Internet Explorer refuse with an indication that the security certificate expired Sunday, October 7.   Please fix.   Thank you.
    Mark Becker
    last modified by Mark Becker
  • LPC series more consuming controllers

    What are the fast moving, more consuming among the LPC series controllers?
    Muralidhar M
    last modified by Muralidhar M
  • LPC4370 TFBGA100 and SDRAM

    I'm new to all of these. Is it possible to configure an 8-bit SDRAM to a 100TFLBGA LPC4370? Noticed there's only a single address pin BA0 (EMC_A13) on the 100pin package.
    Kristina Cortez
    last modified by Kristina Cortez
  • Thingstream button LPC824 with coms module & GPS

    Can anyone assist what the part number for the Thingstream button LPC824 with coms module & GPS as shown in the webinar 'Designing and deploying intelligent, low-power and low cost'? I found the LPC-Link2 tool eas...
    Rory McPhail
    last modified by Rory McPhail
  • How do I use the captouch on the microcontroler LPC845M301JBD48E ?

    I found no examples. Application note AN12178 is insufficient to configure. The files contained in Keil "Fsl_capt.c" and "Fsl_capt.h" didn't have the function of how to select and initialize the pins. Can anybody...
    Rafael Rizzon
    last modified by Rafael Rizzon
  • LPC54114 sleep mode using Interrupt

    Hi,    I have LPCXpresso54114 board. In which I created two external interrupt. INT0 is to wakeup the MCU from Sleep mode. And INT1 is to entering into the sleep mode. when I use INT1 to enter into the...
    Dineshkumar J
    last modified by Dineshkumar J
  • What are the differences between LPC540xx and Kinetis K64 ?

    Hello,  When picking a MCU for a product, what are the differences between LPC540XX and Kinetis K64 ? From my research, the only major difference is LPC has optional M0 core. Both have M4 core, about same c...
    Adrian Mango
    last modified by Adrian Mango