Peter Furtner

LPCXpert V3.4: Software Expert Tool for the LPC Families of Micro-Controllers

Blog Post created by Peter Furtner Employee on Mar 26, 2017

LPCXpert V3.4 is the latest release of a freeware expert tool for the CORTEX-M based LPC families of microcontrollers. This tool simplifies the selection of a MCU device, speeds up the creation of application code and initialization code and supports generation of an application specific schematic Symbol. This version supports more than 410 different CORTEX-M based micro controllers from NXP.

  

LPCXpert supports all phases of a development. During the MCU selection phase LPCxperts supports selection of a target MCU by providing selection features in the "MCU Select" tab. During the software implementation phase LPCXpert provides a graphical user-interface to configure the pinout (Pin-MUX) and the peripheral interfaces of the target device. LPCXpert then also generates projects providing a framework of reference applications. These applications configure the Clock Generation Unit (CGU) and the on-chip peripheral interfaces of the device to test and demonstrate the setup.

  

New and enhanced features include support for LPCopen software package from NXP. Features also include generation of a Schematic Symbol for the ALTIUM Designer and the CADSOFT EAGLE V6.2 and generation of projects for the NXP LPCXpresso and MCUxpresso IDE, IAR Embedded Workbench (EWARM), Keil µVision and GNU C-Compilers, as well as links to Internet Sites for additional information.

Using LPCXpert it is possible to set the pins of each peripheral (i.e. for SPI, CAN., I2C, EMC, ETH, ...) and to configure the features of each pin (Pull-Up, Pull-Down, ...). In addition LPCxpert V3.4 also supports configuration of pre-built demo code for the LPC8xx and LPC54xxx Families of MCUs.

  

Based on the configuration LPCXpert may generate a C-Code Project or a Schematic Symbol. In addition LPCxpert saves up to 8 different pin-mux configurations and restore from up to 10 different configurations. Additional Information and the download is available from the following Web-Site:

--> http://www.lpcxpert.com

Outcomes