• I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes

    I have just downloaded the MCUXpresso 10.3.1 build 2233 (32-bit) for the first time to use with my new FRDM-KW41Z board and I have hit a snag when I try to debug any program in that it says it cannot link any pro...
    Colin Gerrish
    last modified by Colin Gerrish
  • Application solved with uTasker

    This is a message to all of you who are as new into embedded development as i was a couple of months ago.   Me and my colleague had an application to solve but did not know how we where going to solve it when we...
    Andreas Andersson
    last modified by Andreas Andersson
  • KW36 IQ method of BLE localisation

    Hi,      I see that KW36 is supported for IQ localisation. Please give me some API documents or examples to realize this.
    VIGNESH BALAJI
    created by VIGNESH BALAJI
  • Bluetooth SIG Component QDIDs for declarations

    Are updates to the Bluetooth SIG component QDIDs planned to satisfy the requirement to use TCRL 2018-1? The Launch Studio only shows these older QDIDs: D031669 84040 - Component (Tested) NXP Semiconductors Kinetis...
    Bob Recny
    last modified by Bob Recny
  • how to add support for kw41z in kinetis design studio?

    Hello, i installed kinetis design studio and i'm trying to create new projects for kw41z mcu. Unfortunately when i create a new kinetis project and i try to select processor name i read many mcu name but there is not ...
    marco mangraviti
    last modified by marco mangraviti
  •       [USB-KW41Z] Demo gpio_led_output wont seem to work

    Hello,    i'm just getting started with the USB-KW41Z and was trying to get the sample project to blink the LED to work but noting seem to happen. I build it and everything looks good:    Bu...
    Cesario Dos Santos
    last modified by Cesario Dos Santos
  • FRDM-KW24D512 un-responsive after Bricking in Windows10

    Board:       - FRDM-KW24D512 Problem:       - Out of my four above types of boards, three became unresponsive due to bricking in Windows 10 or while trying to unbri...
  • NXP BLE corporate training

    Does NXP give any corporate training for BLE stack or BLE products? I am working on BLE with Kinetis W series device and would like to know that if there is any training program NXP offers on this?
    VIGNESH BALAJI
    last modified by VIGNESH BALAJI
  • Obtaining a FRDM-KW36 and Documentation

    I'm trying to procure a FRDM-KW36 evaluation board for testing and development, but I cannot find them for sale anywhere yet. Documentation is not available either. Our usual hardware vendor has been getting the ...
    Jacob Whiteley
    last modified by Jacob Whiteley
  • KW36 Bluetooth low energy stack documentation

    Hi,     Please help me in getting documentation for BLE stack for KW36
    VIGNESH BALAJI
    last modified by VIGNESH BALAJI
  • Programming KW36 FlexNVM with MCUXpresso IDE Example

    Introduction This document provides guidance to program or store code in FlexNVM memory available in KW36 MCU to use it as P-Flash memory. This article uses as the starting point, an example imported from the connecti...
  • KW41Z Hybrid BLE + 802.15.4 coordinator example does not work

    Has anyone got the example project below working because I cannot? frdmkw41z/wireless_examples/hybrid/ble_802_15_4_fsci_black_box_bm   This project appears to have been used in "https://www.nxp.com/docs/en/appl...
    Liam Hayes
    last modified by Liam Hayes
  • OM23221ARD: NTAG I2C plus kit with FRDM-KW41Z

    I am using the OM23221ARD: NTAG I2C plus kit with a FRDM-KW41Z board. According to the pinout, the NFC energy-harvesting output VOUT is routed to the P5-9VIN pin on the KW41Z Arduino header. As the output voltage...
    Steve Smythe
    last modified by Steve Smythe
  • Can't flash kw2xd since Low Power Mode enabled

    Hi,    I'm working on phyWAVE  KW2xD ARM Cortex-M4 board (KW22D512VHA5) with RIOT-OS.  I had no prior problems for flashing, debugging, running my code through OpenOCD / JLink / SWD interfac...
    Olivier Fauchon
    last modified by Olivier Fauchon
  • I want to know about maximum timer value for KW36z controller. How to get that value by calculation.

    KW36z Microcontroller
    Abhijeet Tippanna
    last modified by Abhijeet Tippanna
  • S32K DMA传输ADC数据

    #S32K ADC DMA :由FTM1每隔1ms触发PDB0,PDB0设置pretrigger 3个ADC0通道,3个ADC0通道采集完一遍通过DMA中断读取。之前用过采集4路ADC并通过DMA读取,但是改成3通道时进入不了中断,不知道是不是DMA传输ADC只支持特定的通道数。 配置程序如下,接收RecordBuf_ADC0[3]是uint32_t类型,ADC通道从2~4, 请大佬们帮忙分析一下问题: &...
    王 云
    last modified by 王 云
  • MCG/PLL Configuration

    Hello,    I am using a KV46 in my design and have the MCG setup to run in PEE mode. I am using an external 8MHz xtal for clocking and I have the PLL setup so that the 8MHZ is /1 coming in. from there I hav...
    Brian Mohlman
    last modified by Brian Mohlman
  • KBOOT Compatible Loader with additional AES-256 Encryption/Decryption for very strong IP protection

    Hi All   I am pleased to announce that the uTasker project now includes small-footprint KBOOT compatible UART/USB-HID loaders for (almost) all Kinetis boards and Kinetis parts that can be built with MCUXpresso, ...
    Mark Butcher
    last modified by Mark Butcher
  • Input interrupt or event in KW41Z with wireless_examples_thread_router_eligible_device

    Hi, I want to make at the Coap application from the example wireless_examples_thread_router_eligible_device an custom application. I need to send my luxometer value through Coap when an input interrupt comes in P...
    DIEGO COMIN
    last modified by DIEGO COMIN
  • Error in LPTMR SDK

    I'm using the SDK for MKW41Z512 and have found a probable error in the SDK related to the LPTMR. In fsl_lptmr.h there is a function for setting the compare register. For some reason (which does not make sense if the t...
    Samuel Vestlin
    last modified by Samuel Vestlin