• Interface with Alexa (568-SLN-ALEXA-IOT-ND )

    Hi, I am working on project that collecting data form the sensor and plotted them by Matlab. I want to interface my system with Alexa, so when my sensor detect the level is low then Alexa will speak up " Are you...
    ABDULLAH ALHAZMI
    last modified by ABDULLAH ALHAZMI
  • i.MX RT106F for Face Recognition

    im need pard number of lcd module and camera module in imxrt106f for buy. please tell me exact part number. please heelp me.
    farhad vahdani
    last modified by farhad vahdani
  • i.MX RT1064 & Internal 4MB of Flash   

    Hello team,   I'm trying to figure out how the internal 4MB of Flash in the RT1064 works, I want to recommend the device to a customer looking for an MCU with the amount of RAM that RT has and the power of ...
    Atzel Collazo
    last modified by Atzel Collazo
  • Can we use a XIP flash and a data flash at the same FlexSPI controller?

    Hello,   the reference manual of RT1020 shows how to connect flash devices to FlexSPI (RT1020 has only 4 data lines for A and 4 for B not 8 as shown in the picture) We want to use XIP on Flash A1 (read only) ...
    Stefan Mitterhauser
    last modified by Stefan Mitterhauser
  • iMXRT1052 Link Application to RAM

    I have a question regarding the linker option: "Link application to RAM" when using Managed Linker Scripts in MCUXpresso IDE (v10.3.1 [Build 2233] [2019-02-20] Manifest for SDK SDK_2.x_EVKB-IMXRT1050 V 2.5.1). ...
    Johann Hagler
    last modified by Johann Hagler
  • Bad USB device mode DMA performance in RT1064/1062

    Hi,   We experience data loss in USB device mode when isoch and bulk endpoints are used in parallel. We analyzed this issue in detail (we specialize in USB technology) and found the following:   1) If one ...
    Udo Eberhardt
    created by Udo Eberhardt
  • Littlefs on RT1064 internal flash.

    I found the Littefs example on SDK. But It use the External Flash through the FlexSPI.   I would like to use the Internal Flash. 3MB for Program Area. 1MB for littefs Area.   In the lfs_support.h  ...
    ChoonGyeong Lee
    last modified by ChoonGyeong Lee
  • Programming the internal Flash of RT1064

    Is there any updated examples for programming ("IAP") the internal 4 MByte Flash of the RT1064 ? In the SDK there is the "flexspi/nor/polling transfer" example, but this is only for the external Flash on the EVK (on ...
    Carsten Groen
    last modified by Carsten Groen
  • I.MX RT1061 Writing flexspi flash through edma wrongly

    Is there a example code of I.MX RT1061 FlexSPI using edma? The manual is simple. I'cant figure out the methods. I try to set watermark to 0, debug a few times and finally program the flash by edma. But there are...
    莫 郑
    last modified by 莫 郑
  • i.MX RT106x: enhanced tx buffer descriptors + hardware checksums...?

    On the i.MX RT106x, I'm trying to combine enhanced buffer mode (for 1588 timestamps) and the IP accelerator (for hardware calculation of both IP header checksums and IP protocol checksums). In my tests, it seems that ...
    Nick Pelling
    last modified by Nick Pelling
  • XIP through OTFAD problems on RT1011

    Hello, we are using RT1011 and we are having troubles with XIP from FLASH on FLEXSPI through OTFAD. Our application is correctrly encrypted and we can see that the startup code at the reset vector is executed co...
    Stefano Voulaz
    last modified by Stefano Voulaz
  • Source for sdphost and blhost?

    Hi,   Is it possible to get the source to sdphost and blhost please?   Thanks and regards, Ronnie  
    rshipman
    last modified by rshipman
  • RT1020 - Fixed OTPMK

    Hi,   What is the Fixed OTPMK and how do I set it and use it?   Thanks and regards, Ronnie
    rshipman
    last modified by rshipman
  • PHY_xxx, ENET_xxx functions are thread safe?

    Hi   I don't think PHY_xxx and ENET_xxx functions are not thread safe but want to clarify if they really are and want to know how to use it in the right way.   Q1) is it possible to call PHY_GetLinkStatus fu...
    JIWON KIM
    last modified by JIWON KIM
  • RT1015 USB1 Download and LPUART1 Download

    Hi,   I am using RT1015 EVK, I found two condition.   Condition 1: If I connect USB1(J9) and set the switch to download mode, after power on LPUART1(J41) cannot upgrade.   Condition 2: If I do...
    Ken Su
    last modified by Ken Su
  • RT1020 - How is the OTPMK set and used?

    Hi,   I have some questions regarding the OTPMK key:   How do I set the OTPMK for the RT1020? When setting BEE_KEY0_SEL=b10 to use the OTPMK, does it use the OTPMK unchanged, or does it combine it with other...
    rshipman
    last modified by rshipman
  • IrDA

    I'm having issues getting my IrDA communications working on a 1064.  It appears to only get locked when I over-ride the autobaud to OSR 32 no matter the baud rate and it's accuracy (still <3%).  Does the ...
    Steven Jones
    last modified by Steven Jones
  • imxrt1064 USB video bit rate

    Hello, I have been experimenting with USB video lately and I would like to know if a imxrt 1064 can stream video over USB at 30 FPS for an uncompressed image with the resolution 640 x 480 (16 bit per pixel). If not -...
    Tamir Michael
    last modified by Tamir Michael
  • RT1064 can't boot from the interior Flash ROM

    Hi NXP,   I am debugging iMX RT1064 MCU right now. I meet a problem to run the code on the chip. The chip can’t boot from the interior Flash ROM when I power up and reset the MCU. I try several thing...
    JIAN LU
    last modified by JIAN LU
  • MX RT1064 EVK use internal Flash as NVM

    Hi there, I'm using a MX RT1064 EVK board. Are there any examples on how to use the internal Flash of the RT1064 as non-volatile memory that can be written to/read from at runtime? I know for example that for the KW4...
    Pascal Häfliger
    last modified by Pascal Häfliger