• Application Note (AN12751): How to Enable Recovery Boot from QSPI Flash for i.MX RT600 MCU

    This document describes how to program a bootable image into the recovery Flash device using i.MX RT600 MCUs.   Click here to access the full application note.
    Monica Velez
    last modified by Monica Velez
  • Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

    The i.MX RT600 MCU includes a Cadence® Tensilica® HiFi 4 DSP running at frequencies of up to 600 MHz.The XOS embedded kernel from Cadence is designed for efficient operation on embedded system built using th...
    Monica Velez
    last modified by Monica Velez
  • Application Note (AN12762): Develop Audio Player In HiFi 4 for i.MX RT600 MCU

    This application note describes how to develop an audio player with NXP i.MX RT600 crossover MCU family. Click here to access the full application note.
    Monica Velez
    last modified by Monica Velez
  • How to configure LPSPI clock on I.MXRT1050

    The document will introduce how to configure LPSPI clock on I.MXRT1050. The purpose is to help IMXRT customers better understand the clock tree and configure LPSPI clock in SDK.    Customer can configure LP...
    fangfang
    last modified by Adrian Puga Candelario
  • RT1060 Normal GPIO vs Fast GPIO

    The i.MXRT1060 provides the tightly coupled GPIO, enable to be accessed with high frequency. RT1060 provides two set of GPIOs registers to control pads output. GPIO1 to GPIO3 is general GPIO, and GPIO6 to GPIO...
    Victor Jimenez
    last modified by Victor Jimenez
  • The “Hello World” of TensorFlow Lite

    Goal Our goal is to train a model that can take a value, x, and predict its sine, y. In a real-world application, if you needed the sine of x, you could just calculate it directly. However, by training a model to appr...
    jeremyzhou
    last modified by jeremyzhou
  • 如何为RT1050生成可启动映像文件

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341317
    Leo Lin
    last modified by Leo Lin
  • Crossover Code Challenge webinar - Dec 10.pdf

    Slides from webinar hosted by NXP on Dec 10, 2019.
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • One-stop secure boot tool: NXP-MCUBootUtility is upgraded to v2.1.0

    Source code: https://github.com/JayHeng/NXP-MCUBootUtility   【v2.1.0】 Features: > 1. [RTyyyy] Support for loading bootable image into SEMC NOR boot device >     [RTyyyy] 支持下载Bootable i...
    Jay Heng
    last modified by Jay Heng
  • RT1050 HAB Encrypted Image Generation and Analysis

    RT1050 HAB Encrypted Image Generation and Analysis 1, Introduction      The NXP RT series can support multiple boot modes, it incluses: unsigned image mode, HAB signed image mode, HAB encryption i...
    Kerry Zhou
    last modified by Kerry Zhou
  • Design an IoT edge node for CV application base on the i.MXRT1050

    Overview of i.MX RT1050        The i.MX RT1050 is the industry's first crossover processor and combines the high-performance and high level of integration on an applications processo...
    jeremyzhou
    last modified by jeremyzhou
  • Breaking Speeds Limits, Without Going Broke! -i.MX RT1010 webinar

    In case you missed our recent webinar, you can check out the slides and comment below with any questions.
    Kathleen Jachimiak
    last modified by Kathleen Jachimiak
  • RT600 ROM API for w25q128fw

    RT600 ROM API example for w25q128fw support.
    Richy Ye
    last modified by Richy Ye
  • One-stop secure boot tool: NXP-MCUBootUtility v1.0.0 is released

    1 Introduction   NXP-MCUBootUtility is a GUI tool specially designed for NXP MCU secure boot. Its features correspond to the BootROM function in NXP MCU. Currently, it mainly supports i.MXRT series MCU chips, Compared...
    Jay Heng
    last modified by Jay Heng
  • One-stop secure boot tool: NXP-MCUBootUtility is upgraded to v1.4.0

    Source code: https://github.com/JayHeng/NXP-MCUBootUtility   【v1.3.0】 Features: > 1. Can generate .sb file by actions in efuse operation utility window >    支持生成仅含自定义efuse烧写操作(在efuse operat...
    Jay Heng
    last modified by Jay Heng
  • 一站式安全启动工具:NXP-MCUBootUtility v1.0.0 发布

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342297
    Leo Lin
    last modified by Leo Lin
  • RT1060 的普通 GPIO 和 快速 GPIO的对比

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342954
    Leo Lin
    last modified by Leo Lin
  • RT1050采用不同存储器的启动时间

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341316
    Leo Lin
    last modified by Leo Lin
  • i.MXRT1050 SDRAM 的时钟配置

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340813
    Leo Lin
    last modified by Leo Lin
  • i.MXRT 1050 EVK + MCUXpresso 的快速入门

    [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341985
    Leo Lin
    last modified by Leo Lin