• Should there be a command line after booting Android?

    Hey guys, I have configured Android 9 for our custom board based on Sabresd board.It is booting properly, I am also able to see the android display. But in the log I keep getting healthd status lines. There should b...
    Himanshu Savargaonkar
    last modified by Himanshu Savargaonkar
  • hwclock -w causes kernel panic and reboot in rtc pcf2129

    Hello Everyone, I am using pcf2129 rtc ic for rtc clock as well as tamper detection. and I am using the driver file from the link linux/rtc-pcf2127.c at master · torvalds/linux · GitHub  but I am getti...
    Anusha N
    last modified by Anusha N
  • Qemu Enable with Sabrelite board

    Hi all I am trying to enable sabrelite board with Qemu Qemu supported machine with ./qemu-system-aarch64 -M ? sabrelite            Freescale i.MX6 Quad SABRE Lite Board (Cortex A9...
    satish kumar
    last modified by satish kumar
  • Imx6ull -- To create uImage what is CONFIG_LOAD_ADDRESS

    Hi all I am trying to compile & create uImage for imx6ull board  & success in creating the vmlinux & but failed to create uImage as it is failed to load the Image address to create the same Can you...
    satish kumar
    last modified by satish kumar
  • While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs

    Hi I am testing FRDM33772BSPIEVB and S32K144EVB-Q100. While checking the BCC_S32K144_Monitoring example, a red LED is displayed and an error occurs. The battery pack is not connected. Is there a way to check the code ...
    jang junghoon
    last modified by jang junghoon
  • Windows 10 IoT Core 솔루션 소개 드립니다.

    안녕하세요? i.MX6 CPU는 Android, Linux, Window Embedded Compact 2013(Wince 8), Windows Embedded Compact 7(Wince 7), Windows 10 IoT Core 운영체제를 지원합니다. NXP와 Microsoft 사가 함께 Windows 10 IoT Core 운영체제를 개발하고 장기간 지원한다고 발표하였습니다. ...
    Minsung Kim
    last modified by Minsung Kim
  • Yocto toolchain build fail

    Hi! I try to build toolchain according to this guid: link. But as the result I get this error on cmd bitbake meta-toolchain: ERROR: nativesdk-glibc-2.24-r0 do_compile: oe_runmake failed ERROR: n...
    Alexandr Kolesnikov
    last modified by Alexandr Kolesnikov
  • How to change CCM_CSCMR2[7:2] (CAN_PODF) using clock API from the module

    Hello all,   I look for rationale of design of imx_clk_divider(), choice of CLK_SET_RATE_PARENT for such clock instances like CAN_PODF. and here is the line of my interest from clk-imx6ul.c: 787b4271a6a0c (Fra...
    Krzysztof Blaszkowski
    last modified by Krzysztof Blaszkowski
  • Not able to print chatater/string on display using imx6q-sabrelite

    hi ,    am using a imx6q, and a display connected through parallel RGB , using "echo "hello world " > /dev/fb0"  cmd  am tying to display charater/ string on screen , in screen a...
    Arjun k
    last modified by Arjun k
  • TED KIT2(OM6716,599) 실행 소프트웨어 업그레이드버전 확인요청?

    현재 VER3.4.1를 사용하고 있습니다만 콘티넨탈 회사에서 VER3.6 버전을 사용한다고 하는데 같은 버전을 다운 받을수 있는지 문의 합니다
    kim younghyun
    last modified by kim younghyun
  • Using of ZMK on IMX6 board

    We want to use to software programming method to write some value to ZMK. And want to read the same from software program i-e using c language.   Is it possible to get the sample program which will do the same? ...
    Vikas Sharma
    last modified by Vikas Sharma
  • Unable to have custom i.MX233 board boot from SD Card

    Hi,   For the past months I'm trying to get my custom board with the i.MX233 boot from SD card. However without success, the only thing I get out on Debug UART, are the following boot codes: H0x80501003 0x80502...
    Onno van der Leun
    last modified by Onno van der Leun
  • i.MX6 CPU용 코덱 솔루션 소개 드립니다. [Directshow]

    안녕하세요? i.MX6 CPU로 임베디드 솔루션을 개발하고 있는 위아데브 입니다. i.MX6 CPU는 Android와 Linux 뿐만 아니라 WinCE 계열인 Windows Embedded Compact 7과 Windows Embedded Compact 2013 운영체제를 지원합니다 저희가 만든 Directshow 기반 코덱 솔루션을 소개 드립니다. 참고 부탁 드립니다. -...
    Minsung Kim
    created by Minsung Kim
  • Delete!  Just a test thread. No action required.

    This is just a test question.  no action required.  Please DISREGARD
    Enrique Encarnacion
    last modified by Enrique Encarnacion
  • i.MX6Q  인터럽트 핀 사용 방법은?

    i.MX6Q 와 리눅스를 사용하려 합니다. 이때 i.MX6Q의 인터럽트 설정을 어떻게 하나요?    예로 SPF-27392_C5.sche 회로에서 NADNF_ALE(A16)을 CAP_TCH_INT0로 사용 할 경우   해당 레지스트에서 인터럽트로 사용 시 어떤 모드로 설정해야하나요?"
    hongsoo kim
    last modified by hongsoo kim
  • bitbake를 이용해서 build를 했고 /deploy/images/imx6qsabresd/ 하위 폴더에 많은 이미지들이 생성되었는데요

    .sdcard 를 그냥 sd카드에 쓰면 부팅이 되지만   그렇게 말고   u-boot, 커널이미지, 루트파일시스템을 개별적으로 sd카드에 올려서 동작시켜보고싶은데   생성된 이미지들이 많아서 무얼가지고 만들어야 하는지 잘 모르겠습니다   창에 출력될때 색깔도 다르고 하던데, 각 파일들이 갖는 의미를 좀 알려주셨으면 합니다.   감사합니다.
    jungsae yim
    last modified by jungsae yim
  • Neon vector stores slow depending on destination

    Hello,   I have written a neon-optimized box filter in assembler for my i.MX6 system. I know about the memory bandwidth problems of the machine, but this doesn't explain my observation:   This part of my c...
    Philipp Sasse
    last modified by Philipp Sasse
  • i.MX8에 대한 개발 자료 요청

    안녕하세요? 저희는 i.MX6 를 이용해서 개발보드를 만들고 있는 업체입니다. 주로 사용하는 운영체제는 Android, WEC2013이고, BSP와 어플리케이션, 그리고 코덱 개발을 함께 하고 있습니다.   NXP 홈페이지에는 i.MX8 제품이 나와 있지만, 개발 문서는 제공을 안해 주고 있는 것 같습니다. 저희 개발 라인업을 i.MX8 으로 확장해 나아가고 싶은데,...
    JaeHyeok Shin
    last modified by JaeHyeok Shin
  • i.mx6sx Bt656 영상 캡처 문제

    i.mx6sx의 CSI0, CSI1을 이용하여 영상캡처를 할려고 합니다.   CSI0는 VADC를 이용하여 NTSC 카메라 영상을 받고 있습니다. 그리고 CSI1는 TW9900(비디오 디코더)을 이용하여 NSTC 카메라 영상을 BT656,YUV422으로 받으려고 합니다.   현재 TW9900 드라이버 작업을 통해 받은 영상을 보여드립니다.   ...
    moowonlee
    last modified by moowonlee
  • sabresd adb 연결

    sabresd 보드에 메뉴얼을 따라서 만든 이미지로 lollipop5.1을 부팅하는데 성공했습니다 imx6q sabresd보드에 pc를 연결하여 adb접속을 시도하는 중에 usb연결 문제가 생겼습니다 해당보드에 pc와의 adb를 위해 usb를 연결할 수 있는 포트는 otg포트 하나 뿐으로 마우스나 키보드를 사용하기 위해서는 usb허브를 연결하여 연결 가능 usb 수를 늘리는 방법밖에...
    suhyun choi
    last modified by suhyun choi