• video device node entry for OV5640 MIPI CSI board (mini SAS)

    Hi All,   I am working on imx8qm with Android 9 Automotive. I got the following response from OV5640 MIPI CSI board (mini SAS)   ov5640_mipi_v3 5-003c: 5-003c supply DOVDD not found, using dummy regulator ov...
    vinothkumar s
    created by vinothkumar s
  • work with 3840x412 LCD

    Hi all!   I want to work with i.MX6 Quad with linux and LCD display with 412 vertical by 3840 horizontal pixel resolution. Does i.MX6 support it? Thanks!   Artur.
    Artur Null
    last modified by Artur Null
  • I.mx8mmini Error: imx-gpu-viv/imx-gpu-viv_6.2.4.p2.3-aarch64.bb:do_instal

     Hi,   Getting this below error how to resolve ERROR: imx-gpu-viv-1_6.2.4.p2.3-aarch64-r0 do_install: Function failed: do_install (log file is located at /home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/t...
    Santhosh Kumar
    last modified by Santhosh Kumar
  • SDK 2.7.0 - broken?

    Hello,   I am running MCUXpresso v11.0.1 on Linux, with SDK_2.X_EVK-MIMXRT1064 installed. However, none of the newly generated SDKs v2.7.0 can be installed - they all report    "java.lang.Exception: ...
    Tamir Michael
    last modified by Tamir Michael
  • how to send meaning values by uart ?

    Hello ı am working on imxrt 1050.    I tried to send unsigned 32 bit value and encountered meaningless values. How can ı fix it?     uint32_t x = 0x12345678; LPUART_RTOS_Send(&handle,(u...
  • MFGTool Error when flashing a MX6SX 14x14 board with eMMC

    Hello all,   I'm trying to boot a board based on SABRESD design. The board had passed the memory test, but  mfgtools won't flash it.   Last error I can see in the log is 'Failed to Initialize memory!'...
    Victor Palacio
    last modified by Victor Palacio
  • Wi-Fi capability of i.Mx 8M Nano evk

    Does the EVK come with Wi-Fi in built? Or do I need to buy a wi-fi module separately? If so, what are some of the modules that are compatible with the evk?
    Dibyajyoti Ghosh
    last modified by Dibyajyoti Ghosh
  • i.MXRT1064 EVK PCB file

    Dear NXP Deam,   Kindly help me on this customer support.   We want to study the i.MXRT1064 EVK PCB file which is in Allegro tool. We want to open it in Altium, for that ASCII file generated from Allegro...
    BALASUBRAMANIAN M.S.
    last modified by BALASUBRAMANIAN M.S.
  • USB3.0 MSD may be ignored by i.MX8M.

    Dear CarlosCasillas,   We are developing products using i.MX8M. However, the product finally has one problem.   We developed on BSP 4.14.98_2.0.ga. Out board may ignore USB3.0 MSD to Port USB1 in most ca...
    George Fukutomi
    last modified by George Fukutomi
  • Linux BSP can suspend only one time.

    Hello community,   I'm trying to suspend/resume function with i.MX6Q SABRE-AI + base board. Using Linux BSP is a L4.19.35-1.1.0   In first time, it is success to suspend by following command and success t...
    Takayuki Ishii
    last modified by Takayuki Ishii
  • set-public-key AVB

    I am trying to set public key for board IMX8QuadXpus... Android Auto. Android P9.0.0_2.3.3_AUTO-ER  After i set random key for rpmb fastboot oem set-rpmb-random-key   I got error  AVB ReadVbmetaPub...
    Tam Nguyen
    last modified by Tam Nguyen
  • Spread Spectrum Enable in plug in with secure boot

    Hello Everyone,   I am trying to enable Spread Spectrum in our board which is running uboot version: U-Boot 2018.03-00038-g34c3d6bfa9-dirty and kernel version: 4.19.35-04790-ga5119fdf76b3-dirty also I ...
    Asma Alekar
    last modified by Asma Alekar
  • Usb UVC webcam gadget bulk transfer

    Hi, I'm developing a Linux camera and the output is uvc via the g_webcam gadget. For now I'm capable of 40fps with a resolution of 640x480 yuy2. I'm working with a imx7D   I'm capable of much higher fps on a cyp...
    Alexandre Caron
    last modified by Alexandre Caron
  • NXP's Secure boot variant for i.MX8M

    Hi All, it is going to be a bit long question as I'm putting the questions and observations I had.   I'm using i.MX8M EVK and trying to enable the secure boot feature on the same. After doing some study & se...
    Venkatasai Thotakura
    last modified by Venkatasai Thotakura
  • Where is the source code in built embedded linux distribution?

    I built image for imx8qxpmek evaluation board using Yocto Project.  Where is the source code that exactly matches this image ? I'm particularly interested in USB Subsystem.  This subsystem must be in u-boot...
    Amer Naseem
    last modified by Amer Naseem
  • Operate DAC in mkl27Z644, ( LQFP64)

    Operate DAC in mkl27Z644, ( LQFP64)   Hi, I have to operate PTE30 as DAC0_OUT, but without any success. Few general questions:   1) Did I need to operate the comparator ? what the input channle I configu...
    zvika grinberg
    last modified by zvika grinberg
  • P9.0.0_2.2.0-ga on imx6 getting hot and shutting down

    Hi,   Using i.MX Android™ P9.0.0_2.2.0-ga release on imx6. On running a graphics test app (GPUBenchmark3D), system is getting hot and shutting down. Is this a known issue? What could be the reason?  &...
    Sreejith S
    last modified by Sreejith S
  • IMX8QXP ELCDIF DVI mode with external sync signals

    Hi We have imx8qxp Soc with the off-chip hdmi converter (sii9022a). I'm trying to get picture using ELCDIF DVI mode ( i think problem is in embedded sync signal settins which is not yet clear for me. The question ...
    MIKHAIL Levitin
    last modified by MIKHAIL Levitin
  • i.mx8, ethernet mac features for AVB / 802.3 / 802.1Qav

    Hi,   In the i.MX 8M Mini Applications Processor Reference Manual, there is a bit of info around the "Ethernet MAC core", but I can't seem to find the details on some of the bullets listed. Would be great w...
    dav1
    last modified by dav1
  • Where are physical location of the memories in the pico-imx7D SOM?

    Hi,   I have pico-imx7d SOM and I need to know where are physical location of the memories:   Qjestion 01 : Where is this?   Qjestion 02 : Where is this?   Qjestion 03 : Where is this? ...
    NEUBER DE SOUSA
    last modified by NEUBER DE SOUSA