• NXP's Secure boot variant for i.MX8M

    Hi All, it is going to be a bit long question as I'm putting the questions and observations I had.   I'm using i.MX8M EVK and trying to enable the secure boot feature on the same. After doing some study & se...
    Venkatasai Thotakura
    last modified by Venkatasai Thotakura
  • Where is the source code in built embedded linux distribution?

    I built image for imx8qxpmek evaluation board using Yocto Project.  Where is the source code that exactly matches this image ? I'm particularly interested in USB Subsystem.  This subsystem must be in u-boot...
    Amer Naseem
    last modified by Amer Naseem
  • Operate DAC in mkl27Z644, ( LQFP64)

    Operate DAC in mkl27Z644, ( LQFP64)   Hi, I have to operate PTE30 as DAC0_OUT, but without any success. Few general questions:   1) Did I need to operate the comparator ? what the input channle I configu...
    zvika grinberg
    last modified by zvika grinberg
  • P9.0.0_2.2.0-ga on imx6 getting hot and shutting down

    Hi,   Using i.MX Android™ P9.0.0_2.2.0-ga release on imx6. On running a graphics test app (GPUBenchmark3D), system is getting hot and shutting down. Is this a known issue? What could be the reason?  &...
    Sreejith S
    last modified by Sreejith S
  • Usb UVC webcam gadget bulk transfer

    Hi, I'm developing a Linux camera and the output is uvc via the g_webcam gadget. For now I'm capable of 40fps with a resolution of 640x480 yuy2. I'm working with a imx7D   I'm capable of much higher fps on a cyp...
    Alexandre Caron
    last modified by Alexandre Caron
  • IMX8QXP ELCDIF DVI mode with external sync signals

    Hi We have imx8qxp Soc with the off-chip hdmi converter (sii9022a). I'm trying to get picture using ELCDIF DVI mode ( i think problem is in embedded sync signal settins which is not yet clear for me. The question ...
    MIKHAIL Levitin
    last modified by MIKHAIL Levitin
  • i.mx8, ethernet mac features for AVB / 802.3 / 802.1Qav

    Hi,   In the i.MX 8M Mini Applications Processor Reference Manual, there is a bit of info around the "Ethernet MAC core", but I can't seem to find the details on some of the bullets listed. Would be great w...
    dav1
    last modified by dav1
  • Where are physical location of the memories in the pico-imx7D SOM?

    Hi,   I have pico-imx7d SOM and I need to know where are physical location of the memories:   Qjestion 01 : Where is this?   Qjestion 02 : Where is this?   Qjestion 03 : Where is this? ...
    NEUBER DE SOUSA
    last modified by NEUBER DE SOUSA
  • i.MX 8M Secure Boot Procedure and OTP customization

    Hi Experts,   I am currently working in i.MX 8M based SOM and built a BSP for the same using Yocto Project.  Now I want add Secure Booting feature for i.MX 8M but most the document I am getting are confusin...
    Ashok Soundararajan
    last modified by Ashok Soundararajan
  • USB3.0 MSD may be ignored by i.MX8M.

    Dear CarlosCasillas,   We are developing products using i.MX8M. However, the product finally has one problem.   We developed on BSP 4.14.98_2.0.ga. Out board may ignore USB3.0 MSD to Port USB1 in most ca...
    George Fukutomi
    last modified by George Fukutomi
  • i.MX6Solox with EPD Display

    Hi,  I would like to interact with an EPD raw display, 4.7inch 800x600 pixel,  using i.MX6Solox SoC, NXP Part number = MCIMX6X1CVO08AB. The SoC has 24-bit display interface , but not EDP. Does NXP...
    Musadjan Alim
    last modified by Musadjan Alim
  • about bitbake fsl-image-validation-imx -c populate_sdk

    I get the following error when I create the SDK, the cmd line is : DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b imx8m_build/ bitbake fsl-image-validation-imx bitbake fsl-image-validation-...
    y yq
    last modified by y yq
  • i.MX8M Mini RoT

    Hi, I am using an i.MX8 Mini board, I wanted to know to which processor the RoT boot is controlled, the cortex-A or the cortex-M?   Thanks.
    Iñigo Vicente
    last modified by Iñigo Vicente
  • work with 3840x412 LCD

    Hi all!   I want to work with i.MX6 Quad with linux and LCD display with 412 vertical by 3840 horizontal pixel resolution. Does i.MX6 support it? Thanks!   Artur.
    Artur Null
    last modified by Artur Null
  • MFGTool Error when flashing a MX6SX 14x14 board with eMMC

    Hello all,   I'm trying to boot a board based on SABRESD design. The board had passed the memory test, but  mfgtools won't flash it.   Last error I can see in the log is 'Failed to Initialize memory!'...
    Victor Palacio
    last modified by Victor Palacio
  • MINISASTOCSI - MIPI-CSI Camera Module is not detecting in iMX8QM_MEK Board

    Hi,   I am working on Android 9 Automotive with IMX8QM-MEK. I needs to configure OV5640 MIPI CSI board (mini SAS). I enabled the following in kernel but still the camera is not detecting.   +CONFIG_IM...
    vinothkumar s
    last modified by vinothkumar s
  • How to activate IC resizer

    Hi to all, I'm trying to activate the resizer hardware of the i.mx6 Dual. I can't understand how to do that. I'm using kernel 4.9.11 and it's not possible for me to update it. So I'm trying to manipulate driver for ...
    Denis Matteazzi
    last modified by Denis Matteazzi
  • I.mx8mmini Error: imx-gpu-viv/imx-gpu-viv_6.2.4.p2.3-aarch64.bb:do_instal

     Hi,   Getting this below error how to resolve ERROR: imx-gpu-viv-1_6.2.4.p2.3-aarch64-r0 do_install: Function failed: do_install (log file is located at /home/santhosh/Desktop/imx-yocto-bsp/bld-xwayland/t...
    Santhosh Kumar
    created by Santhosh Kumar
  • imxvideoconvert_ipu Gstreamer plugin

    Dear all, I am using Variscite's DART-MX8M-MINI platform, running Yocto Sumo (i.e. sumo-fsl-4.14.98-mx8mm-v2.2) I would like to test some features that combines a prosperity algorithm with gstreamer elements. ...
    Nissim Beja
    last modified by Nissim Beja
  • How to use usb 2.0 and Type-c connectors at the same time on i.mx8mini

    Hello I used a USB hub on i.mx8mini to make 4 usb ports. By the way, if I use Type-c and usb 2.0 together, I don't know how to configure   i.mx8mini has two USB ports One used for FW download The other one will...
    Danny KIM
    last modified by Danny KIM