• i.MX53 (also i.MX6) PWM Glitches on Duty Cycle Change

    I'm using PWM on the i.MX53 as an LCD Backlight Driver control.   When the brightness is ramped up it all works fine. When it is ramped down there are glitches.   That happens a lot on old and cheap PWM ti...
    TomE
    last modified by TomE
  • HAB version on iMX8M mini

    Hello, I read on the HAB code signing Tool User's guide that there are 3 different versions of HAB, HAB3 , HAB4 and AHAB. I cannot see clearly on the iMX8M mini manuals which version is on this processor. Which it ...
    Antonio Santagiuliana
    last modified by Antonio Santagiuliana
  • I.MX8QXP Android P auto camera HAL3

    Dears,   If I want to used enable /imx/libcamera3 camera HAL3 code in OS,and used Max9286 to connect camera, how to I change the source code? I think now get video devices flow not proper for MAX9286 chip,log ...
    Xu Ji
    last modified by Xu Ji
  • Unstable work of 1Gbit ethernet on imx6

    Hello! I fased with trouble when copy file to imx6 device by scp in gigabit network. It continously prints in terminal "fec 2188000.ethernet eth0: rcv is not +last" and disappear from network. And it may hapene after...
    Maxim Kuk
    last modified by Maxim Kuk
  • I need optee_os support for Maaxboard in yocto project, any help?

    I have successful built yocto project image with the maaxboard company's kernel and u-boot code at here: https://www.element14.com/community/message/288659/l/re-how-can-i-build-an-image-for-the-maaxboard-myself#2...
    peter zhang
    last modified by peter zhang
  • Using I2C api in uboot with 7ulp

    Hi,    I am using uboot from official repository Aurora : uboot-imx - i.MX U-Boot  Tag : rel_imx_4.14.98_2.3.0   I am using the mx7ulp_10x10_arm2 defconfig.    I would ...
    Arthur LAMBERT
    last modified by Arthur LAMBERT
  • what is the i2cdump register values for working codec?

    Im using Imx6ulevk board,at present working on on-board wm8960 codec . wm896 codec is detected under i2cdetect, but when i check the i2cdump values for 0x1a , all register address having the value xx .Even  not ...
    Dhanush V
    created by Dhanush V
  • I.MX8QMAX - QT

    Hi I am trying too work on QT on I.MX8QMAX.. Is there Any guide /Manual document for cross compiling the QT code for I.MX8QMAX   Regards Santhosh
    Santhosh Kumar
    last modified by Santhosh Kumar
  • Close cameras error when use max9286 cameras on imx8qm Android P OS

    hi nxp , I found some errors when closing cameras that is openned at the same time on imx8qm platform with Android P OS. Please help me analysis  to resolve ,Thanks a lot for your reply. The error log as follw: ...
    yingjin yan
    created by yingjin yan
  • IMX8M mini application processor software support

    Hello,   Can anybody please provide me the Linux image, Boot code and drivers (complete software files and documentation) for the IMX8M mini-application processor (MIMX8MM6DVTLZAA).   Thanks 
    Mudassir R
    last modified by Mudassir R
  • android_O8.0.0_1.0.0 ncm

    Hi,friend Has imx6q supported cdc-NCM default on android O8.0.0_1.0.0? I can find relative ncm driver in kernel code, but can not find ncm support in device\fsl\imx6\etc\init.usb.rc. If not, are ther...
    贻才 林
    created by 贻才 林
  • i.Mx8Mini HABV4 Errors

    i.mx8 mini HABv4 I am trying to get HABv4 working on the HABv4 mini.  The system is running Android version 9 and is on the evaluation board.  I have followed the instructions using the User Guide :  ...
    Wendi Whitcomb
    last modified by Wendi Whitcomb
  • PCB Layout  MCIMX8M-EVK

    Hello, help me to convert pcb MCIMX8M-EVK from alegro to altium.
    vlad gorodovich
    last modified by vlad gorodovich
  • Flashing Build Image to eMMC without using SD card

    Hi Experts,   I am using i.MX 8M  SOM (nitrogen8M of Boundary Device), this SOM has only inbuilt eMMC chip as a memory device. I have checked steps to flash the image to eMMC of SOM, all of them suggesting ...
  • setting procedure of function allocation on each cores

    Dear Person in charge,   Now, we're developing our product based on i.MX 8M Mini (Linux on Cortex-A53 and RTOS on Cortex-M4) as bellow. - MIPI-DSI ( display indication ) on Cortex-A53 side - MIPI-CSI ( for cam...
    野田 周作
    last modified by 野田 周作
  • iMX8MP:  virtual channel support in CSI-2? i want to use isl79987

    Hello,   i can not fonud iMX8MP reference manual. Maybe it's because it's not on the market yet   - how can I filter out data of virtual channel 2?   - can i use isl79987 on iMX8P
    p nix
    last modified by p nix
  • repo sync error

    Hi,         I did "repo sync" o8.1.0.2.0.0.ga android source code, I got these error message repeatedly.         What can I do next? repo: warning: Python 2 is no longer...
    Kevin Li
    last modified by Kevin Li
  • Can not connect to git.freescale.com when trying to build yocto krogoth

    WARNING: firmware-imx-1_5.4-r0 do_fetch: Failed to fetch URL git://git.freescale.com/imx/imx-firmware.git;branch=master;destsuffix=/home/jenkins/tnAp6212/technexion/technexion.1/local_build/tmp/work/cortexa9hf-neon-mx...
    q x
    last modified by q x
  • HW platform to work on Android Automotive

    Hi, We are looking for a promising HW platform to work on Android Automotive. Have couple of queries on the same. 1) Does NXP have HW platform and support for Android Automotive(not Android Auto). Hope it i...
    Sarathy P
    last modified by Sarathy P
  • This is a question about the wifi / bt module information available in imx8qm mek.

    Hello. I would like to ask about the wifi / bt module. Is there a list of wifi / bt modules available for imx8qm? please answer about my question. Thank you.
    sujin kim
    last modified by sujin kim