kernel memory corruption in galcore under high load Hi everyone, I am encoutering an issue with what I suspect is a galcore crash. For testing purposes, I put an i.MX6 QuadPlus under high load (CPU, VPU and GPU). After a few seconds or minutes of this wor... Rebuild kernel and modules for i.MX8 MEK Hi, I'm using an imx8qxpmek devkit and the fsl-imx-xwayland distro. This is basically what I have done to build a new Yocto Warrior image: . /opt/poky/2.7.2/environment-setup-x86_64-pokysdk-linux ... Default state of i.mx6 GPIO Hi, What is the default state of i.mx6 GPIO, before the booting Regards Prev Ravanth IMX6DL LVDS+HDMI同显问题 BSP:4.1.15-1.2.0 Kernel:4.1.15 dts文件:BLTP01lvds_lvds_hdmi.dts、blt-p01-test.dtsi 当设置fb0为ldb的时候,lvds能正常显示1920x1080 当设置fb0为hdmi的时候,hdmi能正常显示1920x1080 但是就是不能同时显示,求指导 Qiang Li - Mpu Se mxcfb1: f... imx6ull custom board with eth0 down Hi, my custombord with IMX6ULL designed on EVK bases, has now the eth0 not working. This is the behaviours root@imx6ull14x14evk:~# ifdown eth0 root@imx6ull14x14evk:~# ifup eth0 Micrel KSZ8081 or KSZ80... How to reduce boot time on iMX6UL-evk ? Hi everyone, My name is Toan. Currently, I'm using iMX6UL-evk with kernel rev L4.14.98_2.0.0_ga. The boot time is approximate 30 seconds. And I wanna reduce this time to under 10 seconds. I tried to set boot delay t... QCA6174 bluetooth Validation with i.MX8QM MEK Android Pie Automotive Hi NXP Team, We are trying to validate the QCA6174 PCI module with i.MX8QM MEK platform and we are able to successfully test WiFI. But when we try to validate Bluetooth we are facing below issues. We have even tested... How to set IMX8MM colour space for G2D conversions The IMX8MM reference manual section on the G2D specifies support for BT.601 and BT.709 YUV to RGB color conversions, including the formulas used. How are these set as they are not exposed in the G2D API? ... IMX8QM uuu u-boot Failed hi sir, when i use uuu tool in windows to update android 9(which i compiled), there is one error happened at the beginning,log as follow: >uuu D:\uuu\Windows\uuu-android-mx8qm-mek-emmc.ls... Does i.MX8M support boot from QSPI? In i.MX8M reference manual revision 1. 1.6 says support boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet. 6.1 says support boot from SD/MMC and NAND flash. Which one is right? iMX8QM RAW12 Camera (AR0231) Hello everyone, I have a custom board with an iMX8 Quad Max and a max9286 deserializer. The OS is built with yocto starting from the release L4.14.98_2.0.0_ga. Using a sensor (AR0231) that outputs RAW12 pixels,... Adding QEMU Emulator Support in Android Dear NXP, I am working on Android 9. I needs to add ro.kernel.qemu support in Android 9. By default ro.kernel.qemu is false. std::unique_ptr<CommBase> CommFactory::creat... HOW to flash EMMC in imx7 with android image? hello all, i am working in custom board based on imx7 evaluation board by NXP, now i am trying to flash EMMC with an android image (i am using marshmallow with linux kernel version 4.1.15) i come across diffe... Can i use EIM for data transfer from FPGA? --------------------------------------------------------------------- Ubuntu 12.04 Kernel 3.14 Yocto system i.MX6DL sabresd board --------------------------------------------------------------------- Hi e... imx6ull burned image to nand by uuu Hello, I'm using the imx6ullevk board and L4.14.98_ga, and want to burn image to nand using uuu. I have change some parameters to ahieve uboot for nand & ubi rootfs. And as for imx6ullevk's "nand read", I set that... VPU encode on i.MX8 Hello, Does i.MX8 VPU encode support V4L2_Y12 format input source to make avi or mp4? use unit_test/V4L2_VPU/ or GSTL VPU used demo Thanks Memory issues with i.mx233 rev. B Hi, We're using custom-made SoM based on Olinuxino Micro design in our products. Couple of months ago we purchased the next small batch of SOCs. They turned out to be mcimx233cag4b , not mcimx233cag4c ... To Wigros Sun, 在iMX6DQ上使用USB TO ETHERNET 芯片同时扩展2个网络口可以吗 我们想在iMX6DQ的板子上,USB HOST1 上先用USB-HUB芯片扩展出4个USB口,再用2个USB TO ETHERNET芯片扩展两个网络口,这样可以吗,速度上会有影响吗 i.MX7ULP is it possible to access the PMU (Performance Monitoring Unit) interrupts? Hi, I'm trying to get perf recording working on the i.MX7ULP platform running linux 4.14.98-imx_4.14.98_2.0.0_ga but I'm not able to figure out how/or if it's possible to access the interrupts from the PMU by ... How to migrate form i.MX8QXP to i.MX8DX ? We currently developing a board with (i.MX8QXP + DDR3L16bit) and running Linux (L4.14.98_2.0.0). We plan to replace i.MX8QXP with i.MX8DX in the future, so we are starting software porting for i.MX8DX. The ...