• i.MX8 QuadXPlus chipset roadmap

    Hi. i.MX8 QuadXPlus chipset has been developed, so please contact us to know the schedule available. Please share if you have the latest (2020year) Roadmap related to i.MX8 QuadXPlus chipset.   Have a nice day.
    hwang jinha
    last modified by hwang jinha
  • about imx8mm on android9

    first、Our board is resigned by imx8mm evk,while some module chips had been removed. second、I flash images to sd card and boot from sd,the android kernel is stop here and not return [    5.202213] dm ...
    zhou wei
    last modified by zhou wei
  • Udoo Neo Full is loading imx6q-udoo-hdmi.dtb

    Hi Everyone! I'm newbie in linux system! After checking /sys/var/term.log, I saw linux OS of my udoo board, it load imx6q-udoo-hdmi.dtb and it dose not load any *.dtb file in /boot/dts folder. I tried to at this li...
    Anh Pham Tuan
    last modified by Anh Pham Tuan
  • Automatic configuration of ddr stress tool within uboot

    Hi,   We use the ddr stress tool via uboot as part of our QA process. It's manually driven and we would like to automate it. Is it possible to automatically configure it to run a preconfigured stress test via ub...
    joerutledge
    last modified by joerutledge
  • How to identify display on imx8qxp

    As imx8qxp can driver more displays(DSI0, DSI1 and LCDIF),  How to identify display in application while all these display drived ? thanks. our test environment is L4.14.98_2.3.0_images_MX8QXPMEK(rootfs is&...
    Ping Wu
    last modified by Ping Wu
  • imx8mm evk HABv4 problem

    Dear nxp     use   i.MX_Android_Security_User_Guide.pdf documents verification 8mm HABv4 Funtion,the motherboard cannot start or burn. What caused this problem. Have you encountered such a pr...
    Aber fu
    last modified by Aber fu
  • i.MX8M EVK MIPI CSI Camera Frame Rate

    Hello, We have purchased NXP MIPI-CSI camera MINISASTOCSI kit and followed the instructions in this application note https://www.nxp.com/docs/en/application-note/AN12187.pdf  to test the camera on NXP i.MX8M EVK...
    Felix Radensky
    last modified by Felix Radensky
  • error: expression .... ->CCM_Type::ROOT[0].CCM_Type::<unnamed struct>::TARGET_ROOT' has side-effects    kCLOCK_RootM4_1 = (uint32_t)(&((CCM_Type*) ... ->ROOT[0].TARGET_ROOT),

    The solution to this problem is to use the offsetof, review this single line in the fsl_clock.h that needs propagated for both enums that use the CCM macro and all their entries.      /*! @brief ccm ro...
    Thomas Orsi
    last modified by Thomas Orsi
  • How to access to the top address of OCRAM for i.MX8QXP

    Hello,   From RM (IMX8DQXPRM_Rev.0.pdf)     OCRAM is mapped to address of 0x100000 to 0x13FFFF. But, I could not access to address range from 0x100000 to 0x117FFF by u-boot prompt. Can w...
    Kazuma Sasaki
    last modified by Kazuma Sasaki
  • onnxruntime fetch fail

    Hi All Right now ,i am try to build the new yocto bsp 4.19.35 to generate the eiq for our algorithm development , but i encouter the issue showed below .   bitbake imx-image-full     WARNING: onnxrun...
    King Liu
    last modified by King Liu
  • i.MX8 MM Not detected eMMC Slot

    hi communicators.   I have one specific question plz help...   - My NXP Board Description Picture:    i.MX 8M Mini ----------------------------------------------------------------------------...
    lim eon
    last modified by lim eon
  • Want old design data for i.MX6Q-SDB

    Hi all, I am using i.MX6Q to check S/W operation for my customer. Unfortunately I have only an old revision (SCH-27516 Rev.B3) board in my hand. Please provide design data for this revision to someone.   BR, ...
    George Fukutomi
    created by George Fukutomi
  • Application Layer: IMX8MQ to IMX8MQ communication using PCIe cross-link

    Hi NXP Team,   We have gone through the reference of the below link: i.MX6Q PCIe EP/RC Validation System    In our end application we want to establish full-duplex communication between two ...
    Harshit Shah
    last modified by Harshit Shah
  • PMIC read error | imx6q sabreAI

    Hi All, I am working on imx6q based sabre AI custom board, running android 7.1.Everything works fine on our first version but in our latest version of our custom board,it is showing PMIC read and write error and boot...
    RICHU C J
    last modified by RICHU C J
  • Imx6ull buildroot flash with mfgtool

    Hi,   I have custom imx6ull board and I need to flash nand with buildroot. I think that better is to flash device to SD card via mfgtool before try to boot to nand version.   I have two boards. One with n...
    Janne Terho
    last modified by Janne Terho
  • Problems with imx7d overlay setting rgb565 mode?

    Hello everyone On imx7d, I successfully enabled the overlay layer, and my screen resolution is 720x1280. And when bits-per-pixel = <32>, everything looks good except for screen jitter. Later I set bits-per-pixel...
    其东 刘
    last modified by 其东 刘
  • i.MX8QXP+MAX9286

    Now,our customer is use i.MX8QXP L4.14.98 +SerDes MAX9286+MAX96705+Sensor AR1043 as Sourding 360 solution. MAX9286 and MAX96705 should be found and initial is ok.But:  Error:write reg error:reg=0x3024,val=0x1. ...
    George Li
    last modified by George Li
  • imx8mm worrior build fails on busybox

    hi We are upgrading our BSP to the worrior on the imx8m-mini but when i build with fsl-image-qt5 the busybox fails.  Value of CONFIG_SH_IS_NONE is redefined by fragment .config.app.suid: | Previous value: # CON...
    ran gree
    last modified by ran gree
  • I can't find i.MX 8QuadMax / QuadPlus register Manual on Nxp website

    Hello, everyone   I can't find i.MX 8QuardMax / QuadPlus  register manual on nxp website
    William Gou
    last modified by William Gou
  • iMX8QXP Bare metal Cortex m4 cache initialization

    Hi,    I'm currently working on a baremetal application on the M4 inside the i.MX8QXP and I'm having issues activating the cache. I would like to make sure I'm not missing any steps. I based my configu...
    David Binet
    last modified by David Binet