• U-boot DDR init files to FreeRTOS sdk

    Hello I am a student at Grand Valley State University. Me and 2 other students are trying to work with the nxp i.mx8m nano evaluation board. We are currently only using the base SDK and FreeRTOS. Currently we are tryi...
    William Mckeever
    last modified by William Mckeever
  • imx6q yocto环境搭建

    我选择$ DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build 然后 $ bitbake fsl-image-qt5 在编译中途出错,就停止了   试过取消,再编译,还是这样子,不知道怎么解决
    jin zou
    last modified by jin zou
  • Bluetooth: Receiving files failure

    Hi, I am using imx7d processor interfaced with the wifi/bluetooth module wl1831.  I need to transfer files between a the board and a phone. Pairing and connection to the phone is working well using  bluetoot...
    Blessy Abraham
    last modified by Blessy Abraham
  • Parallel RGB driver is not worked on i.MX8QXP MEK board

    Hello experts, In order test imx8qxp parallel RGB LCD Interface, I download  L4.14.98_2.3.0_images_MX8QXPMEK.zip from nxp site and test it on imx8qxp mek board as below steps: 1. hw board:  imx8q...
    Ping Wu
    last modified by Ping Wu
  • Temperature monitor of iMX6UL doesn't work as expected

    Hi Yuri,   Temperature monitor of IMX6UL doesn't work as expected  Our engineering team has a question for this, but Ethan has leave for a long time. Could you provide the patch for us? And we need try t...
    SHIH-CHIEH CHOU
    last modified by SHIH-CHIEH CHOU
  • Question about max9286

    I have some problems. Now I am using max9286 + max96705 + ov10635 to debug the camera, but now there are two problems that prevent me from solving it: 1. There will always be the phenomenon that the camera cannot...
    Cocoin K
    last modified by Cocoin K
  • Temperature monitor of IMX6UL doesn't work as expected

    We now have the use of i.MX6UL on our products. According to the Security Reference Manual, low-temperature monitor should assert between -40 and -20 degree. However we found that some units will start to have the t...
    Ethan Yang
    last modified by Ethan Yang
  • Debian packages on imx8m mini evk linux image

    Hello everyone,   I have been stuck for days. I couldn't install debian packages using apt-get. Even I added the apt-get command in the linux image, I couldn't install any of the packages. I want to install s...
    chayma hajjem
    last modified by chayma hajjem
  • the whole system hang on when imx8qm m40 watchdog triggered

    I use below cmmand to run my m40 appliction 1. insmod ./m4ctrl_dev.ko 2. ./m4ctrl --deploy=./m4_0.bin --core=0   My m40 application code: #ifdef __cplusplus extern "C"{ #endif /*!  * @brief WDOG0 IRQ handl...
    974782852@qq.com
    last modified by 974782852@qq.com
  • 主流MCU参数对比

    我想了解我们的LPC55S69,K32L2B3,IMXRT1050跟其他主流厂家(ST,TI,华大)的参数性能对比图?
    Flex Chen
    last modified by Flex Chen
  • Correct register value for RAW12 data reception

    Hello, I want to receive RAW12 image data with MIPI-CSI and set the data to FB1 and FB2 with DMA of CSI Bridge. However, I don't know the proper register settings for MIPI-CSI and CSI Bridge for RAW12. 1.TWO_8BIT_SEN...
    Tetsuya Sugiyama
    last modified by Tetsuya Sugiyama
  • i.MX8MQ PCIe Tx and Rx Swapping

    Hi NXP Team,   We are working for communication between two i.MX8MQ processors using the PCIe link. For the same, we are planning to do below connections from the hardware.    To support the above c...
    Harshit Shah
    last modified by Harshit Shah
  • Power Mode Switch Application in IMX8QM-MEK

    Hi All,   I done the following for build the power_mode_switch demo application with Arm Cortex-M4 on IMX8QM-MEK. power_mode_switch demo application is running but android is not booting.   diff --git a/mc...
    vinothkumar s
    created by vinothkumar s
  • how to encrypt rootfs in imx8mq?

    Hi, We are working on imx8mq and we have the requirement of the encrypted boot. So what are the steps to encrypt the rootfs for imx8mq?   Thanks, Nilesh Patel
    Nilesh Patel
    created by Nilesh Patel
  • i2c communication in uboot

    Hi,   I have an LCD module. I would like to initialize the LCD from uboot over i2c. I'm using imx6ull based custom board.   Are there any existing solutions available to do that? If not, how I can get the...
    mathew_k_t
    last modified by mathew_k_t
  • Device not wakeup after suspend

    I have useing IMX8M som with custom carrier board. When the device goes to suspend or lock mode when the power button is pressed, its not able to resume on a power button press. The CPUs are going to shutdown mode and...
    vimal mano
    last modified by vimal mano
  • openocd JTAG  with the iMX 8M Mini EVK.

    I'm trying to get openocd JTAG running with the iMX 8M Mini EVK. Couldn't find a proper JTAG cfg file so I made one from a imx 8Mq I found,   nxp_mcimx8m-evk.cfg File # # configuration file for NXP MC-IMX8M-EV...
    Wes Philbrook
    last modified by Wes Philbrook
  • Is it able to use mfgtool v2 in kernel 5.4?

    Hi guys,   I have doing to job to upgrade from kernel 4.1.14 to kernel 5.4. I did use mfgtool v2 in kernel 4.1.14, and I am trying to use mfg tool v2 in kernel 5.4. Should I modify kernel or uboot configuration...
    Yibeom Han
    last modified by Yibeom Han
  • i.MX8M Mini error

    Hi,Sir I got the error on the i.MX8M Mini, any adrise for the error?TKs!
    George Li
    last modified by George Li
  • Want old design data for i.MX6Q-SDB

    Hi all, I am using i.MX6Q to check S/W operation for my customer. Unfortunately I have only an old revision (SCH-27516 Rev.B3) board in my hand. Please provide design data for this revision to someone.   BR, ...
    George Fukutomi
    last modified by George Fukutomi