• usb1-1 wlxd4ca6ea21080:renamed from uap0

    hi:    imx6D is communicated with LilY-W31, when i load xxx.ko of wifi,uap0 is renamed for wlxd4ca6ea21080,I should resolve this problem
    1 1
    last modified by 1 1
  • GYRO and GSM driver integration for IMX8QM-MEK Arm Cortex M4 Platform

    Hi All,   Is there any available source code for GYRO sensor and GSM  for Arm Cortex-M4 core for IMX8QM-MEK platform.     Thanks & Regards, Vinoth S,
    vinothkumar s
    last modified by vinothkumar s
  • MX8M GPIO Input_Val Setting conflict for i2c2

    Hello,   I am currently using yocto for the VAR-SOM-MX8M-MINI which uses the freescale imx8mm-var-som.dts file.  In this file, the I2C2 SDA and SCL signals are defined with an input_val of 0x400001c3.&...
    Matthew Mader
    last modified by Matthew Mader
  • Android Verified Boot 2.0 support on imx6

    Hi, We are using imx6dl which runs on Android 8.0.0 Oreo and Linux kernel 4.9.17. My doubt is, in this release Android Verified Boot 2.0 support is available or not?
    Prasanna Kulkarni
    last modified by Prasanna Kulkarni
  • Custom boot.img with android_p9.0.0_2.3.0

    Hello! We're attempting to create a custom boot image alongside other pre-made image files for a custom Android build. Currently, we're using the IMX8mm EVK for development and separate hardware that we've written c...
    Dylan Johnson
    last modified by Dylan Johnson
  • how to change Launcher 2 into launcher3 in android-5.1

    android 5.1 default launcher is 2, how i can change it into launcher 3?
    liang yan
    last modified by liang yan
  • Yocto imx8m tensorflow-lite

    I would like to build C++ code and use tensorflow as a library. What do I have to ad to the Yocto image recipe to have header and required libs in SDK?  For the rootfs it seems that IMAGE_INSTALL += "...
    Arno Steffens
    last modified by Arno Steffens
  • The results I get using GPU (UMAT) are worse than on CPU(MAT)

    I'm trying to compare the performance of OpeCV algorithms on CPU and on GPU using OpenCL capabilities on the IMX8M.The results I get using GPU (UMAT) are worse than on CPU(MAT). I was checking the gputop and top ...
    Truman Burbank
    last modified by Truman Burbank
  • Booting sequence of IMX8QM-MEK

    Dear NXP,   Will you please give me the short notes for booting sequence of IMX8QM-MEK with Arm Cortex-M4.   Some times resources (Display and Camera)  are occupied by Arm Cortex-M4     ...
    vinothkumar s
    created by vinothkumar s
  • Failed to upgrade with update.zip

    We're running on IMX8mini, Android9.0, 8G EMMC, flash partition with partition-table-7GB.img, and I can build out the OTA file, update.zip.   And I've verified this .zip file with update_device.py scri...
    Yang Songxiang
    last modified by Yang Songxiang
  • i.MX GPIO PU/PD/keeper admittable configurations

    Hi all,   I wrote this question to try to summarize things on official documentation and to get an explanation about the topic GPIO PU/PD/keeper admittable configurations, for GPIO output and input configuration...
    Mauro Salvini
    last modified by Mauro Salvini
  • i.MX6DL boot hang on 4.9.88 or 4.14 kernel with latest galcore.ko

    Hi:   I test the customized board which has  i.MX6DL and i.MX6Q CPU on imx_4.9.88_2.0.0_ga and imx_4.14.98_2.0.0_ga.   The i.MX6DL kernel hang when insmod the galcore.ko (6.2.4.p1.8 with 4.9 kernel, 6...
    YenChin Lee
    last modified by YenChin Lee
  • i.MX8M Mini GPIO timing question

    Hi,   at the reset state all GPIO will be in input mode, what will be the delay from reset state to configuration, for a GPIO on the 3.3V domain, let say I need to configure a GPIO in output and set a specific l...
    Martin Bernier
    last modified by Martin Bernier
  • Parallel RGB driver is not worked on i.MX8QXP MEK board

    Hello experts, In order test imx8qxp parallel RGB LCD Interface, I download  L4.14.98_2.3.0_images_MX8QXPMEK.zip from nxp site and test it on imx8qxp mek board as below steps: 1. hw board:  imx8q...
    Ping Wu
    last modified by Ping Wu
  • OpenCV Build imx8mmevk

    Hello,   I'm trying build using bitbake imx-image-multimedia, build configuration:   Build Configuration: BB_VERSION = "1.44.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-18.04" TARGET_SYS = "aarc...
    Uri Madmon
    last modified by Uri Madmon
  • iMX6Q Yocto version for optimal graphical performance

    Hi   I got an iMX6Q board. Specifically this one: i.MX 6Quad SABRE Development Board | NXP    I have been using the zeus branch of meta-freescale, and thereby using the 4.9 kernel including the vivan...
    Christian Sørensen
    last modified by Christian Sørensen
  • How to get slave details of a module connected to imx6q over SPI?

    Hi,   I'm using imx6q reference board with yocto BSP.   I've configured the dts as: &ecspi1 { fsl,spi-num-chipselects = <1>; cs-gpios = <&gpio4 9 0>; pinctrl-names = "default"; pi...
    Sujay S
    last modified by Sujay S
  • Design files for i.MX 8 Multisensory Enablement Kit (MEK)

    Hi NXP Community Could you please email me the allegro files for i.MX 8 Multisensory Enablement Kit (MEK) because it is not available in the website, My email: calibronic@yahoo.com    with regards, Saei...
    saeid fallah
    last modified by saeid fallah
  • Secure boot issue with HAB_INV_ADDRESS for i.MX6DL custom board

    Hi All,   We have an i.MX6DL custom board with the following information:    CPU:   Freescale i.MX6DL rev1.2 at 792 MHz    U-Boot 2017.11-imx6dl   Now we want to a...
    Shunnian Zhai
    last modified by Shunnian Zhai
  • encrypt and decrpt kernel Image, dtb, intramfs

    Hello everybody,    I'm looking for a solution to my problem, I'm working on imx8M and I have a secure u-boot that is capable to authenticate the signature of the kernel.    I want to ...
    Manjunath Basappa Bentur
    last modified by Manjunath Basappa Bentur