• IOMUX sheet for imx7ulp

    Hello,   I have been trying to find iomux sheet for imx7ulp but I could not find anywhere in the NXP website. Can anyone please share me the link for the same ?   Thanks, Jai Ganesh Sridharan
    jai ganesh sridharan
    last modified by jai ganesh sridharan
  • How to get periodic scheduled tasks (on the order of 10us)?

    Hello!   I've got the i.MX 8m Mini EVK, and for my application, I need to be able to schedule periodic tasks, with triggers on the order of 10s of microseconds. Now I realize that since the timing is short, and ...
    Stephen Eng
    last modified by Stephen Eng
  • Can't Build L4.14.78_1.0.0 for i.MX 8M Mini EVK?

    I would like to rebuild the 4.14.78_1.0.0 Yocto Linux image for my i.MX 8M Mini EVK. The reason is I could go and make custom changes as needed for my application. I know that the current Linux image that I have on my...
    Stephen Eng
    last modified by Stephen Eng
  • can not run chromium-x11 with myuser user in xwayland on imx8 maaxboard (imx8mqevk)

    Hi  my yocto image I built works well in  imx8 maaxboard porting from imx8mqevk. in root user: chromium --no-sandbox  it works. but I use another user myuser, it can start up: error output as...
    peter zhang
    last modified by peter zhang
  • iMX8M Mini / IoT Core: power management support?

    Greetings, we're evaluating power management capabilities of NXP's Windows 10 IoT Core BSP for iMX8 Mini EVK (W1860_1_0_1_IMX-IOTCORE-B191011). Power management is claimed to be supported, but powercfg reports on...
    Gennady Kuznetsov
    last modified by Gennady Kuznetsov
  • How can I reduce the number of parallel yocto builds?

    I am trying to build an image on a machine with only 8 GB of RAM. It seems setting PARALLEL_MAKE and BB_NUMBER_THREADS should allow reducing the concurrently run builds. Where do these settings fit in the NXP build pr...
    Jonah Firchilt
    last modified by Jonah Firchilt
  • ConfigTools problem with I2S

    I am having trouble setting up an I2S peripheral in ConfigTools/Peripherals for iMX RT1020.   The ADC is I2S format, ADC is the source for all I2S clocks, L and R channel, 24 bits packed in 32 bit word, sample r...
    Graham Haddock
    last modified by Graham Haddock
  • onnxruntime fetch fail

    Hi All Right now ,i am try to build the new yocto bsp 4.19.35 to generate the eiq for our algorithm development , but i encouter the issue showed below .   bitbake imx-image-full     WARNING: onnxrun...
    King Liu
    last modified by King Liu
  • about how to flash android images to sd card?

    first:our board usb typec device is not work well ,so i want,Is there anyways to flash android images to sd card without board?
    zhou wei
    last modified by zhou wei
  • Broken HDMI-Audio on i.MX6

    Hello   Starting with the release 4.14.98-2.3.0 HDMI-Audio stopped working on our i.MX6 boards. Investigations resulted, that this patch breaks it:   MLK-22713-1 dmaengine: sdma: drop dma_pool_alloc for BD...
  • 8MMINILPD4-CPU Schematics

    Hi ,     can i get 8MMINILPD4-CPU board schematics in pdf format?
    Jois Srinidhi
    last modified by Jois Srinidhi
  • Issue building IOT Core for NXP imx8m mini

    I'm trying to build a BSP for a NXP IMX8M mini I've followed the users guide and installed VS 2017 along with the 1809 rev of the ADK and WDK, I've run the setupcertificate.bat and all of this happens in administrativ...
    William Dunkley
    last modified by William Dunkley
  • Autosar with Imx8/Imx6

    Hello Team,    I am planning to use the Imx8/Imx6 for integrating the Autosar. Could you kindly let me know on how to proceed with this. If i purchase the development board, will this come with the Autosar...
    Naveen B
    last modified by Naveen B
  • USB_HostEhciTaskFunction hangs in USB_HostEhciPortChange

    I'm using the MCUXpresso SDK USB version 2.2.1 with MCUXpresso SDK 2.6.2. Disconnect a device sometimes causes the host task (USB_HostEhciTaskFunction) to hang in USB_HostEhciPortChange. The break condition is never s...
    Jeffery Thompson
    last modified by Jeffery Thompson
  • iMX6 LVDS -24 bit mapping

    Hi, I am not clear about the 24 bit SPWG/PSWG/VESA  data mapping given in imx6 technical reference manual section 39.5.2. In below table 39.6, R6,G6,B6 represents LSB color bit  or 6th color bits ...
    Tamilarasan E
    last modified by Tamilarasan E
  • Can I burn eFuses for iMX8M Mini family using direct register access via JTAG?

    Hello,   I have a similar question as in https://community.nxp.com/thread/499677 .   We have programmed some of the eFuses (a.o. Boot cfg., MAC addresses) of various iMX6 devices with direct OCOTP_CTRL re...
    Stefan Konrad
    last modified by Stefan Konrad
  • Android P9.0.0_2.2.0-ga booting issue with i.MX6 Solo

    Hi community,   Has anyone ever booted in 6Solo mode with i.MX6DL SABER-SD? I am trying to boot android p9 as i.MX6Solo mode using i.MX6DL SABRE-SD board. But  after booting u-boot, kernel don't boot-up a...
    Mamoru Kanou
    last modified by Mamoru Kanou
  • fsl-image-validation-imx-1.0-r0 do_rootfs: Could not invoke dnf

    Hello experts,   I'm building the fsl-image-validation-imx image using fsl-yocto-L4.9.123_2.3.0_mx8mm under Ubuntu-16.04 :   $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-li...
    Khang Le Truong
    last modified by Khang Le Truong
  • How to enter SNVS mode by SW on imx7d?

    Hi!   According to "i.MX 7Dual Applications Processor Reference Manual, Rev. 1, 01/2018"  part 5.1.4.4 "Power Modes" there are two ways to enter "SNVS" mode  from "RUN" mode: ONOFF long press, or SW. ...
    Pawel Lenkow
    last modified by Pawel Lenkow
  • Command Line utility command for MFGtool2  to display the result and exit the command prompt.

     I am using the MCIMX6Y2DVM microcontroller in my testing board, I am programming this controller manually using MFGtool2.exe. I want to automate the programming for my project. I am using LabVIEW an industrial a...
    M Harishankaran
    last modified by M Harishankaran