Skip navigationLog in to follow, share, and participate in this community. Hello everyone , I am working on imx6 solo sabresd board i had sucessfully completed booting uboot,zimage,dtb file and rootfs through sd card.. Present i want to boot through ... Booting through Emmc on Imx6 solo sabresd
BackIt seems my only two options to get 8GB of RAM is either connect 8x 8gb (1GB) DDR3/3L ICs or I was thinking I can just connect to a SODIMM module. If I get a non-ecc module all of the connections seem to make sense an... I'm trying to build OpenCV for iMX6 dual lite. The following procedure is used as a reference. Is this procedure valid for iMX6 dual lite? http://imxcv.blogspot.com/2014/02/building-opencv-24x-for-freescales-i... Build OpenCV on iMX6 dual lite.
BackI'm trying to build OpenCV on iMX6 Dual Lite. The following procedure is used as a reference. Is this procedure valid for iMX6 dual lite? http://imxcv.blogspot.com/2014/02/building-opencv-24x-for-freescales-im... OpenCV build on iMX6 Dual Lite
BackiMX6DQ主板测试时我们用MfgTool2工具,通过拨码开关设置BOOT_MODE0和BOOT_MODE1,下载Linux系统,进行调试的,如果后期我们批量生产时,也用这种方法吗? To Wigros Sun, iMX6DQ板子批量生产时,烧录Linux系统一般有什么方法?
BackDear NXP, I'm running android 9 automotive on imx8qm mek board. In my project, I need to display a logo in u-boot. How can I do it, and keep the logo untill android bootanimation start? Thanks. Hi, I am currently working with Yocto project with warrior branch. I have generated the core-image-base and i am successfully able flash binaries using sdcard. But i want to flash binaries using USB . I have find to... How to Flash *.wic.gz fromat binaries on IMX6 Solo using USB OTG
BackHi, i'm trying to test the XOpenDisplay and other related to X11 functions. I'm using custom board based on IMX6Q and the display is cvbs(interlaced). And i'm using yocto image fsl-imx-x11. However, when i e... Is there any constraints to use cvbs(interlaced) monitor in imx6q X11?
BackNVCC_DRAM is 1.35V . i.MX6 solo is input range of the NVCC_DRAM 1.283V to 1.450V. Due to Output transient response, NVCC_DRAM will be less than 1.283V between 20us and 40us. When using MMPF0100(SW3B) The output vol... Output transient response
BackI have an IMX6ULL EVM board, and this is my EVM kernel info ID="fsl-imx-xwayland" ... How can I Turn on the usb uvc camera and sendout the stream through internet
BackWe want to upgrade from i.MX6 DualLite to i.MX6 QuadPlus. In i.MX6DL, we used i.MX Yocto Project BSP with imx-4.1.15-2.1.0. In i.MX6QP, we also used the same setting. We built image in the following commands... Failed to use MfgTool for i.MX6 with Yocto Project
BackUsing the TSC driver with Linux, we see a behavior of the 4W resistive touch which happens on any kind of connected 4W RTP (Resistive Touch Panel), independent of the size and form-factor. Basically, this is th... iMX6UL TSC (Resistive Touch Interface) Problem
Back你好, 在imx8qxp-mek上的MIPI-CSI链接一个sensor接收的是2clock/pixel的yuv422_8_8数据格式的数据源,图像尺寸设定为1920*1080,但显示出的尺寸为960*1080,且显示图像为带有深浅的绿色剪影,反色显示,不丢帧,如下图 使用的命令为:gst-launch-1.0 v4l2src device=/dev/video0 ! 'video/x-raw,formate=YV12,w... imx8是否设置2clock/pix模式存放sensor传来的数据
BackWhether using UART5 creates issue in HID detection in mfg tool? Is it mandatory to use uart 1/2 as debug console ? Hi, I am using imx7d processor interfaced with the wifi/bluetooth module wl1831. I need to transfer files between a the board and a phone. Pairing and connection to the phone is working well using bluetoot... Bluetooth: Receiving files failure
BackHi All. What should I do to modify the amount of CL_DEVICE_GLOBAL_MEM_SIZE? I am trying to use Darknet_On_OpenCL(using yolov3-tiny.cfg and yolov3-tiny.weights) on i.mx8mq. but I got this error after executing ... What should I do to modify the amount of CL_DEVICE_GLOBAL_MEM_SIZE on i.mx8mq?
BackI am using IMX7 Dual SABRE Board. I've built the Yocto project and booted through the SD card. The board has booted fine and everything is working as expected. I want to interface an I2C device with a slave addre... I want to know the different of performance bettween SAI1 and SAI3. As i know the SAI1 from M4 and SAI3 from A53.So can I use the SAI3 to send the music to the audio ca... ask for audio and audio card
BackHi, Kernel prints are not coming while booting Linux 4.1.15 on custom imx6ull board. I am using UART 8 as my debug port, related to that I have done configuration in boot arguments at U-boot, Kernel and roo... Kernel prints are not coming while booting in custom imx6ull
BackHi, I have dart mx6 with evaluation board and custom adv7180 board. I want to connect them together to get analog video input to record using gstreamer. I'm using Debian R02(kernel 4.9.88), looks like adv7180 kernel m...