• USB3.0 device mode speed in IMX8X

    Hi,   We are working with IMX8X based device , where the device will act as a webcam and using the USB3.0 port. The device is now getting detected as a  super speed uvc gadget device. We have the requiremen...
    ros M
    last modified by ros M
  • 5.4.3 Linux version  run jh_mmcboot issue

    Now I used 5.4.3 Linux + imx8mq board, and I would like to boot the jailhouse root cell, when I run jh_mmcboot in u-boot, it hang at rootfs with sd card as blew: It seems the sd card issue, but I have modify any co...
    Hongxing Yu
    last modified by Hongxing Yu
  • helloworld no print on imx8qxp-mek

    硬件:imx8qxpC0-mek 软件:起初使用的l4.14.98_2.0.0的yocto编译出的rootfs.sdcard烧写到SD卡上,后来用l4.14.98_2.3.0:uboot,scfw,atf,kernel-image都是统一版本编译的并替换掉原来的flash.bin和image&dtb hello.c: #include<stdio.h> int main(){   ...
    peterson hou
    last modified by peterson hou
  • i.MX6ULL EVK design questions

    In the page 10 of SPF-29364_A1.pdf, There is an MOSFET Q707 and gate pin connected with signal named DISCHG_EN. 1. What is function of Q707? 2. Can customer remove Q707 on their board? 3. Any side ef...
    m.c
    last modified by m.c
  • IMX8MQuad audio codec

    Hi to All,   I am new in this IMX8MQuad processor. We have an EVK for this IMX8MQuad. If we check audio part, audio codec is not working. But when we tried with hdmi audio its working fine. we checked the fo...
    prathap ponnuchamy
    last modified by prathap ponnuchamy
  • Running Ubuntu BSP on 8MMINILPD4-EVK

    Hi All,   I have 8MMINILPD4-EVK running Android image. But I am planing to run Ubuntu BSP on it. There is no information available on NXP site for it. Where as many NXP vendors support Ubuntu.   Will...
    Prashant Chopade
    last modified by Prashant Chopade
  • helloworld recipe using autotools

    Hello all,   Below is the recipe given by poky documentation in reference manual and i am not able to bitbake. ***************************************************************************************************...
    Manjunath Joshi
    last modified by Manjunath Joshi
  • Cannot capture video or image for SBGGR12_1X12 format with Pico DCAM20 Camera Module

    Hi, Currenty I am working on i.MX8M Nano with Camera module Pico DCAM20 (2 lanes). To add support for this driver, I added the driver file addi903x.c as attachment. Mark , the addi903x need 2 lanes 135Mhz mipi cl...
    Michael Tong
    last modified by Michael Tong
  • why the Flexcan can't be set bitrate with 5000bps

    Hello, is there someone can help me ?    I get some problems when development with imx6ul processer, that i can't set the bitrate with 5000bps;   what i have done: 1. ifconfig can0 down...
    mio zhang
    last modified by mio zhang
  • Android USB Camera - How is it tested?

    I'm running Android P (2.3.4) on iMX8MQ and trying to use an external USB camera. I haven't seen anything that implements the Camera2 external camera config (External USB Cameras  |  Android Open Source Proj...
    Michael Brooks
    last modified by Michael Brooks
  • Where can we find the USB Certification Guide for i.MX8M Mini?

    Where can we find the USB Certification Guide for i.MX8M Mini like below? https://community.nxp.com/docs/DOC-105609 https://community.nxp.com/docs/DOC-333262
    m.c
    last modified by m.c
  • Does IMX8MM support WQHD?

    Hi Community.   I set a 2400x480 display to panel-simple.c with IMX8MM, I am getting the following error.   [ 0.000000] Kernel command line: console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 root=...
    Takashi Kashiwagi
    last modified by Takashi Kashiwagi
  • Can anyone explain how and where display is configured in windows 10 IoT for imx8mq ?

    In imx-iotcore\driver\video\imxdod directory, I found display driver which has code related to HDMI for imx8mq and MIPI DSI, LCDIF for imx8mm. But the driver seems incomplete as there is no code for DCSS for imx8...
    Abhishek H
    last modified by Abhishek H
  • DDR4

    hi,         My chip is i.MX8M MINI, I replaced DDR, use 4GB ram, uboot will get stuck every time.       1.     I used mscale_ddr_tool_v310 to test,     &...
    扬 杨
    last modified by 扬 杨
  • IMX6 Fast Boot

    Hello I am using Linux 4.1.15 on IMX6 and need to have a faster boot time.   Unit spends 12 seconds waiting for random number entropy. ie 'non blocking pool initialisation'.   Is there a way to disable, po...
    Ian Fox
    last modified by Ian Fox
  • Cannot wake from deep sleep on imx8m (Google Coral dev board)

    Hi,   I'm using the Google Coral Dev Board (i.mx8m SoC) running BalenaOS , and I'm trying to wake the board from deep sleep.   I'm entering deep sleep using   echo mem > /sys/power/state   I...
  • i.MX 8M Nano - Enable .NET Core on Yocto Linux

    Hello team,   I have customers how are trying to Enable .NET Core on Yocto Linux. .NET core it's a runtime for C# programs, mainly works on Debian Distribute, please refer to Install .NET Core an...
    Shai Berman
    last modified by Shai Berman
  • CST 3.3.0 returns Undefined error

    Hello, I am trying to setup secure boot on my iMX8MM device I end up with an error with cst tool versio 3.3.0 : Error: Cannot open key file CSF1_1_sha256_4096_65537_v3_usr_key.pem 140578450752768:error:06065064:dig...
    AURELIEN BOUIN
    last modified by AURELIEN BOUIN
  • HAB authentication Faild

    I upload signed uboot image to device, program SRK and closed the device with trustfence. After boot I get error:   Loading file 'boot.scr' to addr 0x8000000... Done    Autenticating image from DDR ...
    Adrian Dusinski
    last modified by Adrian Dusinski
  • Using cst-tools signing *.out file

    Hi,   I am using sbc connect core 6 board for my product development. I have to add security to my developed firmware application. Because we are planning to use secure update of the application firmware. For th...
    vijith G
    last modified by vijith G