• Downloading binary to SDCARD(SD4 Slot) using MfgTool on the MCIMX6SX-SDB board

    Hi,   I'm using MfgTools in Windows 10. The MfgTool_MultiPanel(Library: 2.7.0) was performed by executing the mfgtool2-yocto-mx-sabresd-sdcard-sd4.vbs of L4.9.88_2.0.0_mfg-tool. LOG : MfgTool_Initial.log ...
    DongHyun Kim
    last modified by DongHyun Kim
  • compile error u-boot-fw-utils under yocto zeus

    I am trying to compile the u-boot-fw-utils under yocto zeus. Earlier i was getting compilation error but somehow imanages to replace my config with mx6sxsabresd_optee_defconfig as defined in default configuration...
    Nikhil sahu
    last modified by Nikhil sahu
  • Questions about IMX8QXP Seboot  function

    dear expert :   now i debug seboot of IMX8QXP , i have  some questions which need answer;   1、i fuse my board and sign the flash.bin  refer to introduction_ahab.txt and mx8_mx8x_secure_...
    ma shaofeng
    last modified by ma shaofeng
  • Adding packages under core-image-base image

    Hi All,   I am working on yocto zeus (https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml).I am adding some packages under core-image-base image. I modified th...
    Nikhil sahu
    last modified by Nikhil sahu
  • i.MX8M Mini MIPI CSI RGB888

    Hi guys,   I'm just working on a project, that requires support for RGB888 video data over the i.MX8's CSI interface.   Unfortunately the current drivers don't support RGB888 data, so I tried to add suppor...
  • Dual display (HDMI + OLED) on i.MX 8M Quad EVK

    Hi All,       I try to use dual display via HDMI + OLED panel on i.MX 8M Quad EVK, but default fsl-imx8mq-evk-dual-display.dts is used for HDMI + MIPI DSI to HDMI. so, Is it p...
    Sam Wu
    last modified by Sam Wu
  • How to identify display on imx8qxp

    As imx8qxp can driver more displays(DSI0, DSI1 and LCDIF),  How to identify display in application while all these display drived ? thanks. our test environment is L4.14.98_2.3.0_images_MX8QXPMEK(rootfs is&...
    Ping Wu
    last modified by Ping Wu
  • CST HSM 3.2.0 compiled against Openssl 1.1.1f leaks memory and segfaults

    Hi,   I'm attempting to compile CST against OpenSSL 1.1.1f. To achieve this I've recompiled libfrontend (as the packaged one seems to be compiled against older openssl) and used this binary to compile the comple...
    Atte Pellikka
    last modified by Atte Pellikka
  • Secure Boot on imx8mq.

    Hi, What are the step for secure boot on imx8mq?   Thanks, Nilesh Patel
    Nilesh Patel
    last modified by Nilesh Patel
  • PMIC read error | imx6q sabreAI

    Hi All, I am working on imx6q based sabre AI custom board, running android 7.1.Everything works fine on our first version but in our latest version of our custom board,it is showing PMIC read and write error and boot...
    RICHU C J
    last modified by RICHU C J
  • I.MX 7 ULP/Solo datalogger use

    I'm new to I.MX processors and only familiar with Beaglebone black (AM355x). But i'm looking for a 'upgrade' to the BBB, any idea how the 7(ULP/Solo) compare? It's a core A7 compared to core A8 but a much newer design...
    Michiel TJampens
    last modified by Michiel TJampens
  • How to calculate sleep timings in i.MX6solo processor

    Hello Sir/Madam,   In our custom board we are using processor i.MX6solo(MCIMX6S6AVM10AC), i need to keep this device for sleep mode so i need to know how long it can be in sleep mode.  If you any calculati...
    Ramesha S P
    last modified by Ramesha S P
  • i.MX7ULP: IO configuration

    Hi,   I am planning to use imx7ULP in one of the medical applications device. And require 3 Mic to interface with iMX7ULP. And it is battery operated device so we have to select iMX7ULP. I have some of the ...
    Mrudang Shelat
    last modified by Mrudang Shelat
  • Android 10 - i.MX8MMini - g2d rotation issue

    Hi,   I've found an issue with the G2D HWC layer on i.MX8M Mini, here is my setup: - Android 10.0.0-1.0.0 release - i.MX8M Mini EVK platform - MIPI display (1280x800 in my case) - SF_PRIMARY_DISPLAY_ORI...
    Gary Bisson
    last modified by Gary Bisson
  • PHY on MCIMX6Q5EYM10AD PLATFORM

    I am using the IMX6Q platform now, and the PHY is using the KSZ8041FTLI. However, during mass production, I found that some boards cannot be directly connected to the computer network to ping, the link light is always...
    zhang ha
    last modified by zhang ha
  • DDR Interface Control on I.MX8 NANO

    Hello I am a student at Grand Valley State University. Me and 2 other students are trying to work with the nxp i.mx8m nano evaluation board. We are currently only using the base SDK and FreeRTOS. Currently we are tryi...
    William Mckeever
    last modified by William Mckeever
  • i.MX8 MM Not detected eMMC Slot

    hi communicators.   I have one specific question plz help...   - My NXP Board Description Picture:    i.MX 8M Mini ----------------------------------------------------------------------------...
    lim eon
    last modified by lim eon
  • i.MX6ULZ CCM_CLK1_N/P question

    1. Can CCM_CLK1_N/P output 32.768KHz? 2. Can CCM_CLK1_M/P still output in suspend mode?
    m.c
    created by m.c
  • How to access to the top address of OCRAM for i.MX8QXP

    Hello,   From RM (IMX8DQXPRM_Rev.0.pdf)     OCRAM is mapped to address of 0x100000 to 0x13FFFF. But, I could not access to address range from 0x100000 to 0x117FFF by u-boot prompt. Can w...
    Kazuma Sasaki
    created by Kazuma Sasaki
  • IMX8MM   RMII for dp83848 in Uboot and Linux

    Hi, We have the custom board IMX8MMINI with Ethernet Phy dp83848, How to customize IMX8MM for  RMII for Ethernet Phy dp83848 in Uboot and Linux and we are using  50MHz external oscillator clock for Ethernet...
    Santhosh Kumar
    last modified by Santhosh Kumar