Skip navigationLog in to follow, share, and participate in this community. Hi everyone, My name is Toan. Currently, I'm using iMX6UL-evk with kernel rev L4.14.98_2.0.0_ga. The boot time is approximate 30 seconds. And I wanna reduce this time to under 10 seconds (from start to show up login ... How to reduce boot time on iMX6UL-evk ?
BackHello community, If default Linux BSP image, it have H/W VPU library and enable VPU module clock and power, on no-VPU device like MCIMX6Q4AVT08AER, what happen to run video encode/decode application on ... Linux Kernel setting for MCIMX6Q4A
BackHi, as far as I can see from Android BSPs for iMX8 family, there is no support for DisplayPort for iMX8MQ. The file signed_dp_imx8m.bin is not even available in the imx-image folder. Using Android 9.0.0 v2.0.0... iMX8MQ: DisplayPort support in Android
Backhi sir, when i use uuu tool in windows to update android 9(which i compiled), there is one error happened at the beginning,log as follow: >uuu D:\uuu\Windows\uuu-android-mx8qm-mek-emmc.ls... Hi, I am currently working with Yocto project with warrior branch. I have generated the core-image-base and i am successfully able flash binaries using sdcard. But i want to flash binaries using USB . I have find to... How to Flash *.wic.gz fromat binaries on IMX6 Solo using USB OTG
BackHi, We have an issue about USB connection as below. Could you tell us the suggested configuration range of LDO_USB and LDO_2P5? (Currently BSP provided their values LDO_USB = 3.2V and LDO_2P5 = 2.5V, but... i.MX 6DL LDO_USB & LDO_2P5 configuration
BackHello, I'm looking for instruction on how to make 8MMINID4-EVK boot from NAND. 1. We have received Micron MT29F64G08CBABBWP NAND chip and the Linux has recognized it: [ 1.262362] nand: devi... HowTo NAND boot for 8MMINID4-EVK?
BackWhy join the queue in the V4L2 framework?Interrupts and queues are not used in SDK routines. But it can also be displayed。So what's the point of being in a queue? About queues in the V4L2 framework
BackI have working for device imx8m mini evaluation for some similar product. I tried build default Linux kernel source code and try to boot from SD card. But the Linux kernel has not fully boot. I have attached log... Hi, i have a problem with SPI on iMX6. I'm using a Congatec Module. The module mount a iMX6 Solo. I want to configure ECSPI1 as a "spidev" device. Initially the congatec dtsi was: &ecspi1 { fsl,... SPI don't work on iMX6 - Linux
BackHi, I am using IMX6ULevk board with wm8960 codec,but when i want to record audio ,its not happening . Please can i know what may be the problem and which part of the driver i need to check for mounting the mic and s... Recording of audio is not happening
BackDear NXP, I want to use uuu download mode to recovery my device, I use commang below: cd C:\platform-tools uuu.exe F:\IMX8\android_p9.0.0_2.0.0-ga_image_8mqevk\uuu-android-m... IMX8 UUU.exe Download Mode hang
BackWe are using an imx6-based board running Linux with Wayland. I need use the Vivante GPU's imxeglvivsink to display video inside a GTK+3 window with GStreamer. The problem is that the video with the imxeglvivsink plugi... imxeglvivsink inside a GTK window in Wayland
BackI can build out the Linux image, but I can't find any document for flashing these images.... For Android cases, all these flash script can be found under out/target/product/xxx/ dir, but for Linux, no such fla... How flash linux image for imax8 Mini
BackHello, Customer : Harman Project : M.A.R.S at BMW Device: i.MX8QXP BSP : L4.14.98-2.0.0_ga or later release Are there any performance data for the released audio codec optimized by NEON SIMID i... Performance results for DSP using NEON co-processor on i.MX8/8X
Back Hello, I'm trying to build an image for an IMX6UL-EVKB. I followed the instructions of this documentation : i.MX Yocto Project User's Guide (Rev. L4.14.98-2.0.0_ga, 04/2019). I'm working on Ubun... IMX6UL-EVKB Image building issue
Back你好, 在imx8qxp-mek上的MIPI-CSI链接一个sensor接收的是2clock/pixel的yuv422_8_8数据格式的数据源,图像尺寸设定为1920*1080,但显示出的尺寸为960*1080,且显示图像为带有深浅的绿色剪影,反色显示,不丢帧,如下图 使用的命令为:gst-launch-1.0 v4l2src device=/dev/video0 ! 'video/x-raw,formate=YV12,w... imx8是否设置2clock/pix模式存放sensor传来的数据
BackHello, All I'm using YOCTO for imx6dl board, set up as follow from NXP document: Command Line $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://source.codeaurora.org/external/... [YOCTO] How to Change Python3.5 to Python3.6 over
BackHello, All I'm beginner about imx6 processor. Checking functions with the SABREAUTO RDK board. I was getting started with i.MX_Yocto_Project_User's_Guide.pdf inside of imx-yocto-L4.14.98_2.0.... Boot MMC/eMMC on SABREAUTO Board
BackHi Team I am trying to flash android on already loaded yocto linux imx8mmevk. When I try to run the command ./uuu_imx_android_flash.sh -f imx8mm, it repeatedly loops in flashing u-boot.imx and on the ... imx8mmevk android flashing
Back