• imx-image-full fails building. Some packages failed with an error during build

    Hello Guys,   I want to use the i.MX8M mini for some ML & KI Application. Therefore I want to build the imx-image-full with Yocto. I followed the Instructions on the YoctoUserGuide Rev. L5.4.24_2.1.0, 06/20...
    Patrick Stenger
    last modified by Patrick Stenger
  • how to add meta-clang to Imx8qm  iwave board yocto?

    how to add meta-clang to Imx8qm  iwave board yocto?   ERROR: Layer clang-layer is not compatible with the core layer I am using meta-clang commit 6475bb23b98160bfe6c5b2acf3e5e76ad8a05345 to add meta-clang i...
    peter zhang
    last modified by peter zhang
  • Ethernet Communication over longer cable length

    Hi NXP Team,   We are designing a product on i.MX8M Mini processor and Ethernet signals are used for VoIP calling and we have implemented Microchip PHY- KSZ9031.   We are trying to check the communication...
    Dhara Pillai
    last modified by Dhara Pillai
  • i.MX8MSCALE DDR Tool - TrainInfo Detailed Debug Information

    We use the i.MX8MSCALE DDR Tool (i.MX 8M Family DDR Tool Release ) für i.MX Nano (Rev.3.10) to stress and analyse our LPDDR4 Memory interface. We want to increase the debug Output and set TrainInfo fro...
    Daniel Koethe
    last modified by Daniel Koethe
  • Does anyone have patch for rpmsg wakeup source for kernel L4.1.15

    Hi,   As per below document, iMX8QXP: Use RPMSG to wake up M4 and A35    patch : L4.14.78_rpmsg_wakeup.patch is for only L4.14.78.   Is there any patch for L4.14.15 as I see there are many...
    Rakesh Patel
    last modified by Rakesh Patel
  • IMX8M populate sdk error

    system info: Linux Version:Ubuntu 19.04 BSP version :repo init -u https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml  Build command:DISTRO=fsl-imx-xwayland ...
    zhaoping yang
    last modified by zhaoping yang
  • USB OTG Eye Diagram test for i.MX6Q

    Hi,   I referred to https://community.nxp.com/docs/DOC-105609 (I.MX6 series USB Certification Guides) to configure the eye Diagram test , With reference to https://community.nxp.com/docs/DOC-94460?commentID=17030...
    zero zero
    last modified by zero zero
  • imx8mm lpddr4 issue: Fail to resume from suspend

    Hi,        I encounter issue on our imx8mm board when resume from suspend. Comparing to imx8mm-evk, we use lpddr4: FORESEE_LPDDR4X_NCLDXC1MJ512M32. both hardware design and software code are ...
    Junsheng Zhang
    last modified by Junsheng Zhang
  • Configuring ECSPI2 SS0 to Low in iMX8MM EVK

    Hi,   I am working with iMX8MM EVK and Yocto distribution 4.19.35 version   Build Configuration: BB_VERSION = "1.42.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-16.04" TARGET_SYS = "aarch64-poky-l...
    Sreedhar A
    last modified by Sreedhar A
  • Replacement part number for i.MX8M EVK BOM (Crystal and RJ45 connector)

    Hi everyone, I am going to design a custom board based on i.MX8M EVK. First of all, I have checked i.MX8M EVK BOM in terms of market availability of components in Digkey, Mouser,.. I founded all the components except ...
    saeid fallah
    last modified by saeid fallah
  • Secure boot issue  for i.MX6DL custom board

    Hi Yuri and all,   As you may noticed, with help from Liu Kui, I managed to resolve the HAB_INV_ADDRESS issue. However, my first custom board was locked (bricked) after programming to close the device...
    Shunnian Zhai
    last modified by Shunnian Zhai
  • Same content on LCD as on LVDS

    Hello, We have a custom board (imx6q) on which one time a LVDS panel is connected, and another time an lcd panel. These are connected on the same IPU - DI. I thought it was going to be as simple as just configure the...
    Wouter Vanhauwaert
    last modified by Wouter Vanhauwaert
  • How to up eth0 when power on  at imx8qxp

    How to up eth0 when power on  at imx8qxp ? 1.Hi,I am debug imx8qxp and sja1105r 1G communication.but first up eth0 then up sja1105R P0 port .imx8qxp and sja1105r can communication success. 2. kernel version 4.1...
    gao yuan
    last modified by gao yuan
  • IMX6D 可见光滚屏

    你好!           imx6DQ 移植xc7160外置isp +  imx298 sensor,可见光滚屏,    正常成像:    滚动异常成像如下:          更详细的滚动现象见附件...
    Lee Shuai
    last modified by Lee Shuai
  • The issues on "mmc0: cqhci: timeout for tag 0"

    Hi NXP teams    Recently We have a rather troublesome problem. After we flash the image of android Android P9.0.0_2.1.1_AUTO done,then  system boot up. Execute adb shell command,in the shell cmd,exec...
    yingjin yan
    last modified by yingjin yan
  • Enabling DM-Verity singing failed on i.MX8MQ

    Hello,   I am using i.MX8MQ custom board. I want to enable DM-Veiry signing using dm-verity RSA private key available at "Android-9.0/build/target/product/security/verity/verity.pk8".   The kernel configur...
    pratik manvar
    last modified by pratik manvar
  • BUCK2 efficiency of PCA9450A together with i.MX8M Mini

    Hi   The PMIC PCA9450A has an input range of 2.85V to 5.5V and has six high efficient step-down regulators. To optimize our power design we would like to know the efficiency of the reference design of ...
    Patrick Morger
    last modified by Patrick Morger
  • Incorrect SECO FW Version

    I am using an iMX8QM-MEK board and making a custom SCU Firmware (scfw_tcm.bin). With the debug monitor enabled, upon boot, I get the following error: "Incorrect SECO FW Version 2.3.1 (2.5.4 or later required)"  ...
    Stuart Rubin
    last modified by Stuart Rubin
  • Support for VC MIPI IMX327C Bayer RAW10 camera on IMX6

    Hello. I am working on camera support for visual components VC MIPI IMX327C for DART-MX6 from Variscite. Camera transmits video in bayer raw10 format 1920 x 1080 60FPS. I modified the standard ov5640_mipi.c dri...
    Valentin Ryzhenko
    last modified by Valentin Ryzhenko
  • Secure boot issue with HAB_INV_ADDRESS for i.MX6DL custom board

    Hi All,   We have an i.MX6DL custom board with the following information:    CPU:   Freescale i.MX6DL rev1.2 at 792 MHz    U-Boot 2017.11-imx6dl   Now we want to a...
    Shunnian Zhai
    last modified by Shunnian Zhai