• Hi can imx28 control 600x1024 tft lcd displaye.

    Am working on a project for only for e reader with 600x1024 TFT LCD and touchscreen and any one help me any microprocessor from imx product for this and is imx28 good for this project?
    Melaku Zeleke
    last modified by Melaku Zeleke
  • i.MX GPIO PU/PD/keeper admittable configurations

    Hi all,   I wrote this question to try to summarize things on official documentation and to get an explanation about the topic GPIO PU/PD/keeper admittable configurations, for GPIO output and input configuration...
    Mauro Salvini
    last modified by Mauro Salvini
  • i.MX6 QMediaPlayer does qtvideosink use IPU?

    I want to use qt5 with qml to show a dual-stream.   main.qml: import QtQuick.Window 2.1 import QtQuick 2.0 import QtMultimedia 5.12   Window {     id: window     visible: tr...
    Michael Stahl
    last modified by Michael Stahl
  • I want to set Camera I/O of IMX8QXP to 10-bit.

    Hello, #I want to set Camera I/O of IMX8QXP to 10-bit. So I want to know how to use 10-bit parallel CSI of IMX8QXP.   I can understand usage of 8-bit pallael CSI from the IMX8QXP Datasheet,  but 10-bit pa...
    Yoshihiro Takahashi
    last modified by Yoshihiro Takahashi
  • reboot and shutdown are not working in custom imx7 board..?

    Hi all,   i am working on custom board base on imx7d, my board is freezing after a while when i reboot or shutdown, also i tried reset command from uboot here also it is freezing can anyone suggest me any solut...
    Flaby Jacob
    last modified by Flaby Jacob
  • Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory

    Hey guys,   I am using the BSP Linux Image L5.4.24-2.1.0_images_MX8MMEVK for  my i.MX8M mini Evalkit. I want to use several i2cdevices on my i.MX and therefore I need to install some pa...
    Patrick Stenger
    last modified by Patrick Stenger
  • i.MX 8X/8 Hardware Resource Partition

    Hi Guys,       Is there any document about how to do i.MX 8X/8 hardware resource partition?Is there any considerations about   hardware limitation and sofeware implement?
    Ethan Li
    last modified by Ethan Li
  • Does NXP provide  imx6ul RNDIS drivers for windows?

    Hi  everyone, I'm reviewing RNDIS devices using imx6ul. When I connect to Windows PC, it is recognized as an Unknown device but the driver is not installed. Is there an RNDIS driver provided by NXP? If there i...
    Youngjoo Kim
    last modified by Youngjoo Kim
  • 想问问Linux4.1.15下SPI的MOSI管脚默认低电平怎么设置

    我在用IMX6DL的核心板,系统用linux 4.1.15,我用了SPI功能,想问问,如果我想  SPI的  MOSI 管脚默认低电平 我怎么设置。
    Dong Jing
    last modified by Dong Jing
  • BUCK2 efficiency of PCA9450A together with i.MX8M Mini

    Hi   The PMIC PCA9450A has an input range of 2.85V to 5.5V and has six high efficient step-down regulators. To optimize our power design we would like to know the efficiency of the reference design of ...
    Patrick Morger
    last modified by Patrick Morger
  • imx8qxp-mek lpspi问题

    我们在imx8qxp-mek开发板上测试LPSPI模块的SPI功能,将fsl-imx8qxp-mek.dtsi文件添加了imx8qxp-lpddr4-val-lpspi.dts/imx8qxp-lpddr4-val-lpspi.dts中的 pinctrl_lpspi0: lpspi0grp {       fsl,pins = <   ...
    peterson hou
    created by peterson hou
  • imx8mq接三星evo 970 ssd硬盘

    各位版主好,请问imx8mq的usb1作为3.0的host,接ssd固态硬盘出现这个现象是什么问题导致的?   有时候又出现这个信息
    小辉哥
    last modified by 小辉哥
  • imx8: Traffic light recognition sample code

    Exploring Traffic light recognition, can you provide any sample c++ code to start with? Will build for target: imx8mq evk
    vipul Suneja
    last modified by vipul Suneja
  • IMX8MM :   How to remount the ov5640 driver

    Hi,  I am using the custom hardware and i am facing a problem when the processor is booting it tries to check for the camera data but the camera bridge ic configuration happens after the board has booted up, sin...
    Santhosh Kumar
    last modified by Santhosh Kumar
  • wlan0 interface is not coming up for onboard wifi module with imx8 Nano evk

    Dear NXp, As i am not able to bringing up the wifi module that is connected on imx8 Nano evk board, running below commands to bring up the interface, included wifi-tools to my .bblayer. is there any other packages n...
    shilesh babu
    last modified by shilesh babu
  • i.MX8M GPU seems still OOM after apply patch

    We got patch from support case: #00266485, but seems still OOM after apply patch. Previous report at i.MX8M GPU test oom  We lower the memory to 560M for Linux for decrease the time of duplicate issue...
    m.c
    last modified by m.c
  • Cortex-A toolchain/BSP/IDE info

    Hello,   I'm looking for clarification for which tool-chain, BSP version and IDE  I can use for building Cortex-A53 and A72 simple apps for i.MX8QM platform (linux or win).   I didn't find support und...
    ravi.kohli@l3harris.com
    last modified by ravi.kohli@l3harris.com
  • CSI0 with 16-Bit video does not receive any frame

    We have some issues with our Board trying to receive a 16-Bit video Stream (YUYV with external HSync and VSync) with 1080p25 resolution from an external SOC connected to CSI0 of IPU1 of our iMX6DL (Pixel Clock ~ 78MHz...
    Sebastian Wendt
    last modified by Sebastian Wendt
  • About SD Card Power Down

    Hello,Community   As shown below, at power down, CLK, CMD and DATA must be logic 0. For example, if you use SW_MUX_CTL_Register(IOMUXC_SW_MUX_CTL_PAD_SD1_CLK) for ALT0_SD1_CLK and use it as a clock, do you have...
    goto11@wantsinc.jp
    last modified by goto11@wantsinc.jp
  • FlexSPI layout guidelines

    HI NXP Team,   We are using i.MX8DualXPLUS processor in our custom platform development based on the MEK. Please recommend some good reference document/link for the FlexSPI Octal interface layout guidelines. 
    Harsh Mistry
    last modified by Harsh Mistry