Skip navigationLog in to follow, share, and participate in this community. Hi, I'm trying to find lpddr4 configuration for imx8qxp-mek -development board from U-boot, but either it's not there or I'm blind because I just can't seem to find it. There is one for imx8m, but that is diff... Memory configuration for i.MX8QXP in U-boot
BackDear friends, Given the available examples, such as the NXP SDK examples for RT1050 family processors, what are the best examples that use processor timing? Thank you for your attention, a hug! ... Hi, I found this link How to get IEEE 1588 1PPS on i.MX6Q? talking about getting the 1PPS signal working for 1588. I made the change to the fec_ptp.c driver and I "think" I have pinmux setup corr... Trying to get 1588 working on imx8 mini
BackHello, I am working on phyCORE-i.MX8 which is been customized from i.MX8QM emk board. Which tool dose the board support for flashing. Can I get the document on how to build the Xen H... How to build Xen Hypervisor on imx8qm and flashing tool
BackHi, Kind NXP and everyone! I want to show splash screen for U-Boot and Linux, and I completed the U-Boot logo for iMX6ULL and Yocto(Linux kernel imx6ulevk 4.1.15, U-Boot 2016.03). But at Linux kernel... Linux logo image from U-Boot for iMX6ULL
BackI can't get the 1000Mbps external loopback to work on i.MX8M eval board. The link just never comes up even though I have followed all the suggested steps and have a gigabit external loopback connected. FYI, t... Gigabit ethernet loopback on i.MX8M eval board
BackSaved FAQ from Freescale.com for information only: Topic: GPIO IOMUXC Question. Please clarify how to use the SION bit ? Answer. The SION, Software Input ON, bit field on many ... Hello, Im trying to get st_pressure driver working with IIO driver with MX8M Variscite eval kit board using linux 4.4.78 In menuconfig i activated drivers + device tree looks like : ... This guide will show you how to debootstrap Debian Buster on imx8mminievk on a SD-card, but will very likely help you on other systems as well. First you need a Linux installation present on the imx8mminievk. ... debootstrap Debian Buster on imx8mminievk
Back各位大神们: 有人使用过该patch吗?需要注意哪些地方。 首先、我使用的系统:android6.1,内核: 4.1.15,uboot:2015.04-dirty。参考的是sabresd_6dq参考板。使用的是6q6a。 根据readme: ... M6.0.1_2.1.0_uboot_logo_keep_patch_2017-01-06.zip patch use condition
Backhi all, I would like to drive a stepper motor using the SPI interface on imx6solosabresd board . problem is I have no idea what I am doing. I don't even know what all the pins are for on the board. here we are going ... stepper motor interfacing through spi on imx6solo sabresd
BackOpenGL GLX extension is not supporting for hdmi display connected on im8qxp.... I ahve written a sample code based on glut...and run as following freeglut (./sample): OpenGL GLX extension not supported by di... OpenGL GLX extension to be checked
BackThis thread continues an earlier email conversation between a number of parties. It relates to IoT Core boot freezes where a Quad Core iMX6 Hummingboard has been placed in a third-pa... Hummingboard/Custom Carrier Board IoT Boot Issues
BackHi All, We are going to make product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor. Currently we are doing POC on IMX8MQ processor EVK. We are using imx-yocto-sumo with kernel version (imx_4.14.98_2.0.0_g... Weston issues on IMX8MQ evk
BackI want to do video coding and decoding on imx8m, but I'm not sure which library I should use, libhantro.so or lisfslvpuwrap.so,. I didn't find the documentation again. The vpu encoding and decoding of imx8m seems to ... I want to share some measurements that we did in the office for the initial boot steps, from POR until user code is executed from DDR. Measurements were made with no HAB and don't include Power time, which is device d... ROM Code Boot Time Measurements
BackHi, I am having an issue with the imx-spi driver on linux imx branch 4.9.88. On one of my ecspi channel (i.MX6 quad), I am connecting a SPI slave device that works in mode 3 (CPOL=1, CPHA=1). This devi... i.MX6 ecspi race condition with CPOL=1 and CS GPIO
BackHi, I'm working on a iMX8M Mini EVK (official NXP Android bsp) and I want to use the UART4 , formally used as debug port for M4 microcontroller . Changed the DTS file to include the UART: /*pin muxing... iMX8m EVK UART4 unavailable
BackSometimes after playing decoded video with a gstreamer pipeline the display (including most but not all windows) gets shifted maybe 5 to 10 percent with the right side wrapping around to the left side (pictures attach... iMX8M display shifted after playing decoded video with gstreamer
BackHi, I'm using a iMX8m custom board with a 1024x800 MIPI display, I've changed my the DTS file (using fsl-imx8mm-ddr4-evk-rm67191.dts as reference) to have a panel (no lvds bridge) and try to use the driv...