• MIPI Display to IMX8 MQ

    Dear All, We have connected MIPI display to imx8 MQ, We are concern like panel information along with display-timing parameter shall be defined in in dts file. whether panel and display parameter shall be defined in ...
    kishore poojari
    last modified by kishore poojari
  • Bug-Fixes for FlexSPI

    We are using a SoM with an i.MX8M-Mini and tried to use the FlexSPI to communicate with an FPGA which simulates a flash memory using 1-1-4 or 1-4-4 transfer mode. To get that working we had to fix or extend the linux...
    Christoph Fink
    last modified by Christoph Fink
  • Ethernet ports in IMX6S

    Is that IMX6S supports 2 ETHERNET MII interface(1-RGMII & 1-RMII)??
    HARIHARAN M
    last modified by HARIHARAN M
  • Android Q10.0.0.1.0.0 for i.MX8 MQ evk

    Hello,   I recently found that NXP has released the proprietary source code for Android 10. Just wanted to starting integrating it with Marvell wireless modules for imx8mq evk. Is it been tested before? Now tha...
    Achyut Hegde
    last modified by Achyut Hegde
  • Booting from NAND 4.14.98_2.2.0 imx6ull

    Hi,   We are porting our imx6ull from 4.1.15 to 4.14.98(provided by NXP). Uboot and kernel are successfully up. But filesystem mounting is not happening   UBI error: cannot open mtd 3, error -19 snvs_rtc 2...
    Deepanraj Anbarasan
    last modified by Deepanraj Anbarasan
  • mic recording of voice is not possible

    Hi, Im using the imx6ulevk board ,presently working on the codec section ,when im recording the voice through on board mic and aplay that recorded wav file im not able to hear any thing.But when i record the song thr...
    Dhanush V
    last modified by Dhanush V
  • Video streaming issue from USB Webcame to HDMI in iMX8MQ

    Hi,   We have designed our application board based on iMX8MQ processor. We have completed bring up of all interfaces including USB3.0 & HDMI port. Both USB & HDMI interfaces are working fine. We ar...
    chaitanya sonagara
    last modified by chaitanya sonagara
  • IMX8MQ + DSI host controller support at U-boot

    Hi All, We are working product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor.  We have LCD working fine at kernel level.  In our system LCD is driven by eLCDIF controller via MIPI DSI controller. Now we wan...
    Jemish Patel
    last modified by Jemish Patel
  • i.MX28: How to set up a SSH connection to EVK board

    This page will guide you to setup a SSH connection to i.MX28 EVK board using BSP L2.6.35_1.1.0_130130.   1. Add required package "openssh" & "dhcp" By default, minimal profile is selected and package "opens...
    PeterChan
    last modified by PeterChan
  • mfgtoolcli fails under linux

    I am having the same issue when using mfgtoolcli under Linux. (all works well when running it with Windows) My hardware is  an NXP Imx6ull evk development board. The package I am using is L4.9.11_1.0.0-ga_mfg-t...
    mat kattanek
    last modified by mat kattanek
  • Unboxing MYD-C8MMX Dev Kit Based on NXP i MX 8M mini A53 Quad Processor

    Unboxing MYD-C8MMX Dev Kit Based on NXP i MX 8M mini A53 Quad Processor   The MYD-C8MMX development board is using the i.MX 8M Mini Quad Processor which is among NXP i.MX 8M mini family of applications processor...
    Kiddy Xu
    last modified by Kiddy Xu
  • [YOCTO] Getting started with yocto and debian

    Hi there! i'm getting started with a system embebed from tq, tqma6ulx-mba6ulx, I never work before with an embedded system. I've created an image with Yocto, and differents layer from freescale. Now, I'm trying t...
    Santiago López Pina
    last modified by Santiago López Pina
  • Android and GPU on i.MX53 board -> green screen

    Hello @all,  I'm working on Android for a i.MX535 based TX53 board using the Freescale LVDS display on DI0. I'm using the Adroid SDK release 10.4 including the kernel from this release. I even managed to make the...
    Florian Boor
    last modified by Florian Boor
  • QSPI Flash Help - MIMXRT1050

    Hello,   I am using the MIMXRT1050 with QSPI flash on Keilv5 IDE. My QSPI flash manual: https://www.winbond.com/resource-files/w25q256jv%20spi%20revg%2008032017.pdf   I am using the flexspi_nor_polling_...
    Kamal Nasif
    last modified by Kamal Nasif
  • mfgtool2 damage two pico-imx7d SOM modules. Where it spoiled?

    Hi,   I have this issue: My other imx7d pico android things start kit died, again    I was following the steps of this link: iMX7D Pico won't boot    I used the <LIST name = "e...
    NEUBER DE SOUSA
    last modified by NEUBER DE SOUSA
  • Galcore module initialization failed

    Hello, we are trying to set up our environment for i.mx6dl bsp, based on Yocto Sumo. We have tried both Linux Kernel 4.9.67 and 4.9.88, but we have several problems in Galcore module initialization. Galcore module (v...
    Massimo Volpi
    last modified by Massimo Volpi
  • mfgtool2 damage two pico-imx7d SOM modules. Where it spoiled?

    Hi,   I have this issue: My other imx7d pico android things start kit died, again    I was following the steps of this link: iMX7D Pico won't boot    I used the <LIST name = "eMMC...
    NEUBER DE SOUSA
    last modified by NEUBER DE SOUSA
  • FXOS8700 linux driver

    Hello! In our custom board we use FXOS8700. When I start driver from fsl-arm-yocto-bsp (kernel 4.9.11), I see that it creates only one input device and event from accelerometer and magnetometer are emitting...
    Maxim Kuk
    last modified by Maxim Kuk
  • Ti DS90UB947/948 Linux Driver for I.MX6

    Imx6 can output lvds direct.But the lvds-wire is too  expensive to buy. So they can cannect ds90ub947 serializer to applied in automotive instrumentation. By the way, it need a ds90ub948 ...
    Zhongmao Liu
    last modified by Zhongmao Liu
  • Synaptics RMI4 Multitouch PAD

    Connection NOTE: nINT is an active-low open-drain pin for which the host must supply an external pull-up resistor.DISP2_DAT9        --->  Touch_nINT DISPB2_SER_CLK  ...
    Mark Ding
    last modified by Mark Ding