• stepper motor interfacing through spi on imx6solo sabresd

    hi all, I would like to drive a stepper motor using the SPI interface on imx6solosabresd board . problem is I have no idea what I am doing. I don't even know what all the pins are for on the board. here we are going ...
    anna srikrishna sri
    last modified by anna srikrishna sri
  • OpenGL GLX extension to be checked

    OpenGL GLX extension is not supporting for hdmi display connected on im8qxp....   I ahve written a sample code based on glut...and run as following freeglut (./sample): OpenGL GLX extension not supported by di...
    Sandeep Rai
    last modified by Sandeep Rai
  • Hummingboard/Custom Carrier Board IoT Boot Issues

    This thread continues an earlier email conversation between a number of parties. It relates to IoT Core boot freezes where a Quad Core iMX6 Hummingboard has been placed in a third-pa...
    Andrew Kissling
    last modified by Andrew Kissling
  • Weston issues on IMX8MQ evk

    Hi All,   We are going to make product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor.  Currently we are doing POC on IMX8MQ processor EVK. We are using imx-yocto-sumo with kernel version (imx_4.14.98_2.0.0_g...
    Jemish Patel
    last modified by Jemish Patel
  • imx8m vpu

    I want to do video coding and decoding on imx8m, but I'm not sure which library I should use, libhantro.so or lisfslvpuwrap.so,. I didn't find the documentation again. The vpu encoding and decoding of imx8m seems to ...
    y f
    last modified by y f
  • ROM Code Boot Time Measurements

    I want to share some measurements that we did in the office for the initial boot steps, from POR until user code is executed from DDR. Measurements were made with no HAB and don't include Power time, which is device d...
    AdrianGancev
    last modified by AdrianGancev
  • i.MX6 ecspi race condition with CPOL=1 and CS GPIO

    Hi,   I am having an issue with the imx-spi driver on linux imx branch 4.9.88.   On one of my ecspi channel (i.MX6 quad), I am connecting a SPI slave device that works in mode 3 (CPOL=1, CPHA=1). This devi...
    Théo Bueno
    last modified by Théo Bueno
  • iMX8m EVK UART4 unavailable

    Hi, I'm working on a iMX8M Mini EVK (official NXP Android bsp) and I want to use the UART4 , formally used as debug port for M4 microcontroller .   Changed the DTS file to include the UART:   /*pin muxing...
    mario Sangalli
    last modified by mario Sangalli
  • iMX8M display shifted after playing decoded video with gstreamer

    Sometimes after playing decoded video with a gstreamer pipeline the display (including most but not all windows) gets shifted maybe 5 to 10 percent with the right side wrapping around to the left side (pictures attach...
    Michael Erwin
    last modified by Michael Erwin
  • iMX8M And MIPI display

    Hi, I'm using a iMX8m custom board with a 1024x800 MIPI display, I've changed my the DTS file (using fsl-imx8mm-ddr4-evk-rm67191.dts  as reference) to have a panel (no lvds bridge) and try to use the  driv...
    mario Sangalli
    last modified by mario Sangalli
  • MFG tool to read a file from imx28 

    whats the command to read from the imx28    i am using the following MFG tool version   i could able to dump the file from host PC to imx28 hardware, but not read from the hardware to PC   tri...
    shashikant h
    last modified by shashikant h
  • Bug-Fixes for FlexSPI

    We are using a SoM with an i.MX8M-Mini and tried to use the FlexSPI to communicate with an FPGA which simulates a flash memory using 1-1-4 or 1-4-4 transfer mode. To get that working we had to fix or extend the linux...
    Christoph Fink
    last modified by Christoph Fink
  • RT1064 FlexCAN3 (CAN FD) issues

    Those experimenting with CAN FD on an i.MX RT1064 or similar will have noticed that the 'Enhanced' registers of the CAN FD capable 'FlexCAN3' peripheral are either not implemented at all, or are not working properly (...
    Wolfgang Buescher
    last modified by Wolfgang Buescher
  • iMX8 Android9 fails to build a new target

    Hi, all, I've succesflully build the imx-p9.0.0_1.1.0-ga for evk_8mm demo board: now I will want to build a new target. I've started coping  the android_build\device\fsl\imx8m\evk_8mm into android_build\device\f...
    mario Sangalli
    last modified by mario Sangalli
  • i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines

    The Freescale i.MX6 has many video capabilities that are best accessed through GStreamer.   Gateworks, the leading supplier of Powerful ARM based Single Board Computer solutions using the Freescale i.MX6, has in...
    Ryan Erb
    last modified by Ryan Erb
  • Unboxing MYD-JX8MQ6 Dev Kit Based on NXP i.MX 8M A53 Quad Processor

      Unboxing MYD-JX8MQ6 Dev Kit Based on NXP i.MX 8M A53 Quad Processor   The MYD-JX8MX development board is using the i.MX 8M Quad processor which is among NXP i.MX 8M family (i.MX 8M Dual / 8M Qu...
    Kiddy Xu
    last modified by Kiddy Xu
  • Running Netflix on iMX6 Android Marshmallow

    I managed to integrate Netflix on Android 6.0.1 Marshmallow BSP for the i.MX6DL, i.MX6Q and i.MX6QP. I posted the step by step procedure on the i.mxdev blog: Running Netflix on iMX6 Android Marshmallow - i.MXDev Blog...
    Breno Matheus Lima
    last modified by Breno Matheus Lima
  • Pico-Pi-IMX8M-Quad reboots on playing audio

    Hi NXP Comrades,   I was testing audio on my development device with Voice Hat planted on it. It was a malfunction in playing audio from Cactus Player or any third-party player like MX Player.   The audio wh...
    samad.meets@gmail.com
    last modified by samad.meets@gmail.com
  • IMX6 Xorg HwAccel Crashes

    I am having extreme difficulty getting X working with hwacceleration. I have followed a bit of a different route than you and there is good reasons for that. I have a debian 9 debootstrapped system with all the requir...
    Nico Du Toit
    last modified by Nico Du Toit
  • IMX.6 TVIN signal lock lost Algorithm for 4.1.15

    There is a patch in NXP application note "i.MX6 IPU TVIN Application note" REV 0, 8/2016, has anyone has working patch for Android 4.1.15?
    Willie Niou
    last modified by Willie Niou