• 在i.MX8QXP QM平台(L4.14.98 GA)上的OP-TEE中启用CAAM加速

    [中文翻译版] 见附件   原文链接: Enable CAAM accelerating in OP-TEE on i.MX8QXP/QM platform(L4.14.98 GA) 
    Leo Lin
    last modified by Leo Lin
  • 用于I.MX8QM QXP的AR0144和ov9284驱动程序

    [中文翻译版] 见附件   原文链接: AR0144 and ov9284 drivers for I.MX8QM/QXP. 
    Leo Lin
    last modified by Leo Lin
  • 通过使M4 Hello world正确运行来理解iMX8QX硬件分区(硬件分区实践)

    [中文翻译版] 见附件   原文链接: Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly 
    Leo Lin
    last modified by Leo Lin
  • 使用UUU刷新Linux BSP

    [中文翻译版] 见附件   原文链接: Flashing Linux BSP using UUU 
    Leo Lin
    last modified by Leo Lin
  • 设置i.MX8M Mini和纳米MIPI-DPHY时钟

    [中文翻译版] 见附件   原文链接: Setting i.MX8M Mini and Nano MIPI-DPHY Clock 
    Leo Lin
    last modified by Leo Lin
  • 如何添加iMX8QXP PAD(GPIO)Wakeup

    [中文翻译版] 见附件   原文链接: How to add  iMX8QXP PAD(GPIO) Wakeup 
    Leo Lin
    last modified by Leo Lin
  • i.MX8X_5.4.24_kernel customization application notes: (Chinese Version) i.MX8X 5.4.24 内核定制文档

    目录 1 创建 i.MX8QXP Linux 5.4.24 板级开发包编译环境 ..... 3 1.1 下载板级开发包 ....................................................... 3 1.2 创建yocto编译环境: ................................................. 4 1.3 独立编译 ........................
    John Li
    last modified by John Li
  • 如何使用OpenVX扩展NPU GPU来加速机器视觉应用

    [中文翻译版] 见附件   原文链接: How to use OpenVX extension for NPU/GPU to accelerate machine vision applications 
    Leo Lin
    last modified by Leo Lin
  • 快速,简便地设置i.MX评估板,以通过USB对i.MX板进行编程

    [中文翻译版] 见附件   原文链接: Quick and dirty setup of an i.MX evaluation board to program an i.MX board thru USB 
    Leo Lin
    last modified by Leo Lin
  • 将含有C0芯片的i.MX 8QuadXPlus MEK的DRP更改为DFP

    [中文翻译版] 见附件   原文链接: change DRP to DFP for i.MX 8QuadXPlus MEK with C0 chips 
    Leo Lin
    last modified by Leo Lin
  • 将 KSZ9031 加入到 i.MX BSP

    [中文翻译版] 见附件   原文链接: Porting KSZ9031 to i.MX BSP 
    Leo Lin
    last modified by Leo Lin
  • 带有Arm装置的容器技术在i.MX6UL的使用

    [中文翻译版] 见附件   原文链接: Docker On i.MX6UL With Ubuntu16.04  
    Leo Lin
    last modified by Leo Lin
  • 从TensorFlow开始你的机器学习之旅

    [中文翻译版] 见附件   原文链接: Start your machine learning journey from tensorflow playground 
    Leo Lin
    last modified by Leo Lin
  • OpenVX视觉图像扩展API简介 – 基础API

    [中文翻译版] 见附件   原文链接: OpenVX Vision Image Extension API Introduction - Basic API 
    Leo Lin
    last modified by Leo Lin
  • i.MX8QXP gamma校正

    [中文翻译版] 见附件   原文链接: i.MX8QXP gamma tuning 
    Leo Lin
    last modified by Leo Lin
  • i.MX6Q捕获原始(bayer)数据和debayer

    [中文翻译版] 见附件   原文链接: i.MX6Q capture raw(bayer) data and debayer  
    Leo Lin
    last modified by Leo Lin
  • How to Disable the DM-Verity option in your Android device.

    To disable the Android dm-verity in the new devices you should have the below. A Window/Linux computer The Android SDK platform-packages tools.   Download the Android Packages tool.   To use the Android ...
    Diego Adrian Cuevas
    last modified by Diego Adrian Cuevas
  • mek_8qm/evk_8mq enable uSD/M.2 8987 wifi module

    All below changes are done based on imx_android-10.0_5.4.y.   mek_8qm enable uSD 8987 wifi            1. hardware rework      ...
    Andy Tian
    last modified by Andy Tian
  • iMX8QXP: Use JPEG decoder in M4 SDK

    iMX8QXP/iMX8QM have hardware JPEG decoder: The JPEG-D-X core. This is the example code to use this hw decoder in M4 SDK to decode JPEG files.     M4_JPEG_DECODER_SDK_2.5.1.7z The attached "rear_view_c...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • Build Ubuntu For i.MX8 Series Platform

    The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04.   The Document will be continuously updated with enable VPU, ubuntu...
    Gnar Fang
    last modified by Gnar Fang