• How to locate i.MX6Q pfd issue(ERR006282) without JTAG tools

    When a board is brought up and  the ddr test by link of "https://community.freescale.com/docs/DOC-96412' has been verified, some of boards will have pfd issue(ERR006282). It is suggested that below method could b...
    John Li
    last modified by ebiz_ws_prod
  • iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP

    For iMX6DQ, there are two IPUs, so they can support up to 4 cameras at the same time. But the default BSP can only support up to two cameras at the same time. The attached patch can make the BSP support up to 4 cam...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • i.MX 8 Camera Use Cases

    This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera op...
    Marco Antonio Franchi
    last modified by Marco Antonio Franchi
  • Enable Ethernet for Android Auto with mek_8q

    Default Ethernet feature is removed for Android Auto (both Android_Pie9.0 and Android10) Below are the patched to bring Ethernet feature back to Android Auto. Please try to apply the according patches if you want to e...
    Andy Tian
    last modified by Andy Tian
  • iMX8QM/QXP Reference Patch to Map Bridge Chip to Display without EDID

    In defaut Linux BSP, NXP implemented LVDS to HDMI(it6263) and MIPI-DSI to HDMI(adv7535) bridge chip drivers. And these drivers need read the EDID from display, then apply the timing parameters to DRM driver.   B...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • i.mx8qm HDMI RX

    since imx8qm hdmi rx isn't stable enough, so this document introduce how to  enable HDMI rx simply, as far as I know, 4.14.98_2.3.0 is the most stable version right now, so first, build the 4.14.98_2.3.0 for imx8...
    Joan Xie
    last modified by Joan Xie
  • i.MX 8MM EVK Display Selection Guide

    This document describes the i.MX 8MM EVK mini-SAS connectors features on Linux and Android use cases, covering the supported daughter cards, the process to change Device Tree (DTS) files or Boot images, and enable the...
    Marco Antonio Franchi
    last modified by Marco Antonio Franchi
  • i.MX 8 GStreamer User Guide

    This document is a user guide for the GStreamer version 1.0 based accelerated solution included in all the i.MX 8 family SoCs supported by NXP BSP L4.19.35_1.0.0. Some instructions assume a host machine running a Lin...
    Marco Antonio Franchi
    last modified by Marco Antonio Franchi
  • IMX8QM: LVDS mirror dual mode reference patch

    The iMX8QM LVDS has followed work mode, (There are two LVDS modules in IMX8QM):   Single mode (LVDS panel connects to one channel) panel 1 and panel 2 can be different panels:     Dual channel split...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • i.MX6 serials (i.MX6S/DL/D/Q/Dp/Qp) audio card development guide:MX6X_ASOC_V5-20191115.pdf

    this doc is explain how to develop a audio card driver base on i.MX6 platform. which explain the ASOC architecture struction basic knowledage and then give some sample for the audio driver development like: 1:NXP SG...
    John Li
    last modified by John Li
  • Introduction of wayland simply

    Wayland:   Wayland is a display SERVER and COMPOSITION protocol. It is relatively new, as its first release was in 2012. The protocol enables applications to allocate their own off-screen buffers and render their...
    Joan Xie
    last modified by Joan Xie
  • unable to connect to git.freescale.com

    Recently many customers faced the issue about connecting the git.freesacle .com failed when they built old bsp version like 4.1.15 or 3.14.52,  when the customer repo init according to the yocto user guide, they ...
    Joan Xie
    last modified by Joan Xie
  • Fixing git.freescale.com dependencies on older Android BSPs

    The decommission of the git.freescale.com has caused some problems to BSPs dependent on packages stored in this repository. All contents on git.freescale.com have been moved to one of three locations:   NXP ...
    gusarambula
    last modified by gusarambula
  • Fixing the Direction field for GPIOs on the I.MX V7 Pins Tool

    Some processor’s GPIO settings on the i.MX Pins Tool version 7 may not show allow to select direction and just show an option “Input/Output” as shown. This will be fixed, but the settings can be chan...
    gusarambula
    last modified by gusarambula
  • Win 10 IoT Unstable Gigabit Ethernet Fix

    When using Gigabit Ethernet on boards i.MX running Windows 10 IoT Core users may experience network unstability and low latency using build W1809_1_1_0_imx-iotcore. This was fixed by increasing the size of Rx/Tx ...
    Petr Kovar
    last modified by Petr Kovar
  • Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)

    This patch made the display no interrupt from uboot to kernel to Android. The IPU and related hardware display interface will only be initialized once in Uboot, the kernel code will skip the IPU initialization.  ...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • i.MX Android Frequently Asked Questions

    i.MX_Android_FAQi.MX Android FAQ 1 Sync project and Build1.1 How can I download AOSP repo from mirror server?By default, all aosp repo in the Android project will be downloaded from google server directly. But some ma...
    G.Y. CHEN
    last modified by Faqiang Zhu
  • USB Power Control of i.MX6ULL-EVK

    This document is describe the control method of USB Power based on I.MX6ULL-EVK.   1. Hardware Design USB OTG can be working as device mode, host mode, or switching between both device mode and host mode. (...
    jimmychan
    last modified by jimmychan
  • i.mx8x ADAS support

    Platform: i.MX8QXP/8QM OS: Linux Supported Camera Modules: Max9286 + Max9271 + OV10635, Default BSP Max9286 + Max96705 + AR0144, patch Max9286 + Max96705 + OV9284, patch Max9286 + Max96705 + AP0101 + AR0132, pat...
    Zoey Li
    last modified by Zoey Li
  • How to use non-rpmsg.dtbs on i.MX 8QXP

    The i.MX 8QXP MEK does not allow the OV5640/LVDS/LCD usage only by changing the device tree anymore. It occurs because the M4 owns the i2c resources, so the A core must use rpmsg to enable virtual drivers.   Du...
    Marco Antonio Franchi
    last modified by Marco Antonio Franchi