• Build Ubuntu For i.MX8 Series Platform

    The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04.   The Document will be continuously updated with enable VPU, ubuntu...
    Gnar Fang
    last modified by Gnar Fang
  • Flashing Linux BSP using UUU

    Hello everyone, this document will explain on how to use the UUU (Universal Update Utility) tool to flash Linux to an i.MX device (i.MX 8MM).   Requirements:   MX 8M Mini EVK UUU tool documentation, avail...
    Aldo Gutierrez
    last modified by Aldo Gutierrez
  • Enable GmSSL which supports OSCCA Algorithm Toolbox on i.MX (updating for C-V2X)

    GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secu...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • iMX6 IPU TVIN Application Notes

    Attached is an application note for iMX6 TVIN use case, some internal review was done.   2016-10-08, change it to pdf file.
    Qiang Li - Mpu Se
    last modified by Karina Valencia Aguilar
  • i.MX8 MSCALE SERIES DDR Tool Release (V2.10)

    Important: For any comment/questions related with this document, create your question here https://community.nxp.com/community/imx Private messages will be ignored.          i.MX8MS...
    Oliver Chen
    last modified by m_j
  • Seamless switch between Android/Linux and M4 core using dpu on imx8qxp/qm.

    This document is aimed to introduce seamless switch on rear view camera function in android P9 auto, and this can also be referenced for sharing dpu(display process unit) between A core and m4 core on imx8qxp/qm platf...
    Bert Xu
    last modified by Bert Xu
  • i.MX Development Miscellanea(i.MX 开发杂记)

      Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.  ...
    Biyong Sun
    last modified by Biyong Sun
  • Docker On i.MX6UL With Ubuntu16.04

    Biyong Sun
    last modified by Biyong Sun
  • Change the clocks according to the display (non-default resolution)

    For the board imx8M Quad EVK running the Linux 4.14.78-1.0.0_ga version BSP, the resolutions 3840x2160,1920x1080, 1280x720, 720x480 are support in our default BSP. For the other resolutions how to make it work? This ...
    Rita Wang
    last modified by Rita Wang
  • Nvp6324 driver for imx8qm.

    Platform: imx8qm mek imx-yocto-L4.14.98_2.0.0_ga   Building Step: Apply the nvp6324 patches.   Symbol: IMX8_NVP6324 [=y] Type : tristate Prompt: IMX8 NVP6324 Driver Location: -> Device Drivers ->...
    Bert Xu
    last modified by Bert Xu
  • Porting KSZ9031 to i.MX BSP

    KSZ9031 is a very common PHY used with many ethernet design. This document will show you how to add it in u-boot and kernel.   1. Schematic     The MODE[3:0] strap-in pins are sampled and latched ...
    jimmychan
    last modified by jimmychan
  • Create an Ubuntu VM environment to build Yocto BSP

    Tool: VMware Workstation Player Linux Distribution : Ubuntu 16.04   1. Create the VM in VMware Workstation.     2. Select the .iso file to install the Ubuntu 16.04 in the VM.     3. In...
    jimmychan
    last modified by jimmychan
  • Docker On i.MX8QXP With Ubuntu

    Biyong Sun
    last modified by Biyong Sun
  • Docker On i.MX8MM With Ubuntu

    Biyong Sun
    last modified by Biyong Sun
  • iMX8QXP: Use JPEG decoder in M4 SDK

    iMX8QXP/iMX8QM have hardware JPEG decoder: The JPEG-D-X core. This is the example code to use this hw decoder in M4 SDK to decode JPEG files.     M4_JPEG_DECODER_SDK_2.5.1.7z The attached "rear_view_c...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • Task #2 - First build

    Synchronize your source code Create your local branch Why should I create a local branch? Choose your board Start to build Synchronize your source code  Source code you have is one week old n...
    Daiane Angolini
    last modified by Daiane Angolini
  • Task #1 - Download the source code

    Yocto Project versions and names Preparing host environment For virtual machine (VirtualBox): Download the source code from community Download the source code from NXP Code Aurora Yocto Project ver...
    Daiane Angolini
    last modified by Daiane Angolini
  • Quick and dirty setup of an i.MX evaluation board to program an i.MX board thru USB

    i.MX evaluation board can be a simple solution to program i.MX boards in a factory for instance. i.MX evaluation board are not for industrial usage, but you can find plenty of cheap i.MX insdustrial boards on the web...
    vincent.aubineau
    last modified by vincent.aubineau
  • Measure (RAW) NAND flash performances

    Using a RAW NAND is more difficult compared to eMMC, but for lower capacity it is still cheaper. Even with the ONFI (Open NAND Flash Interface) you can face initialization issue you can find by measure performan...
    vincent.aubineau
    last modified by vincent.aubineau
  • MX8X_4.14.98_ga_kernel_V3-20190903_chn.pdf .i.mx8x内核代码定制文档

    恩智浦BSP的内核定制 ........................................... 103 6.1 IO管脚配置与Pinctrl驱动 .................................... 103 6.2 新板bringup ........................................................ 118 6.3 更改调试串口: ...........
    John Li
    last modified by John Li