• iMX8QXP:使用RPMSG唤醒M4和A35

    [中文翻译版] 见附件   原文链接: iMX8QXP: Use RPMSG to wake up M4 and A35 
    Leo Lin
    last modified by Leo Lin
  • parseIVT - a script to help i.MX6 Code Signing

    The script to parse the IVT. It is a script tool for some case debug and  align the output of uboot log(u-boot-dtb.imx.log)   It is a bach script.    ./parseIVT u-boot-dtb.imx  0 0x00 | iv...
    Biyong Sun
    last modified by Biyong Sun
  • eMMC RPMB Enhance和GP

    [中文翻译版] 见附件   原文链接: eMMC RPMB Enhance and GP 
    Leo Lin
    last modified by Leo Lin
  • 通过i.MX6Q SABRE-SD上的SD卡刷新eMMC的指南

    [中文翻译版] 见附件   原文链接: Guide to flash an eMMC from SD Card on i.MX6Q SABRE-SD 
    Leo Lin
    last modified by Leo Lin
  • i.MX8引导过程和创建可引导映像

    [中文翻译版] 见附件   原文链接: i.MX8 Boot process and creating a bootable image 
    Leo Lin
    last modified by Leo Lin
  • SCFW:为iMX8QXP MEK启用PMIC外部看门狗

    [中文翻译版] 见附件   原文链接: SCFW: Enable PMIC external watchdog for iMX8QXP MEK 
    Leo Lin
    last modified by Leo Lin
  • Porting MARVELL WIFI-BT (88w8987) to i.MX8MNLPDDR4EVK 

    Hardware : i.MX8MNLPDDR4EVK   Build Yocto Image [Linux 4.14.98_2.3.1] Yocto Project Setup          $: mkdir imx-yocto-bsp        ...
    Gnar Fang
    last modified by Gnar Fang
  • i.MX 8QM MEK - IMX-AUD-IO - Audio out

    Quick notes on testing audio on the i.MX 8QuadMax MEK board with 4.19.35-1.1.0 BSP.   Hardware:   - Connect the MCIMX8QM-CPU to the MCIMX8-8X-BB.  - Connect the IMX-AUD-IO to the ...
    Renato Nogueira Frias
    last modified by Renato Nogueira Frias
  • Manually build Boot binary for i.MX8M Mini

    Sometimes it is helpful/faster to build a i.MX8MM boot binary outside of the Yocto environment.   There are instructions on how to accomplish this on different places, this document tries to provide an example f...
    Renato Nogueira Frias
    last modified by Renato Nogueira Frias
  • Info about softISP, eIQ

    About softISP Code : https://github.com/NXPmicro/gtec-demo-framework/tree/master/DemoApps/OpenCL/SoftISP/source Document : https://www.nxp.com/docs/en/application-note/AN12060.pdf demo is on path  /opt/imx-gp...
    Ives Liu
    last modified by Ives Liu
  • Using Cortex-M4 SDK to communicate with Cortex-A7 Android BSP on i.MX 7ULP-EVK

    This document shows how to run the multicore communication examples from MCUXpresso SDK while running the Android BSP on Cortex-A7 on i.MX 7ULP-EVK. Though this document is focused on the multicore demos, similar pro...
    Vanessa Maegima
    last modified by Vanessa Maegima
  • 移植Xenomai到i.MX8M平台上  (Xenomai on i.MX8MQ)

        Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknam...
    Xiaodong Zhang
    last modified by Xiaodong Zhang
  • 在Ubuntu16.04.2 LTS上下载并编译Android9.0.0-2.0.0 BSP

    [中文翻译版] 见附件   原文链接: Downloading and Compiling Android9.0.0-2.0.0 BSP on Ubuntu16.04.2 LTS 
    Leo Lin
    last modified by Leo Lin
  • 从用户空间的GPIO Sysfs接口访问用户空间的GPIO

    [中文翻译版] 见附件   原文链接: Accessing GPIO From UserSpace  
    Leo Lin
    last modified by Leo Lin
  • i.MX JTAG热插拔,无需重置

    [中文翻译版] 见附件   原文链接: i.MX JTAG hot plug with no reset 
    Leo Lin
    last modified by Leo Lin
  • I.MX处理器在Linux BSP上独立运行的详细操作

    [中文翻译版] 见附件   原文链接: Detailed Operations For Standalone On Linux BSP of I.MX Processors 
    Leo Lin
    last modified by Leo Lin
  • i.MX8X 网上设计资源向导

    www.nxp.com公网资源 .............................................. 2 1.1 www.nxp.com Documentation ................................ 3 1.2 www.nxp.com Tools&Software ............................... 7 2 nxp share point资...
    John Li
    last modified by John Li
  • 如何在没有UUU的情况下更新eMMC上的Linux内核和dtb

    [中文翻译版] 见附件   原文链接: How to upgrade  Linux Kernel and dtb on eMMC without UUU  
    Leo Lin
    last modified by Leo Lin
  • iMX8QM QXP参考补丁可将桥接芯片映射到无需EDID的显示器

    [中文翻译版] 见附件   原文链接: iMX8QM/QXP Reference Patch to Map Bridge Chip to Display without EDID 
    Leo Lin
    last modified by Leo Lin
  • 关于开发板 i.MX 8QuadMax 和 i.MX 8QuadXPlus 显示模块扩频技术的使用指南

    [中文翻译版] 见附件   原文链接: User Guide of Spread Spectrum Support for i.MX 8QuadMax and i.MX 8QuadXPlus Display 
    Leo Lin
    last modified by Leo Lin