• 将 KSZ9031 加入到 i.MX BSP

    [中文翻译版] 见附件   原文链接: Porting KSZ9031 to i.MX BSP 
    Leo Lin
    last modified by Leo Lin
  • 带有Arm装置的容器技术在i.MX6UL的使用

    [中文翻译版] 见附件   原文链接: Docker On i.MX6UL With Ubuntu16.04  
    Leo Lin
    last modified by Leo Lin
  • 从TensorFlow开始你的机器学习之旅

    [中文翻译版] 见附件   原文链接: Start your machine learning journey from tensorflow playground 
    Leo Lin
    last modified by Leo Lin
  • OpenVX视觉图像扩展API简介 – 基础API

    [中文翻译版] 见附件   原文链接: OpenVX Vision Image Extension API Introduction - Basic API 
    Leo Lin
    last modified by Leo Lin
  • i.MX8QXP gamma校正

    [中文翻译版] 见附件   原文链接: i.MX8QXP gamma tuning 
    Leo Lin
    last modified by Leo Lin
  • i.MX6Q捕获原始(bayer)数据和debayer

    [中文翻译版] 见附件   原文链接: i.MX6Q capture raw(bayer) data and debayer  
    Leo Lin
    last modified by Leo Lin
  • How to Disable the DM-Verity option in your Android device.

    To disable the Android dm-verity in the new devices you should have the below. A Window/Linux computer The Android SDK platform-packages tools.   Download the Android Packages tool.   To use the Android ...
    Diego Adrian Cuevas
    last modified by Diego Adrian Cuevas
  • mek_8qm/evk_8mq enable uSD/M.2 8987 wifi module

    All below changes are done based on imx_android-10.0_5.4.y.   mek_8qm enable uSD 8987 wifi            1. hardware rework      ...
    Andy Tian
    last modified by Andy Tian
  • iMX8QXP: Use JPEG decoder in M4 SDK

    iMX8QXP/iMX8QM have hardware JPEG decoder: The JPEG-D-X core. This is the example code to use this hw decoder in M4 SDK to decode JPEG files.     M4_JPEG_DECODER_SDK_2.5.1.7z The attached "rear_view_c...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • Build Ubuntu For i.MX8 Series Platform

    The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04.   The Document will be continuously updated with enable VPU, ubuntu...
    Gnar Fang
    last modified by Gnar Fang
  • Dummy audio codec -  play & record on i.MX8MM

    Several customers met problem on audio codec porting. In order to figure out cpu dai setting problem or codec dai problem. Create the dummy codec for test purpose.    What this dummy codec can do This dumm...
    MaxTsai
    last modified by MaxTsai
  • iMX8QM, IMX8QXP: How to adjust DDR clock for EMC test

    For IMX8QM and iMX8QXP, the DDR config is in SCFW porting kit with DDR script.   After boot, for iMX8QM, the LPDDR4 clock is set to 1.6GHz, and for iMX8QXP, after boot, the LPDDR4 clock is set to 1.2G...
    Qiang Li - Mpu Se
    last modified by Qiang Li - Mpu Se
  • Udoo开发板中的ArchLinux

    [中文翻译版] 见附件   原文链接: ArchLinux in Udoo board 
    Leo Lin
    last modified by Leo Lin
  • 系统控制器固件101-资源管理服务

    [中文翻译版] 见附件   原文链接: System Controller Firmware 101 - Resource management service 
    Leo Lin
    last modified by Leo Lin
  • 使用Cortex-M4 SDK与i.MX 7ULP-EVK上的Cortex-A7 Android BSP通信

    [中文翻译版] 见附件   原文链接: Using Cortex-M4 SDK to communicate with Cortex-A7 Android BSP on i.MX 7ULP-EVK 
    Leo Lin
    last modified by Leo Lin
  • 在i.MX8QXP的MEK板上进行简单的CAN(FD)测试

      [中文翻译版] 见附件   原文链接: Simple CAN (FD) test on i.MX8QXP's MEK board 
    Leo Lin
    last modified by Leo Lin
  • 为Yocto 项目在i.MX8MQ 和 i.MX8QM QXP 启用 CLBlast

    [中文翻译版] 见附件   原文链接: Enable CLBlast on i.MX8MQ and i.MX8QM/QXP for Yocto project 
    Leo Lin
    last modified by Leo Lin
  • i.MX 8 - RTSP Streaming Support

    Recently I published this i.MX Dev Blog post about the Gateworks plugin gst-variable-rtsp-server support for i.MX 6. Now, you can check how to use it on i.MX 8 SoCs as well.   1. Preparing the im...
    Marco Antonio Franchi
    last modified by Marco Antonio Franchi
  • i.MX8QXP capture raw(bayer) data and debayer

    This doc show: on i.MX8QXP MEK board, configure ov5640 sensor(parallel interface) output 5MP(2592x1944) RAW(Bayer) data at 15fps, and Parallel Capture Subsystem and Image Sensor Interface capture RAW RGB data, and i.M...
    PengFushi
    last modified by PengFushi
  • i.MX 8 Camera Use Cases

    This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera op...
    Marco Antonio Franchi
    last modified by Marco Antonio Franchi