• i.MX 8M Family DDR Tool Release

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private mess...
    Oliver Chen
    last modified by m_j
  • unable to connect to git.freescale.com

    Recently many customers faced the issue about connecting the git.freesacle .com failed when they built old bsp version like 4.1.15 or 3.14.52,  when the customer repo init according to the yocto user guide, they ...
    Joan Xie
    last modified by Joan Xie
  • i.MX 8/8X Family DDR Tools Release

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages ...
    asimzaidi
    last modified by asimzaidi
  • i.MX 6/7 DDR Stress Test Tool

    Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private mess...
    Oliver Chen
    last modified by asimzaidi
  • iMX 8M Mini Register Programming Aid DRAM PLL setting

    The Register Programming Aid (RPA) provides a default DRAM PLL setting (DRAM frequency) based on the default setting supported in u-boot.  It is highly recommended to use the default DRAM frequency settings in th...
    asimzaidi
    last modified by asimzaidi
  • How to change Linux Kernel configuration file in Yocto Project metalayer

    How to change Linux Kernel configuration file in Yocto Project metalayer Preparing the requirements Download the metalayer Git clone the Linux Kernel source code Customize the configuration Copy the ...
    Daiane Angolini
    last modified by Daiane Angolini
  • Safe video switch using ADV7180 and i.MX6Q Automotive Board

    i.MX6Q Automotive board has one ADV7180 analog video decoder with 2 video inputs. By default, only input 1 is used (connector J42).     To connect 2 analog video sources and switch the display between the...
    rogeriopimentel
    last modified by Adrian Puga Candelario
  • i.MX创建Android SDCard镜像

    [中文翻译版] 见附件   原文链接: i.MX Create Android SDCard Mirror 
    Leo Lin
    last modified by Leo Lin
  • 如何转存GPT SD卡镜像

    [中文翻译版] 见附件   原文链接: How to Dump a GPT SDCard Mirror(Android O SDCard Mirror) 
    Leo Lin
    last modified by Leo Lin
  • 将UART0 RX TX用作iMX8QXP板上的SCU UART调试端口

    [中文翻译版] 见附件   原文链接: Use UART0 RX/TX as SCU UART debug port on iMX8QXP boards 
    Leo Lin
    last modified by Leo Lin
  • 适用于i.MX平台的OTA在Android中的更新指南

    [中文翻译版] 见附件   原文链接: Guide to OTA Update in Android for i.MX platforms 
    Leo Lin
    last modified by Leo Lin
  • Compiling L5.4.3_1.0.0 BSP On Ubuntu 180.4 LTS

    We will cross compile L5.4.3_1.0.0 on ubuntu18.04 LTS platform in three steps. 1. Installing Ubuntu 18.04 to vmplayer14 & Configuring Ubuntu 18.04 LTS 2. Compiling L5.4.3_1.0.0 BSP According to Steps in i.MX_Yoc...
    Wigros Sun
    last modified by Wigros Sun
  • i.MX8MM & i.MX8MQ USB2.0 Design Without USB TYPE-C

    -BACKGROUND       Since the release of i.MX8MQ and i.MX8M Mini, some customers have submitted questions about the design of USB2.0 for these two processors: due to the needs of the projec...
    Wigros Sun
    last modified by Wigros Sun
  • i.MX Development Miscellanea(i.MX 开发杂记)

      Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.  ...
    Biyong Sun
    last modified by Biyong Sun
  • i.MX6 DDR calibration/stress for Mass Production

    Biyong Sun
    last modified by Biyong Sun
  • i.MX7D DRAM Register Programming Aid

    These are detailed programming aids for the registers associated with DRAM initialization (LPDDR3, DDR3, and LPDDR2). The last work sheet tab in the tool formats the register settings for use with the ARM DS5 debugger...
    m_j
    last modified by m_j
  • 在i.MX8MQ 8MM中添加录音驱动程序

    [中文翻译版] 见附件   原文链接: Add audio record driver in i.MX8MQ/8MM 
    Leo Lin
    last modified by Leo Lin
  • iMX8QXP:使用RPMSG唤醒M4和A35

    [中文翻译版] 见附件   原文链接: iMX8QXP: Use RPMSG to wake up M4 and A35 
    Leo Lin
    last modified by Leo Lin
  • parseIVT - a script to help i.MX6 Code Signing

    The script to parse the IVT. It is a script tool for some case debug and  align the output of uboot log(u-boot-dtb.imx.log)   It is a bach script.    ./parseIVT u-boot-dtb.imx  0 0x00 | iv...
    Biyong Sun
    last modified by Biyong Sun
  • eMMC RPMB Enhance和GP

    [中文翻译版] 见附件   原文链接: eMMC RPMB Enhance and GP 
    Leo Lin
    last modified by Leo Lin